element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Booting cisco ios on Raspberry pi
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 30 subscribers
  • Views 2435 views
  • Users 0 members are here
  • idea
  • ras_pi
Related

Booting cisco ios on Raspberry pi

e14 Contributor
e14 Contributor over 10 years ago

i was thinking about booting up cisco ios on raspberry pi. help me regarding that. is it possible to do so?   

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hi jigar

    It looks like your question is answered in this how to guide https://www.raspberrypi.org/forums/viewtopic.php?t=96735 .  Please let us know how you get on.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 10 years ago

    Hi Jigar,

     

    This is a duplicate post of the one you posted a few minutes before this one, here: Running cisco ios on raspberry pi .

    Better to keep one thread, otherwise two (or more) may get considered as spam.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Before we enable logging you should verify that your Pi has its clock configured correctly. ser2net will add a timestamp to its log files and logging is pretty much useless if you don’t have the correct date or time.

    By default it will synchronize its time by using NTP but the timezone might be incorrect. Changing the timezone is easy to do:

    $ sudo cp /usr/share/zoneinfo/Europe/Amsterdam /etc/localtime

    This will change the timezone to CEST (Central European Time) for me. Let’s verify it:

    $ date

    Fri Jul 19 11:55:27 CEST 2013

    That’s looking good to me. Now we’ll create a folder that will hold our log files. I will save everything in the /var/log/ser2net folder:

    $ sudo mkdir /var/log/ser2net

    Now you need to edit the /etc/ser2net.conf file again and add the following:

    TRACEFILE:tr1:/var/log/ser2net/tr-p-Y-M-D-H:i:s.U

    4001:telnet:0:/dev/ttyUSB0:9600 8DATABITS NONE 1STOPBIT banner tr=tr1 timestamp

    The ‘TRACEFILE’ line is new and at the end of the 4001:telnet… line we will add “tr=tr1 timestamp”. This will enable logging for this port and add timestamps to the log files.

    You will have to restart ser2net before logging is active. The next time you connect you will see the log files in the /var/log/ser2net folder:

    $ ls /var/log/ser2net

    tr-4001-2013-Jul-19-09:18:26.893894

    You now have a console server that saves logging information. In the next part I’ll show you how to enable wireless support and how to secure your Pi:

    Wireless Access Point

    Most wireless adapters also support access point mode. This is very useful since we can make our Pi broadcast a SSID and let wireless clients connect to it. This turns our Pi into a wireless console server…nice!

    Plug in your wireless USB adapter and see if it’s recognized:

    $ lsusb

    Bus 001 Device 002: ID 0424:9514 Standard Microsystems Corp.

    Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub

    Bus 001 Device 003: ID 0424:ec00 Standard Microsystems Corp.

    Bus 001 Device 004: ID 0bda:8179 Realtek Semiconductor Corp.

    Bus 001 Device 005: ID 0403:6001 Future Technology Devices International, Ltd FT232 USB-Serial (UART) IC

    Keep in mind that the USB port of the Raspberry Pi has limited power and not all wireless adapters are supported. Take a look at the elinux Rpi page to see which adapters are supported.

    If your USB device is recognized we still have to check if our wireless drivers are operational:

    $ iwconfig

    wlan0 unassociated Nickname:"<WIFI@REALTEK>"

    Mode:Managed Frequency=2.412 GHz Access Point: Not-Associated

    Sensitivity:0/0

    Retry:off RTS thr:off Fragment thr:off

    Power Management:off

    Link Quality:0 Signal level:0 Noise level:0

    Rx invalid nwid:0 Rx invalid crypt:0 Rx invalid frag:0

    Tx excessive retries:0 Invalid misc:0 Missed beacon:0

    If iwconfig doesn’t give you any information you probably have an issue with drivers.

    Once your wireless card is up and running we will install hostapd. This configures the wireless adapter as an access point:

    $ sudo apt-get install hostapd

    We’ll configure the wireless adapter to use a static IP address instead of DHCP:

    $ sudo vi /etc/network/interfaces

    Remove the following two lines from this file:

    iface wlan0 inet manual

     

     

    wpa-roam /etc/wpa_supplicant/wpa_supplicant.conf

    And replace them with the following lines:

    iface wlan0 inet static

    address 172.16.82.254

    netmask 255.255.255.0

    Our wlan0 interface will use static IP address 172.16.82.254 /24. Now we’ll configure hostapd to set some parameters for the access point:

    $ sudo vi /etc/hostapd/hostapd.conf

    ssid=Console

    wpa_passphrase=mysecurepassphrase

    wpa=3

    You can leave most of the settings in this file alone but I will change the SSID and the WPA passphrase. The passphrase will be “mysecurepassphrase” and wpa=3 means we will support WPA and WPA2. Let’s start hostapd:

    $ sudo service hostapd start

    To make sure hostapd runs after rebooting the Pi we’ll add it to the startup list:

    $ sudo update-rc.d hostapd enable

    Your Raspberry Pi should now be broadcasting SSID “Console” but wireless clients will have to configure a static IP address. We’ll fix this by installing a DHCP server:

    $ sudo apt-get install dnsmasq

    At the bottom of this file you should add the following two lines:

    interface=wlan0

    dhcp-range=172.16.82.10,172.16.82.100,12h

    This ensures that the DHCP server only runs for wireless clients and that we’ll use 172.16.82.10 – 172.16.82.100 for DHCP clients.

    Restart the DHCP server:

    $ sudo service dnsmasq restart

    [ ok ] Restarting DNS forwarder and DHCP server: dnsmasq.

    And make sure it boots at startup:

    $ sudo update-rc.d dnsmasq enable

    Your Raspberry Pi is now configured as an access point. Wireless clients are now able to connect to it and access the console port by telnetting to 172.16.82.254:4001.

    In the final part of this tutorial we’ll take a look at some security measures. Your Pi is using a default username / password and the firewall is allowing all traffic.

    Security

    Even though the Pi is a little box, it’s still a fully functional Linux server. It’s best to take some security measures to protect it. I’m going to change the default username, tighten SSH security a bit and add some rules to the IPTables firewall.

    Change username

    First i’ll replace the default user ‘pi’ with my own username:

    $ sudo adduser renemolenaar

    Adding user `renemolenaar' ...

    Adding new group `renemolenaar' (1002) ...

    Adding new user `renemolenaar' (1001) with group `renemolenaar' ...

    Creating home directory `/home/renemolenaar' ...

    Copying files from `/etc/skel' ...

    Don’t forget to add a password:

    $ sudo passwd renemolenaar

    Enter new UNIX password:

    Retype new UNIX password:

    passwd: password updated successfully

    And we need to add the new user to the sudoers list or you can’t run any important commands:

    $ sudo vi /etc/sudoers

    Change the following line:

    pi ALL=(ALL) NOPASSWD: ALL

    to:

    renemolenaar ALL=(ALL) NOPASSWD: ALL

    Now try if you are able to log into the Pi using your new username and if you can use sudo. When it’s working we’ll delete the old ‘pi’ account:

    $ sudo deluser pi

    Removing user `pi' ...

    Warning: group `pi' has no more members.

    Done.

    I always like to change the default SSH port and ensure that the root user can’t login through SSH directly:

    $ sudo vi /etc/ssh/sshd_config

    Now change the following line:

    PermitRootLogin yes

    To:

    PermitRootLogin no

    And change the port number to something else:

    Port 22

    To:

    Port 10050

    Don’t forget to restart SSH to apply the changes you made:

    $ sudo service ssh restart

    This makes SSH a little bit more secure.

    IPTables Firewall

    Your Raspberry Pi has the IPtables firewall installed on it by default but we’ll have to add some rules ourselves. I want to make sure outside LAN users can only connect to TCP 4001 for the console port and TCP port 10050 to access SSH. The same rules will apply to wireless users with the exception that they also will request an IP address through DHCP.

    Create a new file for IPTables:

    $ sudo vi /etc/iptables-rules

    And add the following lines to it:

    *filter

    :INPUT ACCEPT [0:0]

    :FORWARD ACCEPT [0:0]

    :OUTPUT ACCEPT [0:0]

    -A INPUT -i lo -j ACCEPT

    -A INPUT -m conntrack --ctstate RELATED,ESTABLISHED -j ACCEPT

    # LAN Rules

    -A INPUT -i eth0 -p tcp -m tcp --dport 4001 -j ACCEPT

    -A INPUT -i eth0 -p tcp -m tcp --dport 10050 -j ACCEPT

    # WIRELESS Rules

    -A INPUT -i wlan0 -p udp -m udp --dport 67 -j ACCEPT

    -A INPUT -i wlan0 -p tcp -m tcp --dport 4001 -j ACCEPT

    -A INPUT -i wlan0 -p tcp -m tcp --dport 10050 -j ACCEPT

    # Allow ICMP packets necessary for MTU path discovery

    -A INPUT -p icmp --icmp-type fragmentation-needed -j ACCEPT

    # Allow echo request

    -A INPUT -p icmp --icmp-type 8 -j ACCEPT

    -A INPUT -j DROP

    COMMIT

    Save your file and load the firewall rules:

    $ sudo iptables-restore < /etc/iptables-rules

    Let’s make sure these rules are loaded when the Pi reboots:

    $ sudo vi /etc/network/interfaces

    Add the following line at the bottom of the interfaces file:

    pre-up /sbin/iptables-restore < /etc/iptables-rules

    This is a good moment to reboot your Pi and verify that iptables is running:

    $ sudo iptables -L

    Chain INPUT (policy ACCEPT)

    target     prot opt source               destination        

    ACCEPT     all  --  anywhere             anywhere           

    ACCEPT     all  --  anywhere             anywhere             ctstate RELATED,ESTABLISHED

    ACCEPT     tcp  --  anywhere             anywhere             tcp dpt:4001

    ACCEPT     tcp  --  anywhere             anywhere             tcp dpt:10050

    ACCEPT     tcp  --  anywhere             anywhere             tcp dpt:4001

    ACCEPT     tcp  --  anywhere             anywhere             tcp dpt:10050

    ACCEPT     udp  --  anywhere             anywhere             udp dpt:bootps

    ACCEPT     icmp --  anywhere             anywhere             icmp fragmentation-needed

    ACCEPT     icmp --  anywhere             anywhere             icmp echo-request

    DROP       all  --  anywhere             anywhere           

     

     

    Chain FORWARD (policy ACCEPT)

    target     prot opt source               destination        

     

     

    Chain OUTPUT (policy ACCEPT)

    target     prot opt source               destination

    Your Raspberry Pi is now protected by IPTables.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 10 years ago in reply to e14 Contributor

    This is useful information (although not really what the question relates to), but better to just link to the original article by Rene Molenaar, or at least cite the source:

    https://networklessons.com/network-management/raspberry-pi-as-cisco-console-server/