Hi, Just wondering if you are able to mod a camera to be detected on an iPad (Jailbroken) and make it stylishly fit into a Case...
M.M
Singapore
Hi, Just wondering if you are able to mod a camera to be detected on an iPad (Jailbroken) and make it stylishly fit into a Case...
M.M
Singapore
Of course, yes.
Can you provide the communication interface of iPad? then you can write or down a driver and application software to drive and dispay.
oliver zhang
Of course, yes.
Can you provide the communication interface of iPad? then you can write or down a driver and application software to drive and dispay.
oliver zhang
i googled the connection and found this out
http://www.allpinouts.org/index.php/Apple_iPod,_iPad_and_iPhone_dock
But from this list of the connections i dont see how data(camera feed) can be sent in to the device (might be pins 25-27), rather than all of the pins are related to Outputs.
About writing a driver, i am unable to do so which is why i have raised the quesetion, if ben heck can make it possible
Mohamed
Singapore
Apple sells an iPad Camera Connection Kit on its storage:
Hi,
yes they do sell the camera connection kit though i think if you plug in a webcam there is not enough power supplied to power the webcam.
thus a special cable designed to be able to interface with the ipad and a software which allows the image seen to be viewed on the ipad is needed,
which brings me back to my first question is it possible, especially by ben heck.
M.M
Singapore
Pour ceux qui ont un iPhone ou un iPod touch, la fonction webcam est possible sur ipad
Ainsi, en téléchargeant Camera A sur iPad (0,99$) et Camera B sur iPhone 3Gs (gratuit), il est possible de connecter en bluetooth les deux et de partager l'appareil photo du téléphone d'Apple."
I dont actually understand french, but i can decipher that it is some app which uses ur iphone as a camera, but my whole theory/idea is something which can be just plugged in to the ipad and wa'la ... but what i do understand is the complexity of this idea as there are a few parts involved like for eg. the hardware(camera module) and the software (for the imaging sensor inside the camera to translate what it sees in digital form) [driver]
thank you
M.M
Singapore
Hi Oliver,
Do you know if this connection kit is available in the UK?
Hi kirstylou1,
Here below the links
http://store.apple.com/uk/search?find=Apple+iPad+Camera+Connection+Kit&mco=Nzc1MjMwNg