• Products and Partners
    Products and Partners
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
element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Activate BJT with Digital HIGH
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 7 replies
  • Answers 3 answers
  • Subscribers 31 subscribers
  • Views 867 views
  • Users 0 members are here
  • hardware
  • arduino
Related

Activate BJT with Digital HIGH

nbuuck
nbuuck over 15 years ago

Hi all. It's been a while since I studied transistors and I'm having a bit of trouble adapting my needs to the theory of transistors. Specifications for transistors detail the voltage across combinations of the collector, base, and emitter of the transistor. However, my need and thought process is based on the indepentent voltage on each pin of the BJT. My need is to switch a +12V supply completely on or off (trickle current is not a problem, though; we're not being idealistic) using a digital HIGH on the base (I'm planning on using an Arduino Uno, so if someone knows the characteristic voltage of a HIGH on the Uno's digital I/O pins, assume approximately that). Is a BJT appropriate for my needs? Can you think of or suggest a BJT that approximately meets these specifications?

  • Sign in to reply
  • Cancel
Parents
  • Catwell
    0 Catwell over 15 years ago

    You might want to use a relay that completely cuts off the input power instead. Even if you use a BJT, some power will leak through. Usually it is not enough to cause any issues, but I personally like to cut the power completely off. (Safety issues)

     

    Is this 12V a DC source?

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • nbuuck
    0 nbuuck over 15 years ago in reply to Catwell

    Cabe,

     

    Thanks for your suggestion; I like it! This is for an automotive application, and given the popularity of relays for in automotive applications, I had considered it, but didn't really give it as much consideration as I should have, so thank you. That said, it is indeed a 12V DC source.

     

    - Nathan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • nbuuck
    0 nbuuck over 15 years ago in reply to Catwell

    Cabe,

     

    Thanks for your suggestion; I like it! This is for an automotive application, and given the popularity of relays for in automotive applications, I had considered it, but didn't really give it as much consideration as I should have, so thank you. That said, it is indeed a 12V DC source.

     

    - Nathan