• Products and Partners
    Products and Partners
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
element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Servo based Motor-Fader idea
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 30 subscribers
  • Views 1352 views
  • Users 0 members are here
  • controller
  • pro_tools
  • servo
  • motor_fader
Related

Servo based Motor-Fader idea

e14 Contributor
e14 Contributor over 14 years ago

Hey guys,

A quick intro of who I am:

I'm a Sound Design student at Savannah College of Art and Design.  Currently this quarter I'm taking the "Sound in Media" class, (essentially the history of sound) and a few days ago we watched an excellent Doc on the BBC Radiophonic Workshop,  You can watch this Documentary on youtube here.

 

In the doc I noticed that most of the audio faders (essentially a potentiometer) they were using were in an arc formation.  As if the fader knob was attached to a rotary pot, instead of using a linear pot.  That got me thinking...

 

As an sound designer, I'll be mostly using Pro Tools for manipulating sound.  And one of the quintessential tools used for mixing sound is the motor fader.  A motor fader is a linear pot (usually used with midi, or some other automation protocol) with a servo or motor attached to it.  This gives the fader the ability to move according to recorded automation.  Ultimately this means the audio mixer can tweak automation in real time without have the automation jump to whatever the pot was set to previously.  Unfortunately motor faders can be very expensive, individual replacement motor faders can often cost $60+ each, and most fader banks are 8-16 faders per unit.

 

So here's my idea, instead of using cost-prohibitive commercial motor-faders, why not use rotary servos with the (apparently) classic arc fader design.  My current problem is that most RC hobby servos use a PWM signal to control them, and the internal potentiometer is used for internal feedback.  For this to work I need to be able to tap into the resistive values of the pot, while the servo is moving, and use those values to control the faders within Pro Tools.  Then the automation data feedback sent from Pro Tools can control the faders position.  I'm thinking of a capacitive sensor on a metal fader knob to deactivate the servo motor so you can move it freely.


Essentially, is it possible to modify an RC hobby servo so one could measure the resistive values of the internal potentiometer?

 

I'm away at school at the moment, so I won't be able to work on this for another couple of weeks, but I figured I'd knock out a few kinks in my idea before I start tinkering.

 

[EDIT]  I scrubbed through the doc on youtube and found the shot of the arc faders here: http://youtu.be/t9M9k4JnqCk?t=7m6s

  • Sign in to reply
  • Cancel
Parents
  • Catwell
    0 Catwell over 14 years ago

    Bypass the use of the servo and use a Digital Potentiometer. Here is an example: Analog Devices AD5171BRJZ10-R2 - IC 10Kohm digital pot.Analog Devices AD5171BRJZ10-R2 - IC 10Kohm digital pot.

     

    Try to attack the idea via a "no moving parts" viewpoint.

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to Catwell

    Thanks for the reply,

     

    I was apparently not clear on my intentions.  I'm not trying to mix analogue audio through the potentiometer, I'm using the pot to send analogue data to control digital automation within the ProTools software.  Then ProTools will send data back to the servo to match the recorded automation.  I re-read my original post, and I can see how you could come to that conclusion, sorry for the misunderstanding.

     

    Here's one of the mixing consoles we use at SCAD: http://www.avid.com/US/products/ICON-D-Control-ES

    And a significantly cheaper option: http://www.bhphotovideo.com/c/product/321870-REG/Behringer_BCF2000_B_CONTROL_FADER_BCF2000.html

    The Behringer B-Control is on my wish-list, and I'm using it as a maximum price point for this project.

    Essentially, if I'm not able to create a viable fader bank with this idea, for less than $179 in parts costs, then it's not worth creating.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to Catwell

    Thanks for the reply,

     

    I was apparently not clear on my intentions.  I'm not trying to mix analogue audio through the potentiometer, I'm using the pot to send analogue data to control digital automation within the ProTools software.  Then ProTools will send data back to the servo to match the recorded automation.  I re-read my original post, and I can see how you could come to that conclusion, sorry for the misunderstanding.

     

    Here's one of the mixing consoles we use at SCAD: http://www.avid.com/US/products/ICON-D-Control-ES

    And a significantly cheaper option: http://www.bhphotovideo.com/c/product/321870-REG/Behringer_BCF2000_B_CONTROL_FADER_BCF2000.html

    The Behringer B-Control is on my wish-list, and I'm using it as a maximum price point for this project.

    Essentially, if I'm not able to create a viable fader bank with this idea, for less than $179 in parts costs, then it's not worth creating.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Catwell
    0 Catwell over 14 years ago in reply to e14 Contributor

    If you are just sampling the sound for analysis for the system, then I would recommend a data acquisition module or analogue input of a micro-controller. > Analyse the data as needed > the micro-controller can then control the servo motors.

     

    You can get away with controlling one servo motor with a PIC 12F675PIC 12F675, while also sampling analogue data from 1 - 3 other sources.

     

    image

     

    Cabe

    http://twitter.com/Cabe_e14