element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum I have a 5v usb fan and I want to reduce the speed.
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 18 replies
  • Subscribers 36 subscribers
  • Views 12255 views
  • Users 0 members are here
Related

I have a 5v usb fan and I want to reduce the speed.

rayjai
rayjai over 14 years ago

I have a 5v usb fan and I want to reduce the speed. how would I do it?

the fans on my laptop cooler is too loud.

thanks

  • Sign in to reply
  • Cancel

Top Replies

  • YT2095
    YT2095 over 14 years ago +1
    you could also use a simple 1n4001 diode in series with the positive wire, to drop .7 of a volt for each diode you use, doing it this way still lets you draw exactly the same amount of current (about 500ma…
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    @Rayjay

    What needs to be understood here is that a potentiometer will work, but it is not built to handle the load of something like a fan, so its lifespan would be reduced. A good simple method is to put a diode in series with the fan, a common diode has a voltage drop of about 0.7v so this will give you 4.3v from your 5, to drop it more simply add another diode Just make sure you buy (salvage) one that can handle 500mA (milliamp) or more such as 9564993RL. VT2095's circuit would allow you to actually vary the voltage. However if your fan is noisy, it may be worth looking at the fan itself for damage/wear.

     

     

    5v-4.7v

    image

    5v-3.6v

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    @Rayjay

    What needs to be understood here is that a potentiometer will work, but it is not built to handle the load of something like a fan, so its lifespan would be reduced. A good simple method is to put a diode in series with the fan, a common diode has a voltage drop of about 0.7v so this will give you 4.3v from your 5, to drop it more simply add another diode Just make sure you buy (salvage) one that can handle 500mA (milliamp) or more such as 9564993RL. VT2095's circuit would allow you to actually vary the voltage. However if your fan is noisy, it may be worth looking at the fan itself for damage/wear.

     

     

    5v-4.7v

    image

    5v-3.6v