element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum How possible is it to make a wireless 360 controller into a wired one for use on PC?
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 12 replies
  • Subscribers 32 subscribers
  • Views 7472 views
  • Users 0 members are here
  • 360
  • controller
  • wired
  • wireless
Related

How possible is it to make a wireless 360 controller into a wired one for use on PC?

Former Member
Former Member over 12 years ago

Just like the title says, would it be possible to make a wireless 360 controller into a wired controller for use on a pc? I'm tired of getting the charge packs that just stop charging after a while or after they get glitched up.

 

Thanks

  • Sign in to reply
  • Cancel

Top Replies

  • elevatorguy
    elevatorguy over 12 years ago +1
    The hard way: If you are comfortable with soldering and like to take the controller apart, then it is possible, for example, to open up the controller, solder wires from buttons, trigger and joystick potentiometers…
  • t_martins
    0 t_martins over 12 years ago

    If you need only the conction from the controller to the pc you could use a receiver from microsoft (only works on windows) and for the batery problem just use a charger that you can play ate the same time.


    http://www.microsoft.com/games/en-US/Hardware/Controllers/Pages/XboxWirelessGamingReceiverforWindows.aspx/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 12 years ago in reply to t_martins

    The goal of this would be to aviod having a battery pack and also not having to get the receiver.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • t_martins
    0 t_martins over 12 years ago in reply to Former Member

    I think you can use one of these cable to always charge the controler,the part hacking the controlor to add a usb cable i think that is very hard and in my opnion not worth the effort.

     

    The only option is buying the receiver i think. image

     

    http://www.amazon.co.uk/Charger-Cable-Wireless-Controller-Xbox/dp/B004K3N4VU/ref=pd_bxgy_vg_h__text_y

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 12 years ago

    It would be very hard unless there is already a USB controller in there that is either not connected to anything or connected to the wirless module. If there is you would be able to just wire it to USB, but without looking in the controller there is no way to tell if that is the case, and it would have to be clearly labled, which is extremely unlikely.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 12 years ago in reply to Former Member

    Well, that's why I'm posting here. Maybe Ben can figure it out. I have plenty of charge cables that I wouldn't mind repurposing to make a wired controller out of a wireless one.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • elevatorguy
    0 elevatorguy over 12 years ago

    The hard way:

    If you are comfortable with soldering and like to take the controller apart, then it is possible, for example, to open up the controller, solder wires from buttons, trigger and joystick potentiometers, coming out to where the battery pack used to be, and put a teensy there acting as a USB HID gamepad to the computer, wiring the power and ground from the teensy to the gamepad, to power it. (I would double check the voltages, but it's probably 3.3V on both)

     

    Additionaly, it could be possible to still use it with the xbox 360, it would work wirelessly, but using the USB for power. If we are not interfaceing with a chip in the xbox gamepad, but reading the buttons and pots directly (easier programming, but 21 wires), then technically it could be used with both at the same time. We'd have to use pretty thin wires, to fit it all in there. I havn't modded a 360 controller, but when I did a N64 controller like this, it was interesting getting it back together. But in the end, I had a N64 controller that I made myself that showed up as a USB gamepad on the computer.

     

    It's alot of work, but if interested, then it can be a fun and rewarding project image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 12 years ago in reply to elevatorguy

    I'm good at soldering, so that wouldn't be a problem. I was thinking that there might be existing circuitry that can be used, because the pc recognizes a 360 controller plugged in when using the play and charge cable. Sadly, it does not operate like a wired controller when you have it plugged into the pc using the charge cable.

     

    edit:

    maybe these pcbs can help out, it's interesting that the sync button is labeled as "wire/wireless plug switch"

     

    wired pcb

    http://www.slagcoin.com/joystick/pcb_diagrams/360_diagram6.jpg

    http://www.slagcoin.com/joystick/pcb_diagrams/360_diagram1.jpg

     

     

    wireless pcb

    http://www.slagcoin.com/joystick/pcb_diagrams/360_diagram5.jpg

    http://www.slagcoin.com/joystick/pcb_diagrams/360_diagram7.jpg

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • joecr
    0 joecr over 12 years ago in reply to Former Member

    Way to much work & it wouldn't really be cost efective. Just go to the store & buy a wired controller. It's easier & faster than setting everything to use a teensy.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jspliff
    0 jspliff over 12 years ago

    I use the charge cable plugged in to charge my pack but what I did was take the receiver out of an old 360 and wired it to usb. It works plug and play with the microsoft xbox 360 drivers. Gotta sync the controller to the 360 first though and cant resync again unless you plug back to 360. Maybe a little unecessary work but I wanted a way to use my 360 controller with my pc and I didn't wanna buy anything.

     

    Here is a picture.

     

    Red: 5V+           Black: Ground

    Green: Signal +  White: Signal -

     

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jspliff
    0 jspliff over 12 years ago in reply to jspliff

    Sorry I just reread your post and I'm guessing you have the wireless pc receiver already. If these points exist on the reciever though I'm pretty sure it would be easy to find them on the controller itself.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>