Products
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
element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Viewer Question: Simple Pinball
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 32 subscribers
  • Views 781 views
  • Users 0 members are here
  • pinball_machine
  • hack
  • hardware
  • build
  • pinball
  • idea
  • viewer_question
  • arduino
  • question
Related

Viewer Question: Simple Pinball

e14 Contributor
e14 Contributor over 13 years ago

     Does anyone know if it is possible to buid a simple pinball machine with only a small microcontroller? The raspberry pi can act as a microcontroller, and I was wondering if it could run from the Pi. If not, could it run from an arduino? The machine would be very simple and would use LED's or a 2-digit display instead of a DMD or an LCD. The switches on the board would just add another led to light up, or for a couple more numbers would add on the display. Is this possible? I've been wanting to do this project, and I want to know if it can be done.

 

-Nick

  • Sign in to reply
  • Cancel
Parents
  • colecago
    0 colecago over 13 years ago

    Ben's board uses a chipkit which is Arduino compatible.  It does use another processor, a parallax, which does the Audio and DMD.  So I don't see why you couldn't just do it with the Arduino and no parallax processor if you offload the Audio and Video onto the Arduino, which wouldn't be so hard if using a small character display.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ckraft
    0 ckraft over 13 years ago in reply to colecago

    He could also run the whole thing off the Parallax Propeller which is what Ben's first pinball machine did.

     

    To the point about the Raspberry Pi, its a neat device but it is not a microcontroller and cannot act as a microcontroller. There's a specific difference between the devices like that used in the Raspberry pi, which is basically a moble processor, and the microcontroller in an Arduino which is designed for embedded real-time operations.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ckraft
    0 ckraft over 13 years ago in reply to colecago

    He could also run the whole thing off the Parallax Propeller which is what Ben's first pinball machine did.

     

    To the point about the Raspberry Pi, its a neat device but it is not a microcontroller and cannot act as a microcontroller. There's a specific difference between the devices like that used in the Raspberry pi, which is basically a moble processor, and the microcontroller in an Arduino which is designed for embedded real-time operations.