element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Noob questions about 3D printer build
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 29 subscribers
  • Views 339 views
  • Users 0 members are here
  • build
  • episode
  • idea
  • ben_heck
Related

Noob questions about 3D printer build

e14 Contributor
e14 Contributor over 13 years ago

Ben, I just discovered your show on YouTube [Build a 3D Printer...] revisited.

 

I have a few questions about your build-

 

1. Power supply- is it a rechargeable battery or direct plug in?

2. The SD Card- could this be modified to accept multiple format removable storage? (USB, micro SD, etc)

3. What case materials could/should be used and pros/cons?

4. Could a rooted andriod device be used for a control panel, or is there some other touch screen option?

5. Have you addressed any aesthetics for this build?

6. What about a filament feeder- perhaps a swing out arm to hold the spool?

7. Is there any way to "automate" the Y axis tray movement for closure?

 

Thanks and great builds!

  • Sign in to reply
  • Cancel
Parents
  • colecago
    0 colecago over 13 years ago

    1 - I believe its a computer power supply so direct plug in, no battery

    2 - Micro probably with an adapter, USB no, the SD card capability was built into the printer firmware and I don't think any of them support USB flash drives

    3 - 

    4 - Yes, people are doing things like this, you'd might need to modify the code a little (for the different serial port) but an android phone can send serial commands over bluetooth and depending on your control board maybe you can toss a bluetooth module on there

    5 -

    6 -

    7 - Yes you could either mod the firmware to add a button to do a specific movement, or you can call up a gcode "pack" file from the SD card to have it return to a packable position

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • colecago
    0 colecago over 13 years ago

    1 - I believe its a computer power supply so direct plug in, no battery

    2 - Micro probably with an adapter, USB no, the SD card capability was built into the printer firmware and I don't think any of them support USB flash drives

    3 - 

    4 - Yes, people are doing things like this, you'd might need to modify the code a little (for the different serial port) but an android phone can send serial commands over bluetooth and depending on your control board maybe you can toss a bluetooth module on there

    5 -

    6 -

    7 - Yes you could either mod the firmware to add a button to do a specific movement, or you can call up a gcode "pack" file from the SD card to have it return to a packable position