element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Help with Powering a Project
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 2 answers
  • Subscribers 31 subscribers
  • Views 599 views
  • Users 0 members are here
Related

Help with Powering a Project

e14 Contributor
e14 Contributor over 12 years ago

im working on a project that im using an Arduino Uno R3 and a SSC-32 servo controler thats powering 28 HXT900 servos

 

The Arduino is 12V 1A and the SSC-32 is 9V 500mA

 

i have an enercell 18/24V 1A AC power adapter that i have laying around. i was wondering is it possible to us that adapter to power both device and how.

 

Lynxmotion - SSC-32 Servo Controller

  • Sign in to reply
  • Cancel
  • colecago
    0 colecago over 12 years ago

    The Arduino can do multiple voltages so you could use the same supply for both.  And I don't think the Arduino will need a full amp if its not powering many peripherals.  Also the servo controller might draw 500mA but 28 servos will not, you will need a beefier supply.

     

    http://homepages.paradise.net.nz/bhabbott/Servo.html

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • benheck
    0 benheck over 12 years ago in reply to colecago

    Jesse's right you can plug 12 volts into an Arduino (the barrel plug or VIN pin) and it will be fine.

     

    -Ben

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Thanks for your replys

     

    what im wondering is if i was to wire both devices to be powered by this adapter, do i need to worry about ether device being supplied to much power?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • colecago
    0 colecago over 12 years ago in reply to e14 Contributor

    You'd have to look in the datasheets for your devices, they both will specify a range.  If 18V is outside of that range, then don't use it.  You could always use a regulator to get the voltage down, but it's probably easier to just buy a different power adapter with a lower voltage.