element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum need pointed in the right direction, if my project is possible
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 24 replies
  • Subscribers 31 subscribers
  • Views 2710 views
  • Users 0 members are here
  • uno
  • electronics
  • ben_heck
  • arduino
  • solar
Related

need pointed in the right direction, if my project is possible

e14 Contributor
e14 Contributor over 12 years ago

I am newer to arduino, but i have some programming on it. I am a firefighter and want to create a light bar.

I am hoping that this project is possible for a near future completion date.

The project includes:

 

Arduino uno for pattern design and such. looking to use up to 16 3w LED from cree. its a small bar so nothing too much.

microelectronics to supplement the arduino for power as external power, step up if you will.

Bluetooth to turn lights on/off, hi voltage (3w for day use) low (1.5 for night use), change patterns.

solar panel (to create a self contained power (no wire running anywhere)

android app to control all the bluetooth

 

i could just buy a $400 lightbar but this would def be great if this is possible.

Please point me in the right direction on what to look at or such.

 

TIA

 

Matthew

  • Sign in to reply
  • Cancel
Parents
  • atharvabenheckfan
    0 atharvabenheckfan over 12 years ago

    try making this neater than i did

    sorry i could not vary the wattage of the leds

    if you already have an arduino

    just buy a new atmega328p,put in in your arduino program it

    remove an put it in your project wire it all up according to the datasheet on the arduino website.

    you will need to put a 16 mhz crystal and two 22pf caps to pins 9,10

    just to be on the cheap side

    use a vreg that can regulate from 50 volts not 35 or you'll fry it

     

    if you are satisfied please mark this as a correct answer

    man! that was tiering

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 12 years ago in reply to atharvabenheckfan

    If you are going to pay for 16 * 3W LEDs it makes sense to control the current. The forward voltage of the first high power LED I found some data for could range from 2.9 to 3.9V @ 350mA.

    3W LEDs will need more current and an even bigger range of forward voltage can be expected. It varies from part to part and with temperature.

    Some kind of feedback driven current control is needed to use high power LEDs safely and efficiently. A resistor can be used to limit the current but it wastes power.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 12 years ago in reply to atharvabenheckfan

    If you are going to pay for 16 * 3W LEDs it makes sense to control the current. The forward voltage of the first high power LED I found some data for could range from 2.9 to 3.9V @ 350mA.

    3W LEDs will need more current and an even bigger range of forward voltage can be expected. It varies from part to part and with temperature.

    Some kind of feedback driven current control is needed to use high power LEDs safely and efficiently. A resistor can be used to limit the current but it wastes power.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • atharvabenheckfan
    0 atharvabenheckfan over 12 years ago in reply to michaelkellett

    so what would you recomend sir