element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum need pointed in the right direction, if my project is possible
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 24 replies
  • Subscribers 31 subscribers
  • Views 2668 views
  • Users 0 members are here
  • uno
  • electronics
  • ben_heck
  • arduino
  • solar
Related

need pointed in the right direction, if my project is possible

e14 Contributor
e14 Contributor over 12 years ago

I am newer to arduino, but i have some programming on it. I am a firefighter and want to create a light bar.

I am hoping that this project is possible for a near future completion date.

The project includes:

 

Arduino uno for pattern design and such. looking to use up to 16 3w LED from cree. its a small bar so nothing too much.

microelectronics to supplement the arduino for power as external power, step up if you will.

Bluetooth to turn lights on/off, hi voltage (3w for day use) low (1.5 for night use), change patterns.

solar panel (to create a self contained power (no wire running anywhere)

android app to control all the bluetooth

 

i could just buy a $400 lightbar but this would def be great if this is possible.

Please point me in the right direction on what to look at or such.

 

TIA

 

Matthew

  • Sign in to reply
  • Cancel
Parents
  • dougw
    0 dougw over 12 years ago

    Hi Matthew,

    3W LEDs require about 900 mA each.

    If you want to control the LEDs individually, it will require 16 outputs from the arduino and each output will need to control a separate LED driver that can supply 900 mA. It is possible to use a single serial output instead, but then you need a module to convert the serial back to parallel.

    In order to supply 900 mA to an LED with reasonable efficiency, it is necessary to use a constant current switching regulator - so you will need 16 of these driver modules, unless you can find one with multiple outputs.

    The power supply for the driver modules will need to supply at least 50 W.

    So you will need an arduino, a Bluetooth module, 16 LEDs, 16 driver modules (capable of supplying 1A each), a battery capable of supplying 50 W or a big power supply and a 60 W solar panel.

    Doug

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dougw
    0 dougw over 12 years ago

    Hi Matthew,

    3W LEDs require about 900 mA each.

    If you want to control the LEDs individually, it will require 16 outputs from the arduino and each output will need to control a separate LED driver that can supply 900 mA. It is possible to use a single serial output instead, but then you need a module to convert the serial back to parallel.

    In order to supply 900 mA to an LED with reasonable efficiency, it is necessary to use a constant current switching regulator - so you will need 16 of these driver modules, unless you can find one with multiple outputs.

    The power supply for the driver modules will need to supply at least 50 W.

    So you will need an arduino, a Bluetooth module, 16 LEDs, 16 driver modules (capable of supplying 1A each), a battery capable of supplying 50 W or a big power supply and a 60 W solar panel.

    Doug