element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum need pointed in the right direction, if my project is possible
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 24 replies
  • Subscribers 31 subscribers
  • Views 2706 views
  • Users 0 members are here
  • uno
  • electronics
  • ben_heck
  • arduino
  • solar
Related

need pointed in the right direction, if my project is possible

e14 Contributor
e14 Contributor over 12 years ago

I am newer to arduino, but i have some programming on it. I am a firefighter and want to create a light bar.

I am hoping that this project is possible for a near future completion date.

The project includes:

 

Arduino uno for pattern design and such. looking to use up to 16 3w LED from cree. its a small bar so nothing too much.

microelectronics to supplement the arduino for power as external power, step up if you will.

Bluetooth to turn lights on/off, hi voltage (3w for day use) low (1.5 for night use), change patterns.

solar panel (to create a self contained power (no wire running anywhere)

android app to control all the bluetooth

 

i could just buy a $400 lightbar but this would def be great if this is possible.

Please point me in the right direction on what to look at or such.

 

TIA

 

Matthew

  • Sign in to reply
  • Cancel
Parents
  • atharvabenheckfan
    0 atharvabenheckfan over 12 years ago

    so matthew we will need less voltage thus increasing the chances of finding parts

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to atharvabenheckfan

    im still learning so in the pic you did, thats a series? or parallel? i cant remember but if im remembering i should be able to run 1A or so across both lights and make it work?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to atharvabenheckfan

    im still learning so in the pic you did, thats a series? or parallel? i cant remember but if im remembering i should be able to run 1A or so across both lights and make it work?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • dougw
    0 dougw over 12 years ago in reply to e14 Contributor

    Yes you can run the same current from one driver through 2 LEDs in series (one after the other) if there is sufficient voltage from your power supply. You may need 3 or 4 volts per LED - so a 12V power supply would be more than enough to run 2 LEDs in series.

    Yes you can use the arduino to send LED status back though Bluetooth to either a PC or mobile device.

    Doug

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • atharvabenheckfan
    0 atharvabenheckfan over 12 years ago in reply to e14 Contributor

    in the picture it was series

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • atharvabenheckfan
    0 atharvabenheckfan over 12 years ago in reply to e14 Contributor

    now if you want the real time status the code will be edited and the bt module rx line will also be connected to send the host the status of the leds