element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum TFT-LCD Reverse Engeneering Help
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 9 replies
  • Subscribers 31 subscribers
  • Views 1502 views
  • Users 0 members are here
  • composite
  • build
  • raspberry-pi
  • tft-lcd
  • ben_heck
Related

TFT-LCD Reverse Engeneering Help

toxxn
toxxn over 12 years ago

Hello everyone,

I am a young engineer looking for some help.

I am trying to reverse-engineer a Samsung 15.6in TFT-LCD (Model No.: LTN156AT09-H03), that a scavenged from an old laptop I had laying around. I downloaded a PDF of its specifications, which is very detailed, but I am still unsure on how to go about my project. What I want to do, is re-purpose the screen to use it as a screen for my Raspberry Pi, sort of a future MAME arcade project. From what I have gathered from the PDF, I think it has both the Driver and LCD Driver already. (I know it has the LED Driver at the very least.)

 

I provided some information below, (some of what the PDF tells me about it and the pin layout) and my question is, is everything already here that I need to use this right away? and if so, for a composite input, which pins do I need to use, and which pins do I need to use for the LED backlight? Any help would be very much appreciated. If there is anymore information I can provide from the PDF to help, I would be glad to retrieve it for you.

 

The PDF shows this:

LED Back Light with embedded LED Driver, DE (Data enable) only mode, 3.3V LVDS Interface, Onboard EEDID chip, and Green product (RoHS and BFR/PVC free compliance) under the features.

Under general information is also says that the driver element is "a-Si TFT active matrix".

 

Here is the pin layout:

(I was having trouble trying to copy and paste the pin layout because it was in a grid so it copied backwards.)


Input terminal pin assignment (LVDS, Connector : 20455-040E-0 by I-PEX or equivalent )

 

Pin# - Signal - Description

38~40  VBL+  LED Power Supply 6V~20V

37  NC  No Connection

36  BL_Enable  BL On/Off (On:2.0~3.3V, Off: 0~0.5V)

35  BLIM  PWM for luminance control (200~1KHz, 3.3V, 10~100%)
34  NC  No Connection

31~33  VBL-  LED Ground
29~30  NC  No Connection
28  GND  Ground
26~27  NC  No Connection
25  GND  Ground
23~24  NC  No Connection

22 GND Ground

20~21 NC No Connection

19  GND  Ground
18  ClkIN+  +LVDS differential clock input
17  ClkIN-  -LVDS differential clock input
16  GND  Ground
15  Rin2+  +LVDS differential data input (B2-B5, HS, VS, DE)
14  Rin2-  -LVDS differential data input (B2-B5, HS, VS, DE)
13  GND  Ground
12  Rin1+  +LVDS differential data input (G1-G5, B0-B1)
11  Rin1-  -LVDS differential data input (G1-G5, B0-B1)

10  GND  Ground
9  Rin0+  +LVDS differential data input (R0-R5, G0)
8  Rin0-  -LVDS differential data input (R0-R5, G0)
7  SDA  DDC Data
6  SCL  DDC Clock
5  NC  No Connection
4  DVDD  DDC 3.3V power
2~3  AVDD  Power Supply, 3.3V ( typical)
1  NC  No Connection

  • Sign in to reply
  • Cancel
Parents
  • Kilohercas
    0 Kilohercas over 12 years ago

    it will be very hard to make it work on your own, but it is possible. in your place i will leave that LCD alone.
    You must understand how to work with High end processors to be able to show something, if you have a question how to do that, you will not be able to do anything, trust me.

    just to give you perspective, LCD is 1366 x 768 and looks like 18b color depth. at 60FPS that is 1.055Gbps of data, can you handle that ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Kilohercas
    0 Kilohercas over 12 years ago

    it will be very hard to make it work on your own, but it is possible. in your place i will leave that LCD alone.
    You must understand how to work with High end processors to be able to show something, if you have a question how to do that, you will not be able to do anything, trust me.

    just to give you perspective, LCD is 1366 x 768 and looks like 18b color depth. at 60FPS that is 1.055Gbps of data, can you handle that ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • toxxn
    0 toxxn over 12 years ago in reply to Kilohercas

    I just simply wanted to know if this particular TFT-LCD I have is currently set up to be able to add a composite input (or even a HDMI input) without having to purchase a driver board, and if so, what pins I needed to use in order to do that.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Kilohercas
    0 Kilohercas over 12 years ago in reply to toxxn

    it looks like LCD use I2C, so you need to set correct registers. In my opinion, if you get correct ic to convert composite to RGB, that does not mean you will be able to display images via composit input. Look at 6-7 pins

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • toxxn
    0 toxxn over 12 years ago in reply to Kilohercas

    I was just looking at the DDC pins, and was worried about that.

    My goal was to be able to convert this using whats already there without having to purchase anything extra, if that's not possible, then I would gladly set this LCD aside and look for a new one.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Kilohercas
    0 Kilohercas over 12 years ago in reply to toxxn

    i use panel like this for SMD parts, eeproms, large 1210 capacitors and so on. look up ebay, they sell lcd with driver boards.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • toxxn
    0 toxxn over 12 years ago in reply to Kilohercas

    Ill be sure to look around. Thanks for the info.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Kilohercas
    0 Kilohercas over 12 years ago in reply to toxxn

    in the other hand, it looks like where is drivers, but i don' know will it work.
    but at cost low like that you can try it out, just make shure you have same pinout.
    MT6820 B Universal LVDS LCD Monitor Driver Controller Board 5V 17" 42" | eBay
    But question with I2C remains, i don't know why this panel need i2c. some times it is used one time by manufacture for production variations compensation, so you choose .

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • toxxn
    0 toxxn over 12 years ago in reply to Kilohercas

    I appreciate the try, but my LCD uses a 40 pin connection.

    Kind of sucks, because that would have been perfect.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • colecago
    0 colecago over 12 years ago in reply to toxxn

    So?  Its the signals you should be comparing, if it has the signals you need, just hook those up using a custom cable.  It looks like pins 31-40 are for backlight anyways, which would be a different board (CCFL inverter board).

     

    Reverse engineering isn't finding a drop in replacement board, its making it work by any means necessary, and hacking a cable is trivial.