element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Sensor to detect Human Presence
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 31 replies
  • Answers 8 answers
  • Subscribers 41 subscribers
  • Views 6925 views
  • Users 0 members are here
  • human
  • detection
  • internet_of_things
  • arduino
  • sensor
Related

Sensor to detect Human Presence

gunaseelan
gunaseelan over 12 years ago

Hello BEN,

 

                    Is there any sensor to detect human presence . Am aware of PIR (Passive Infra Red) sensor , which would human motion but not the human presence . Another way is by using image processing technique. Kindly suggest me a better solution image .

 

Thanks.

  • Sign in to reply
  • Cancel

Top Replies

  • abdulwaheed
    abdulwaheed over 9 years ago +3 suggested
    Try Microwave Doppler sensor HB100 pefect solution... http://www.limpkin.fr/public/HB100/HB100_Microwave_Sensor_Application_Note.pdf
  • dougw
    dougw over 9 years ago in reply to vvvvipul +3 suggested
    There are 4 main technologies that can meet these requirements - ultrasonic, video, radar, and lidar. You can find many commercial systems based on these technologies, including wireless versions. Search…
  • Workshopshed
    Workshopshed over 8 years ago +3 suggested
    The trains in London are trialing a system that tells you how full each carriage is by weighing is.
Parents
  • dougw
    0 dougw over 12 years ago

    There are numerous ways to detect people, and they all have benefits and drawbacks. If you explain more about the scenario where you need to detect a person, it would help narrow down the choices. For example capacitance could be used at very low cost, but it has a limited range and could detect other things if they are present. However, if the location is known within a couple of feet and it can only be occupied by a single human at a time, capacitance might work well.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • vvvvipul
    0 vvvvipul over 9 years ago in reply to dougw

    Dear Douglas / others

     

    I am also looking for a sensor to detect both - presence of a person or a vehicle behind a mining equipment like a dump truck or say a wheel loader. The sensor should detect say upto 8 mtrs behind the truck and should cover the entire width of the dump truck which means a horizontal angle of 120 degrees. The operating frequency has to be in free band of 2.4Ghz or 5.85 Ghz. The person or vehicle could be either moving or stationary. There are very few companies which produce such sensors which have to be IP 67 and with good vibration resistance. Does anyone know any source for such product / solutions?....vipul from india

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • vvvvipul
    0 vvvvipul over 9 years ago in reply to dougw

    Dear Douglas / others

     

    I am also looking for a sensor to detect both - presence of a person or a vehicle behind a mining equipment like a dump truck or say a wheel loader. The sensor should detect say upto 8 mtrs behind the truck and should cover the entire width of the dump truck which means a horizontal angle of 120 degrees. The operating frequency has to be in free band of 2.4Ghz or 5.85 Ghz. The person or vehicle could be either moving or stationary. There are very few companies which produce such sensors which have to be IP 67 and with good vibration resistance. Does anyone know any source for such product / solutions?....vipul from india

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • dougw
    0 dougw over 9 years ago in reply to vvvvipul

    There are 4 main technologies that can meet these requirements - ultrasonic, video, radar, and lidar. You can find many commercial systems based on these technologies, including wireless versions. Search for terms like rear object detection system or parking assist system or vehicle backup system. Most of these systems are designed for vehicle applications and are suitably rugged. If you want to protect them more, simply mount them in waterproof shock-mounts. All of them probably need periodic cleaning if they are expected to work in muddy environments.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • vvvvipul
    0 vvvvipul over 9 years ago in reply to dougw

    Many thanks. I did find few manufacturers like eaton , rostro vision eagle eye etc... will get in touch with them, though not sure about their operating frequency.  I would be grateful if you can suggest one or two suppliers similar to preco from mining application point of view.

    The frequency should be 2.4 or 5.85 Ghz. Detection distance to be minimum 5 mtrs, preferably 10 mtrs.