element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Sensor to detect Human Presence
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 31 replies
  • Answers 8 answers
  • Subscribers 41 subscribers
  • Views 6850 views
  • Users 0 members are here
  • human
  • detection
  • internet_of_things
  • arduino
  • sensor
Related

Sensor to detect Human Presence

gunaseelan
gunaseelan over 12 years ago

Hello BEN,

 

                    Is there any sensor to detect human presence . Am aware of PIR (Passive Infra Red) sensor , which would human motion but not the human presence . Another way is by using image processing technique. Kindly suggest me a better solution image .

 

Thanks.

  • Sign in to reply
  • Cancel

Top Replies

  • abdulwaheed
    abdulwaheed over 9 years ago +3 suggested
    Try Microwave Doppler sensor HB100 pefect solution... http://www.limpkin.fr/public/HB100/HB100_Microwave_Sensor_Application_Note.pdf
  • dougw
    dougw over 9 years ago in reply to vvvvipul +3 suggested
    There are 4 main technologies that can meet these requirements - ultrasonic, video, radar, and lidar. You can find many commercial systems based on these technologies, including wireless versions. Search…
  • Workshopshed
    Workshopshed over 8 years ago +3 suggested
    The trains in London are trialing a system that tells you how full each carriage is by weighing is.
  • vsluiter
    0 vsluiter over 12 years ago

    You're double posting here: Using Omron Thermal Sensor and here: Using Omron Thermal Sensor, which is confusing. I've commented on those threads to redirect people here

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • hawkeyethehacker
    0 hawkeyethehacker over 12 years ago in reply to vsluiter

    There is actually a lot of doubleposts on this same topic. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • vsluiter
    0 vsluiter over 12 years ago

    This component seems to do what you need: Infrared Array Sensor: Grid-EYE | Panasonic

    Not available from element14 or Newark, but Digikey can provide them : AMG8832 Panasonic Electronic Components | 255-3506-1-ND | DigiKey

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    The solution depend on the enviromental conditions. Are there ony humans which can be detected or are there animals too? How big is the area to supervise? what kind of warm object can be in the area?

     

    Detecting the presens of a person in a car for example is different fom the same question for a room with oly one door or a field.

    In a Car a thermal system is not the best selection, because it would recognize the swtched on seat heater too or the sun heated the seat. (or the dog lies on the seat.)

    For a room with only a door is possible to supervise just the door, or use the named IR detection systems form Omron or Panasonic. 

    For a greater area an image processing system would be the bet choise.

     

    Just tell a litle bit more about your problem, then you get better answers.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Workshopshed
    0 Workshopshed over 10 years ago

    Also capacitive or inductive circuits are often used to detect human presence need an object. They are used for safety sensors on industrial machinery.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    I have near ptoblem , how can I detect human body under the rubble ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to e14 Contributor

    Heat sensor like infra red range assuming the person is alive still.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 10 years ago in reply to e14 Contributor

    Micropower Impulse Radar.

    It is lower power than a cell phone, but it can detect people through concrete and under rubble.

    http://www.internetsec.com/www/video/Werne_files/Werne.pdf

    It can also be low cost.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • abdulwaheed
    0 abdulwaheed over 9 years ago

    Try Microwave Doppler sensor HB100 pefect solution...

    http://www.limpkin.fr/public/HB100/HB100_Microwave_Sensor_Application_Note.pdf

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • vvvvipul
    0 vvvvipul over 9 years ago in reply to dougw

    Dear Douglas / others

     

    I am also looking for a sensor to detect both - presence of a person or a vehicle behind a mining equipment like a dump truck or say a wheel loader. The sensor should detect say upto 8 mtrs behind the truck and should cover the entire width of the dump truck which means a horizontal angle of 120 degrees. The operating frequency has to be in free band of 2.4Ghz or 5.85 Ghz. The person or vehicle could be either moving or stationary. There are very few companies which produce such sensors which have to be IP 67 and with good vibration resistance. Does anyone know any source for such product / solutions?....vipul from india

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<>