element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Fm Arduino Alarm Clock
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 29 subscribers
  • Views 532 views
  • Users 0 members are here
  • clock
  • fm
  • temperature
  • radio
  • alarm
  • arduino
  • sensor
Related

Fm Arduino Alarm Clock

e14 Contributor
e14 Contributor over 12 years ago

Hello, i am new to arduinos and i have this project in mind and i am wondering if it can be done. I want to make a Fm Arduino Alarm Clock. I want to to be able to play the radio too as well as being used as an alarm clock/clock but i also want it to give me the temperature. Can this be done?  I know i would have to build an audio amp for the radio. Thanks Joe

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I dont see why it could not be done. A few buttons, an LCD, add in an RTC, and a DT22. You would have to build a radio circuit but an FM radio receiver is relatively simple. Should be doable with an Arduino Pro Mini.

     

    Heck most FM receiver circuits I have seen are tuned with a potentiometer, you could replace that with a MCP41100 digital potentiometer and control the station directly from the Arduino.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I dont see why it could not be done. A few buttons, an LCD, add in an RTC, and a DT22. You would have to build a radio circuit but an FM radio receiver is relatively simple. Should be doable with an Arduino Pro Mini.

     

    Heck most FM receiver circuits I have seen are tuned with a potentiometer, you could replace that with a MCP41100 digital potentiometer and control the station directly from the Arduino.