element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Quick Question: IF vs Flyback Transformer
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 5 replies
  • Answers 1 answer
  • Subscribers 32 subscribers
  • Views 972 views
  • Users 0 members are here
  • help
  • instructables
  • flyback
  • intermediate
  • transformer
  • shocker
  • schematic
  • frequency
  • question
Related

Quick Question: IF vs Flyback Transformer

RovertScott
RovertScott over 11 years ago

I'm currently trying to build a novelty shocker from instructables,  but I don't have the 5 pin Flyback transformer.

I have a 5 pin IF Transformer from an old radio, can that be used instead?

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 11 years ago +1 suggested
    Hi Rovert, No the IF transformer will not have the proper primary to secondary turns ratio to make the circuit work. When I was a young delinquent I used to hollow out books and put a small buzzer in series…
Parents
  • jw0752
    0 jw0752 over 11 years ago

    Hi Rovert, No the IF transformer will not have the proper primary to secondary turns ratio to make the circuit work. When I was a young delinquent I used to hollow out books and put a small buzzer in series with some batteries and the secondary of a 6.3 volt transformer. The primary would then have about 100 volts AC accentuated with a lot of spikes that were quite a bit higher. I would make a fancy cover for the book laced with tin foil and insulated top to bottom. On a small insulated portion of the cover I had a door bell button that I could push while fully insulated from the rest of the book cover. At one point I stood up in Math class and told our new, fresh out of the university, math teacher that on behalf of myself and the rest of the students I had a gift for him. I held out the book and as soon as he had a grip on it I pushed the button and lit him up. It was hilarious, but he was a really big guy and I had to run like heck to stay ahead of him so he could come to his senses and not hit me. Ah the good old days.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • RovertScott
    0 RovertScott over 11 years ago in reply to jw0752

    Thank you very much, but can I adapt this circuit to use a 4pin transformer? I have two from an emergency dc powered flourecent light. Here's what I have and the actual circuit below.

     

    image

    F3M6UXFFUI0T9WM.MEDIUM.jpg

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • RovertScott
    0 RovertScott over 11 years ago in reply to jw0752

    Thank you very much, but can I adapt this circuit to use a 4pin transformer? I have two from an emergency dc powered flourecent light. Here's what I have and the actual circuit below.

     

    image

    F3M6UXFFUI0T9WM.MEDIUM.jpg

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • jw0752
    0 jw0752 over 11 years ago in reply to RovertScott

    Hi Rovert,  Your hand drawn circuit holds the key to why only a flyback will probably work with this design. Notice on the side of the transformer with three connections the center connection is not really in the center. The short coil is an important aspect of the design and isn't typical on most transformers. Don't get me wrong, there are many ways to do just about anything with electronics and there are probably ways to incorporate different type transformers to get a similiar effect but without better component information on your salvage transformers you are much better off spending your money to get the correct component as opposed to the amount of work to redesign the circuit. The other issue in this redesign is if the original circuit is changed and the shock your circuit creates hurts someone you and whoever helps you modify the design will both be sued. If you stay true to the original design then it will be just you and the instructables designer. Hope this helps.

     

    !!! Just a note of caution, Electrical shocks, even minor ones, can be dangerous to some people.