element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Hot glue high or low temp
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 8 replies
  • Subscribers 31 subscribers
  • Views 6570 views
  • Users 0 members are here
Related

Hot glue high or low temp

e14 Contributor
e14 Contributor over 11 years ago

I'm just wondering on the show whether Ben uses a high or low temp hot glue gun?  Does it matter when gluing to things like PCB's?  Wondering if it can possibly get hot enough to melt solder or plastic if using high temp.

  • Sign in to reply
  • Cancel

Top Replies

  • mvnieuw
    mvnieuw over 11 years ago in reply to e14 Contributor +1 verified
    I did indeed misread your question, thanks for the clarification. When working with PCB's my experience is that the low temperature gun is good enough to do the job. It also depends on the gluesticks you…
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to mvnieuw +1
    Thank you for your help.
  • kidiccurus
    kidiccurus over 11 years ago in reply to e14 Contributor +1
    I personally use a dual temperature glue gun. According to the manual, a low temperature is better for fabric, card and other similar materials whereas high is better for wood, plastic and the like. I…
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Usually the glue stick has a certain temperature that it needs in-order to melt down. So if you are not using two different types of glue sticks there will be no point in, my opinion to have two different temperature levels. But we usually use different temperature levels in soldering because there are different solder with different percentage of lead ( and silver for lead free solder) that melts in different temperatures.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Usually the glue stick has a certain temperature that it needs in-order to melt down. So if you are not using two different types of glue sticks there will be no point in, my opinion to have two different temperature levels. But we usually use different temperature levels in soldering because there are different solder with different percentage of lead ( and silver for lead free solder) that melts in different temperatures.