element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Hot glue high or low temp
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 8 replies
  • Subscribers 31 subscribers
  • Views 6567 views
  • Users 0 members are here
Related

Hot glue high or low temp

e14 Contributor
e14 Contributor over 11 years ago

I'm just wondering on the show whether Ben uses a high or low temp hot glue gun?  Does it matter when gluing to things like PCB's?  Wondering if it can possibly get hot enough to melt solder or plastic if using high temp.

  • Sign in to reply
  • Cancel

Top Replies

  • mvnieuw
    mvnieuw over 11 years ago in reply to e14 Contributor +1 verified
    I did indeed misread your question, thanks for the clarification. When working with PCB's my experience is that the low temperature gun is good enough to do the job. It also depends on the gluesticks you…
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to mvnieuw +1
    Thank you for your help.
  • kidiccurus
    kidiccurus over 11 years ago in reply to e14 Contributor +1
    I personally use a dual temperature glue gun. According to the manual, a low temperature is better for fabric, card and other similar materials whereas high is better for wood, plastic and the like. I…
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Usually the glue stick has a certain temperature that it needs in-order to melt down. So if you are not using two different types of glue sticks there will be no point in, my opinion to have two different temperature levels. But we usually use different temperature levels in soldering because there are different solder with different percentage of lead ( and silver for lead free solder) that melts in different temperatures.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    And further if it is hot enough it can melt solder or plastic too. But since the heating element in the gun is manufactured to emit a lower heat it won't be practical to generate more heat without changing the element. Glue guns have a lower wattage than soldering irons usually.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mvnieuw
    0 mvnieuw over 11 years ago

    If you try to get the heating element to a higher temperature, the plastic of the gluegun itselves will melt and will probably break down. When you are interested in melting plastics, you should consider using an extruder from any 3D printer.

    I have never seen an extruder for solder. Things like resin and/or flux needs to be added to have the solder flow correctly and I think you dont want to go that way.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to mvnieuw

    Thank you for atempting to answer my question, however it seems my question was severely misread.

     

    At least where I come from, glue guns come in two different configurations, Hi temp and low temp. My question was does anyone know what Ben uses on the show, hi or low temp?  And does it really matter, specifically when trying to glue things to PCB's?  Would the glue itself possibly be hot enough to screw up existing solder on the PCB, or possibly melt the PCB itself, when using a HI temp glue gun?  Or must a Lo temp be used for gluing to PCB's.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mvnieuw
    0 mvnieuw over 11 years ago in reply to e14 Contributor

    I did indeed misread your question, thanks for the clarification.

     

    When working with PCB's my experience is that the low temperature gun is good enough to do the job. It also depends on the gluesticks you want to use. The low temp sticks are very cheap and work easy. Also with the low temp stick, when you burn yourself, it will hurt a lot less than the high temp guns. The high temp glue gives 3rd degree burns.

     

    When you look at a PCB, it is resisting very high temperatures, 350 degrees did not burn my pcb at all, it might get a little discolored, but the board was not really affected. At these high temperatures it is possible that small traces come loose from the pcb.

     

    When you look at solder, the temperature for 60/40 solder is 190 degree, 63/37 will melt around 180 degree. Leadfree solder has a higher temperature, but is dependent on the metal mixture. For the solder to become liquid, it will need to take +20 degrees above this temperature to really mess up your work. Also when just placing a small amount of glue, it will not have enough capacity to make a differenct.

     

    Al temperatures are in Celcius.

     

    Marco.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to mvnieuw

    Thank you for your help.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kidiccurus
    0 kidiccurus over 11 years ago in reply to e14 Contributor

    I personally use a dual temperature glue gun. According to the manual, a low temperature is better for fabric, card and other similar materials whereas high is better for wood, plastic and the like. I use the high setting on PCBs all the time with no issues so far.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to kidiccurus

    low temp ok