element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Hi Ben, long time watcher of the TBHS. Love it & you. Need Help with Raspberry pi 2 & LCD please!
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 25 replies
  • Answers 5 answers
  • Subscribers 30 subscribers
  • Views 2650 views
  • Users 0 members are here
  • raspberry
  • waveshare
  • lcd
  • spotpear
  • pi
  • 2
  • tft
  • 3.5"
Related

Hi Ben, long time watcher of the TBHS. Love it & you. Need Help with Raspberry pi 2 & LCD please!

e14 Contributor
e14 Contributor over 11 years ago

Super new to the raspberry pi scene been watching you do various projects with them and figured it would be something new and cool to check out. got my noobs installed perfect now running raspbian.

been moving along following different tutorials trying out new things.

 

I finaly got stuff working on my Raspbian good and I'm starting to get a little more comfortable doing stuff on my Pi like, 1.) Installed apache and MySQL got wordpress working. (been tinkering around with it a little) also got a working copy of minecraft server vrs.1.8.4 working on my Pi.

 

Recently wanted to make it a bit more portable.

So I bought the 3.5" TFT LCD from Waveshare spotpear.

thought it was a no brainer plug N play with the Gpio

I pretty sure it is. but I cant seem to get or find proper soft ware, & or documentation to easily install it. there was no software when I got my lcd. it told me to go to few sites which were for the older pi.

I've read through few pages of peoples post seems a lot of new and regulars on the  Pi scene are having similar problems with lcd installations.

Currently My pi is running on hdmi to tv.

 

Best Related web page related info I could find so far Is http://www.wvshare.com/product/3.5inch-RPi-LCD-A.htm

 

image

image

 

Please say you can help figure this out.

 

Also, if anyone else who reads this if you also have a raspi2 w/ the 3.5" tft lcd Waveshare Spotpear addon card let us know if you got it working right and if so let  us know what you did or didn't do, please also provide software as I have been unable to find it.

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 11 years ago +1 suggested
    I have that same screen, ordered from china off e-mail for around $20. Ill start by saying that you get what you pay for. It is not as easy to install but it works great! These instructions should get…
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    I have that same screen, ordered from china off e-mail for around $20.

     

    Ill start by saying that you get what you pay for. It is not as easy to install but it works great!

     

    These instructions should get it up and running on the Pi.

     

    However, getting it to rotate was a pain and I ended up using bits and pieces of the Adafruit instructions as well.

     

    You have to do quite a bit of mucking with the /boot/config.txt to include the fbtft device entries and some work on the X11Config to get it all rotated and the touch working correctly.

     

    Hope it helps, If not drop me a line and Ill help you get it working.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    well tried your options, think I'm just not doing something right. As I'm still only getting a white screen. nothing else.

    is it possible for you to zip a fresh image with it all installed. and I can install that image on to my 16gb micro sd class 10 card.

    and see if it at least gets the screen to work?

     

     

    ====================================================================================================

    Found someone with same screen (they had a image) but they have old Raspberry pi. Do not know if that matters or not in this case.

    I had spare micro SD card so I applied the image to it. and it booted right up. not sure how but everything sort of works. But as this is I wont be able to use my own image or fresh copy of raspbian, or Ubuntu if I wanted to. I would not know how to make that work.

     

    So if I want to use this 3.5" lcd it looks like I'm stuck using this guys image. image

    But image  happy image to find out that the LCD does work so does the tft part. the windows in the desktop environment are really hard to navigate due to resolution not sure how to make the windows

    fit the 320 x 480 resolution.

    Also another bummer with this image is I can not use the HDMI port anymore. image

    not sure how to make both work at same time or if they can even do that.

     

    Tried to attach the image so you guys could check it out. but the size is over a 1gb even after I Rared it. image

     

    any ideas on any of these issues would be great. thanks for all the help so far.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    I got the same screen

    I followed instructions on http://futurice.com/blog/id-like-to-have-some-lcd-on-my-pi and it works !

    the trick is that

    1. it's called Waveshare Spotpear 3.5" RPi LCD (A)
    2. it is not officially supported yet, but with flexfb one can tweak parameters manually

     

    Hope it will work for you !

    Patrick

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    There is an old saying about giving a man a fish.

     

    Rather than giving you an image, how about I give you step by step instruction with explanations.

     

    Get the latest copy of the Raspbian and boot your pi up. The first time you boot it, there will be a menu to expand the image and do some other stuff. go ahead and set it up as you like. The change is that under Advanced Options you need to turn on "SPI    ENABLE/DISABLE AUTOMATIC LOADING“


    once you are back in and at a command line run the following command


    sudo REPO_URI=https://github.com/notro/rpi-firmware rpi-update


    This will download and update the firmware. Once this process is done it will tell you that you have to reboot. Do do that yet, lets get some other setup out of the way


    edit the /boot/cmdline.txt by doing a


    sudo nano /boot/cmdline.txt


    In this file is a single long line that is used during boot. Add the following to the end of it.


    fbtft_device.custom fbtft_device.name=flexfb fbtft_device.gpios=dc:24,reset:25 fbtft_device.bgr=1 fbtft_device.speed=16000000


    This sets up the frame buffer to use the 3.5" screen and tells it to load the device. If you want the 3.5" screen to be your only video device you can add

     

    fbcon=map:1 fbcon=font:VGA8x8

     

    To the end of the line as well. That sets it up so when booting it shows all the boot information on the screen in the correct resolution and font size.

     

    Now save the file and exit.

    Next we need to setup the kernel module. open it by running the command

     

    sudo nano /etc/modules

     

    Now add the following to the end of the file

     

    # WaveShare SpotPear 3.5" LCD

    fbtft_device debug=3 rotate=90 name=flexfb speed=16000000 gpios=reset:25,dc:24

    flexfb  width=320 height=480 regwidth=16 init=-1,0xb0,0x0,-1,0x11,-2,250,-1,0x3A,0x55,-1,0xC2,0x44,-1,0xC5,0x00,0x00,0x00,0x00,-1,0xE0,0x0F,0x1F,0x1C,0x0C,0x0F,0x08,0x48,0x98,0x37,0x0A,0x13,0x04,0x11,0x0D,0x00,-1,0xE1,0x0F,0x32,0x2E,0x0B,0x0D,0x05,0x47,0x75,0x37,0x06,0x10,0x03,0x24,0x20,0x00,-1,0xE2,0x0F,0x32,0x2E,0x0B,0x0D,0x05,0x47,0x75,0x37,0x06,0x10,0x03,0x24,0x20,0x00,-1,0x36,0xF8,-1,0x11,-1,0x29,-3

     

    # Touchscreen

    ads7846_device model=7846 cs=1 gpio_pendown=17 keep_vref_on=1 swap_xy=0 pressure_max=255 x_plate_ohms=60 x_min=200 x_max=3900 y_min=200 y_max=3900

     

    The above may be wrapped. The file that starts with flexfb should be one single line all the way to the -3 at the end.

    This configures the drives for both the display and the touch screen. Read through those lines carefully as you may need to change the "rotate" on the fbtft driver and you may need to change the "swap_xy=" on the touch screen to make it the way you want it. Personally, I loaded them as is and then went back to adjust later.

     

    Now save that file and open the /boot/config.txt file for editing with the command

     

    sudo nano /boot/config.txt

     

    Add the following line to the bottom of the file

     

    dtoverlay=piscreen,speed=16000000,rotate=90

     

    save and exit the editor. This activates the touchscreen with the same rotation as the fbtft driver.

     

    Go ahead and reboot the unit. when it comes up the screen should go from white to black.

     

    No log back in and we can set up the XWindows system to work with the display.

     

    You need to edit the /usr/share/X11/xorg.conf.d/99-fbturbo.conf This is the config for the frame Buffer driver in X11.

     

    sudo nano /usr/share/X11/xorg.conf.d/99-fbturbo.conf

     

    look for the line that reads

     

    Option     "fbdev"  "/dev/fb0"

     

    That is what tells it to use the HDMI port. So change that to

     

    Option     "fbdev" "/dev/fb1"

     

    /dev/fb1 is the 3.5" screen. You can now save that file.

     

    The last step is to set the touch screen up. Edit the /usr/share/X11/xorg.conf.d/10-evdev.config file with

     

    sudo nano /usr/share/X11/xorg.conf.d/10-evdev.config

     

    The last entry should read

     

    Section "InputClass"

            Identifier "evdev touchscreen catchall"

            MatchIsTouchscreen "on"

            MatchDevicePath "/dev/input/event*"

            Driver "evdev"

    EndSection

     

    You want to add a line just before Driver that reads

     

    Option      "GrabDevice" "True"

     

    Other useful options include

     

    Option     "InvertY" "True"

    Option     "InvertX" "True"

    Option     "SwapAxes" "True"

     

    Inverts the direction of X/Y or swaps the Axes, which is used if you move your finger up and the courser goes left or right.

     

     

     

    Save that file and you should be ready to startx

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Finally got a moment to work on this..

    so I am following your instructions..

    at the fbcon=map:1 fbcon=font:VGA8x8 section

    I left this out as I want to be able to use either 3.5" or the hdmi

    if possible I would like it to work on both simultaneously.

    or be able to detect when I have hdmi plugged in.

     

    ok so made it further down before I ran into a problem..

     

    the sudo nano /usr/shar/X11/xorg.conf.d/99-fbturbo.conf does not seem to exist & wont let me save to create one.

     

    I have stopped at this point do to the fact this appears to be important.

    I do have a black screen now when loading btw.

     

    I checked some of your directories and found the problems.

     

    you left the (e) out in /usr/share/ part that solved that problem

    Ive finished it but cant seem to get the screen to flip or rotate in the upper direction.

    its upside down for me. I tried changing rotate but it would reboot with partial screen working

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Ok, when I run into an issue like that I start by cd'ing to each directory in the list and making sure they are all spelled correct. image

     

    it's "share" not "shar" If what you entered above is a copy of your line then you forgot an e.


    Correction, I left out an e. lol I correct my post above. Sorry about that.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    yeh, my main problem seems to be getting the screen to be right side up yours has mine with cords at the bottom  also the touch screen seems to be off some how.

    I've tried going back through and changing the rotate but only rotate=90 will give me any picture properly and its upside down for me.

     

    Ideas?

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    There are two rotate points. One in modules and one in the boot config.txt

     

    If I remember correctly they can be 0, 90, -90, or 180

     

    I spent a lot of time playing with both for mine the module had to be -90 and the config had to b 90 to get it rotated the correct direction.

     

    It seems that they would cancel each other out but it actually flips the screen the right direction for me.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    ok finaly got screen rotated as I wanted, got the touch going in the right x & y axis but the touch does not go to edge of desktop in any direction it is like a half a centimeter short of space in each direction. what do I play with to make it go to edge of screen?

     

    While I wait for a response I will try to get my IOgear GBU521 adapter running and try to figure out how to make a wireless Bluetooth speaker connect (something I have been unable to do) wish me luck on this.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Try running the touch screen calibration

     

    sudo TSLIB_FBDEVICE=/dev/fb1 TSLIB_TSDEVICE=/dev/input/touchscreen ts_calibrate



    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    sudo: ts_calibrate: command not found
    is what i do when i do your command. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    sudo: ts_calibrate: command not found
    is what i do when i do your command. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    falon wrote:

     

    sudo: ts_calibrate: command not found
    is what i do when i do your command.

    Did you install the command? You can do an aptitude or apt-get to search the repos and install it. I think it is part of libts-bin.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    ok so i installed the

     

      sudo apt-get install evtest tslib libts-bin

     

     

     

    then did update

    then rebooted

    and then did the

     

      sudo TSLIB_FBDEVICE=/dev/fb1 TSLIB_TSDEVICE=/dev/input/touchscreen ts_calibrate

     

    then got the famous

    sudo: ts_calibrate: command not found
    is what i do when i do your command.

     

    So i then googled how to install ts_calibrate,

    everything I have found so far points to the install of the libts-bin

     

    So I went to where it said /dev/input/touchscreen only to find I don't have a touchscreen directory.

    This is what i have in my /dev/input/ directory

     

    pi@rpi2-54 /dev/input $ ls
    by-id    event0  event2  event4  mice    mouse1
    by-path  event1  event3  event5  mouse0  mouse2

     

    At this point I'm stuck. so maybe you know what I should do next? or so I'm hoping.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    cyberlink,

     

    I cannot thank you enough! I was just about to give up hope before finding this thread and your instructions. After doing as you said my display is fully functional touchscreen and all! FYI for others, I have a SainSmart 3.5" TFT touchscreen and the instructions in this thread worked as is.

     

    falon - if you're somehow still searching for an answer to your calibration issue, try running ts_calibrate a few different times and each time try setting TSDEVICE as a different one of the "event" items in /dev/input. I had the same issue but once I tried event3 it worked like a charm.