element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum singing Tesla coil Mark 1
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 2 replies
  • Answers 1 answer
  • Subscribers 30 subscribers
  • Views 654 views
  • Users 0 members are here
  • question
Related

singing Tesla coil Mark 1

e14 Contributor
e14 Contributor over 11 years ago

Dose anyone think that using a car stereo amplifier as the power supplie for a Tesala coil

would work as to make it play music by using the output form a 120 watt car stereo amp

after putting a hefty diode on the out put to get rid of the flip flop effect on the output of the amp

 

Sorry for the schematic quality I drew it with out anything but a ruler but its just a basic idea

 

Relaxed☻Relaxed☻Relaxed☻Relaxed☻Relaxed

 

 

 

 

▄▀▀▄ ▄▄ ▄▀▀█▀▄ ▄▀▀▄ ▄▀▄ ▄▀▀▄ ▀▀▄ ▄▀▀▄ ▀▄ ▄▀▀█▄ ▄▀▀▄ ▄▀▄ ▄▀▀█▄▄▄▄ ▄▀▀█▀▄ ▄▀▀▀▀▄ ▄▀▀▀▀▄ ▄▀▀▀█▀▀▄ ▄▀▀█▄▄▄▄ ▄▀▀▄ ▄▀▀▄ ▄▀▀█▄▄▄▄ ▄▀▀▄ ▀▄

█ █ ▄▀ █ █ █ █ █ ▀ █ █ ▀▄ ▄▀ █ █ █ █ ▐ ▄▀ ▀▄ █ █ ▀ █ ▐ ▄▀ ▐ █ █ █ █ █ ▐ █ █ ▐ █ █ ▐ ▐ ▄▀ ▐ █ █ █ ▐ ▄▀ ▐ █ █ █ █

▐ █▄▄▄█ ▐ █ ▐ ▐ █ █ ▐ █ ▐ █ ▀█ █▄▄▄█ ▐ █ █ █▄▄▄▄▄ ▐ █ ▐ ▀▄ ▀▄ ▐ █ █▄▄▄▄▄ ▐ █ █ █▄▄▄▄▄ ▐ █ ▀█

  █ █ █ █ █ █ █ █ ▄▀ █ █ █ █ ▌ █ ▀▄ █ ▀▄ █ █ █ ▌ █ ▄▀ █ ▌ █ █ 

  ▄▀ ▄▀ ▄▀▀▀▀▀▄ ▄▀ ▄▀ ▄▀ ▄▀ █ █ ▄▀ ▄▀ ▄▀ ▄▀▄▄▄▄ ▄▀▀▀▀▀▄ █▀▀▀ █▀▀▀ ▄▀ ▄▀▄▄▄▄ ▀▄▀ ▄▀▄▄▄▄ ▄▀ █ 

█ █ █ █ █ █ █ █ ▐ ▐ ▐ █ █ █ ▐ █ █ ▐ ▐ █ █ ▐ █ ▐ █ ▐ 

▐ ▐ ▐ ▐ ▐ ▐ ▐ ▐ ▐ ▐ ▐ ▐ ▐ ▐ ▐ ▐ ▐

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 11 years ago

    Did you see http://www.element14.com/community/message/146983/l/re-tesla-coil-music-player#146983 from Mike Wiltrout? Sometimes the best answer is to experiment. But be careful with 120 volts! Never handle without voltage off and a complete understanding...

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to clem57

    Yes i did but it seemed to overly complex to use an interrupter board and also $$$EXPENSIVE$$$

    A 350W car stereo amp with two speaker out puts (only need 1) is about 50$ and that's OVER KILL

     

    But yes Because i have found no one else so far that has experimented with this theory i will just experiment

     

    Thank you for the help though

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to clem57

    Yes i did but it seemed to overly complex to use an interrupter board and also $$$EXPENSIVE$$$

    A 350W car stereo amp with two speaker out puts (only need 1) is about 50$ and that's OVER KILL

     

    But yes Because i have found no one else so far that has experimented with this theory i will just experiment

     

    Thank you for the help though