element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Vape mod from Gameboy Color
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 29 subscribers
  • Views 621 views
  • Users 0 members are here
Related

Vape mod from Gameboy Color

sevenbeloved
sevenbeloved over 11 years ago

Hello,

 

So I'm wanting to build my very own vape mod box and I'm still very new at circuitry so I was hoping to get some guidance on how I could build a circuit board setup that could utilize the gameboy colors directional pad, start/select, and a/b buttons to control the Vape. I figured the directional pad could be used to change voltage/wattage, a and/or b to "fire" the Vape and select/start to turn off and on the whole thing. I would also want to use the gameboy colors screen area to show the amount of voltage/wattage it's set to

and the led spot as feedback for firing. I realize this might be a little much for someone just starting out, but I figured I've got to start somewhere. Thanks in advance for any tips or advice.

  • Sign in to reply
  • Cancel
Parents
  • kidiccurus
    kidiccurus over 11 years ago

    Whilst I can't condone your decision to vape, I can give some help with hacking the gameboy. First of all, make sure you use a broken gameboy for this project, the internal circuitry is largely not needed for this project, and killing a functional unit would be a waste. You will also need to completely replace the screen as interfacing with the existing one would require a large amount of work. To use the buttons, locate the tracks going to the button contacts on the board, remove some soldermask and attatch wires to them. You may also need to cut some traces if the buttons share a common ground. Alternatively, you could try and mount some tact switches inside the unit. This would change the feel of the buttons, and they would need to be firmly mounted, but it is theoretically easier than the other option.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • kidiccurus
    kidiccurus over 11 years ago

    Whilst I can't condone your decision to vape, I can give some help with hacking the gameboy. First of all, make sure you use a broken gameboy for this project, the internal circuitry is largely not needed for this project, and killing a functional unit would be a waste. You will also need to completely replace the screen as interfacing with the existing one would require a large amount of work. To use the buttons, locate the tracks going to the button contacts on the board, remove some soldermask and attatch wires to them. You may also need to cut some traces if the buttons share a common ground. Alternatively, you could try and mount some tact switches inside the unit. This would change the feel of the buttons, and they would need to be firmly mounted, but it is theoretically easier than the other option.