element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum dc generator
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 32 subscribers
  • Views 1438 views
  • Users 0 members are here
Related

dc generator

majorkuso
majorkuso over 10 years ago

I want to use a dc motor to charge a cellphone, how would I choose an off the shelf dc motor to use as the generator? I am looking at something like this  https://www.amazon.com/2-5KG-Micro-Speed-Reducing-Motor/dp/B009AQLDSS/ref=pd_day0_469_2?ie=UTF8&psc=1&refRID=K49X1E2DXFR58MMTJ742. I am assuming if I can match the rpm it should be close to the running specs? I would like a similar current but higher voltage to step down to 5 volts, however I am think a buck/boost converter would be adequate?

  • Sign in to reply
  • Cancel

Top Replies

  • william_hoffer
    william_hoffer over 10 years ago +1
    don't know if this will help but this how ben did it way back in 2011 Episode 10: See Ben Build a Hand Crank Phone Charger
  • jw0752
    jw0752 over 10 years ago in reply to majorkuso +1
    Hi James, It is a matter of conservation of energy. You can not get more power out than is put into the system. In most cases like this one you will get a lot less out than is put in due to heat losses…
Parents
  • majorkuso
    majorkuso over 10 years ago

    the motor i have outputs 7 volts no load I bought an emergency charger uses two  AA batteries from dollar tree and it charges the phone from the Stirling engine however current is lacking , is there anyway i can convert the voltage t a higher current efficiently?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 10 years ago in reply to majorkuso

    Hi James,

    It is a matter of conservation of energy. You can not get more power out than is put into the system. In most cases like this one you will get a lot less out than is put in due to heat losses. If you multiply the voltage by the current (in Amps) you will have a number for the power in Watts. Any process that would increase the current will correspondingly lower the voltage. For example the power of 7 volts at 2 amps is equivalent to the power of 2 volts at 7 amps. In a system where you are wanting to charge a battery however it is necessary to have a voltage level that is above the voltage of the battery so that current can be made to flow back into the battery. The only way to get more current in your situation will be to put more power into the system by spinning your generator faster.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jw0752
    jw0752 over 10 years ago in reply to majorkuso

    Hi James,

    It is a matter of conservation of energy. You can not get more power out than is put into the system. In most cases like this one you will get a lot less out than is put in due to heat losses. If you multiply the voltage by the current (in Amps) you will have a number for the power in Watts. Any process that would increase the current will correspondingly lower the voltage. For example the power of 7 volts at 2 amps is equivalent to the power of 2 volts at 7 amps. In a system where you are wanting to charge a battery however it is necessary to have a voltage level that is above the voltage of the battery so that current can be made to flow back into the battery. The only way to get more current in your situation will be to put more power into the system by spinning your generator faster.

    John