element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Convert mobile DVD player to Pi Entertainment system
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 30 subscribers
  • Views 666 views
  • Users 0 members are here
  • questions_communityfeedback
Related

Convert mobile DVD player to Pi Entertainment system

threealarm
threealarm over 9 years ago

Ben,

 

I've got these portable dvd players that mount on the rear head rests in a vehicle.

I'm planning on removing the DVD guts, then replace with a R PIv3 with kodi installed.

Since this is to be designed with my kids in mind, I also plan to add in the necessary module for  wireless game controllers.

I was wondering if you would be interested in doing a build, I could send you one of the sets that I have.

  • Sign in to reply
  • Cancel

Top Replies

  • william_hoffer
    william_hoffer over 9 years ago +1
    First off I like te idea. I do have two questions, First off by your last sentance I am taken to understand you are talking about a system that has twin screen (one for the back of the driver seat and…
Parents
  • d3angc
    d3angc over 9 years ago

    I have built one. It works quite well. I would suggest that you use an in car DVD player with aux input and solder direct to this channel. Then wire the power input from the pi to the built in usb on the dvd player. It will all run from the built in battery and you can port out the pi usb to the bottom of the player so wired controllers can still be used.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • d3angc
    d3angc over 9 years ago

    I have built one. It works quite well. I would suggest that you use an in car DVD player with aux input and solder direct to this channel. Then wire the power input from the pi to the built in usb on the dvd player. It will all run from the built in battery and you can port out the pi usb to the bottom of the player so wired controllers can still be used.