element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum USB 1GB Flash memory with LCD
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 32 subscribers
  • Views 1762 views
  • Users 0 members are here
Related

USB 1GB Flash memory with LCD

softwareinthecloud
softwareinthecloud over 9 years ago

Dear Element14 Community,

 

I am trying to build a USB flash memory device with built-in LCD.

 

I need to show the files or a particular file on the LCD.

The LCD needs to be very small similar to these:

image

 

Do not need to have a battery, microphone and audio player capability.

 

Could you please let me know if this is possible?

 

I am planning to 3d print the case myself. I just need the pcb+memory & LCD to be around less than $2.

 

How can I get the memory LCD and PCB built? Should I get the components seperately?

 

Is there a board that I can buy off the shelf that can do these at the lowest possible cost?

 

Thank you.

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 9 years ago in reply to softwareinthecloud +2
    softwareinthecloud wrote: THank you Jordan. I can be a bit more flexible with the price but no more than $5. Please also note, i dont need most of the components that mp3 players use like buttons, battery…
  • jdlui
    jdlui over 9 years ago +1
    It technically possible - because MP3 players and similar tech exist that do the same thing. However your constraints are not realistic. I'm not an electronics expert, but wanting a custom PCB and display…
  • cmspooner
    cmspooner over 9 years ago +1
    What's the goal? Sometimes starting at the beginning lets other people give you idea that you haven't thought of. You can get Wemos or arduino pro-mini knock-offs from ebay pretty darn cheap (about $5…
Parents
  • jdlui
    jdlui over 9 years ago

    It technically possible - because MP3 players and similar tech exist that do the same thing.

     

    However your constraints are not realistic.

     

    I'm not an electronics expert, but wanting a custom PCB and display for less than $2 sounds downright impossible.

     

    The hardware costs alone in a device like the MP3 player you suggested are already more than $2, and this item is mass produced. Trying to do this yourself will cost way more, in time and money.

     

    If you're willing to expand your cost constraint, I'm sure something is possible.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • softwareinthecloud
    softwareinthecloud over 9 years ago in reply to jdlui

    THank you Jordan.

    I can be a bit more flexible with the price but no more than $5.

    Please also note, i dont need most of the components that mp3 players use like buttons, battery, audio components, headphone jack.

     

    What options and components would be the best for this do you think?

    Do you know if there is a similar project to this that I can use?

     

    Should I try ink displays instead of LCD? Would this decrease the price?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • softwareinthecloud
    softwareinthecloud over 9 years ago in reply to jdlui

    THank you Jordan.

    I can be a bit more flexible with the price but no more than $5.

    Please also note, i dont need most of the components that mp3 players use like buttons, battery, audio components, headphone jack.

     

    What options and components would be the best for this do you think?

    Do you know if there is a similar project to this that I can use?

     

    Should I try ink displays instead of LCD? Would this decrease the price?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 9 years ago in reply to softwareinthecloud

    softwareinthecloud wrote:

     

    THank you Jordan.

    I can be a bit more flexible with the price but no more than $5.

    Please also note, i dont need most of the components that mp3 players use like buttons, battery, audio components, headphone ....

    Wouldnt you need buttons to be able to highlight the file you wanted to display, and also a button to turn the display on/off so its not on and wasting power all of the time and generally a battery would be needed too unless you only want the display to work when the device is plugged in.

     

    Something you need to understand is that those cheap mp3 players are so cheap because of how many get made and the manufacturers are taking advantage of huge bulk discounts on the components and pcb manufacture. To make a one off, small order run or even a similar prototype would cost a whole lot more which is why people are giving you the realistic $50 type figures. Even if you plan to make millions of these, the prototype is still going to cost you a lot to produce.

     

    There are other pitfalls too for instance you say you need an lcd screen similar to that mp3 player, generally lcd manufacturers dont sell those in small quantities, you would likely need to purchase them in quantities of 1000+ (lcd's like those are also much of the time custom manufactured to the buyers specification hence the minimum order quantities).

     

    I really would just get to hacking existing devices, it would be much easier

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • softwareinthecloud
    softwareinthecloud over 9 years ago in reply to e14 Contributor

    Yes I would only need a button to turn on/off the LCD & maybe a battery.

    I am aware the prototype will cost more initially but I was looking to get the community's opinion as to how I can achieve to bring the costs down.

    Hacking existing devices is viable.

    Do you know any project that may be useful to me?