element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Commodore 64 Laptop
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 30 subscribers
  • Views 860 views
  • Users 0 members are here
  • commodore_64
  • commfeedback
Related

Commodore 64 Laptop

celcius1
celcius1 over 8 years ago

I’m a new user to TBHS, and have been watching his videos, i especially loved the vid’s on the Atari hand held console, and the Apple 1 build.

 

after watching these I felt inspired, and I have at home a couple of C64’s that still work but no PSU, or disk drive, but I do have a working dataset.

 

so i thought, could I use this hardware to rebuild it into a case with a 19” LCD screen and give me self a C64 I can carry round with me, a decent sized screen, as I have a 19” LCD screen in 4:3 format, but seeing as I have two C64’s I could also use parts from the other C64 to do some mod’s like the stereo SID chip mod, use an SD card for the disk drive.

 

So I welcome some suggestions from the community and Ben himself, about my project, inspired by some of ben’s creations.

 

Talk Soon

Celcius1

  • Sign in to reply
  • Cancel
Parents
  • zeropolis1979
    zeropolis1979 over 8 years ago

    In theory it's possible. The disc drive would be the main issue as they're huge, bulky and heavy (and I know as I've dismantled a few to repair)..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • celcius1
    celcius1 over 8 years ago in reply to zeropolis1979

    I’m planning to use an SD card to emulate the disc drive, as the disk drive is big and bulky, I saw an SD card disk drive emulator on the channel run by the 8 bit guy on you tube.

     

    plus I need to figure out how i’m Going to send the video to the LCD screen as it uses a vga input, and the commodore only has composite and RGBI available.

     

    talk soon

    paul

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • celcius1
    celcius1 over 8 years ago in reply to zeropolis1979

    I’m planning to use an SD card to emulate the disc drive, as the disk drive is big and bulky, I saw an SD card disk drive emulator on the channel run by the 8 bit guy on you tube.

     

    plus I need to figure out how i’m Going to send the video to the LCD screen as it uses a vga input, and the commodore only has composite and RGBI available.

     

    talk soon

    paul