Maker Film Festival
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Hack Like Heck
  • Maker Film Festival
  • More
  • Cancel
Maker Film Festival
Documents Hack Like Heck - ShockSlayer - Portable Wii: The WaveRider
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Maker Film Festival to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 2 Apr 2018 6:13 PM Date Created
  • Last Updated Last Updated: 8 Apr 2018 3:08 AM
  • Views 5651 views
  • Likes 20 likes
  • Comments 37 comments
Related
Recommended

Hack Like Heck - ShockSlayer - Portable Wii: The WaveRider

image

A Hack Like Heck Project Video

Vote for this Video by using the Like or Share buttons

Voting Instructions image

About Hack Like Heck
Content Partner Program
All Hack Like Heck Videos

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

The WaveRider is a fully featured Wii Portable, designed to be as comfortable to play as possible. With its never-before-seen software integration and no-expense-spared feature list, it's sure to turn a few heads this year at MGC. Follow ShockSlayer as he takes you on a journey through the advancement of the portablizing community, with the WaveRider as your final destination.

 

 

Parts:

 

  • 1x OMEGA trimmed Wii motherboard
    • Fully featured, including the MX chip, Wifi module, BlueTooth module, etc.
  • 3x 3.7v 2500mAh Li-ion battery cells
  • 1x 800x480 LCD w/HDMI driver board
  • 1x GCVideo-DVI digital signal to HDMI converter board
  • 1x Prototype BGA-style NAND relocation board
  • 1x Prototype "PowerMii" regulator board
  • 1x Prototype "WiiHUD" audio amplifier
    • Prototype boards have too many individual components to list
  • 1x Power button circuit (D flip-flop w/debouncer)
  • 2x Speakers
  • 1x USB port
  • 4x 3D printed case parts
    • Screen assembly, bezel, back plate, and front extended
  • 1x Hand-made battery cover
  • 1x WaveBird controller
    • Gutted for the case, controller board cutouts, and supporting buttons and trigger assemblies
  • 1x Replacement mini rumble motor
  • 2x GC+ Controller replacement board
    • One of which has custom firmware for controlling RGB LEDs via custom controller protocols
  • 2x RGB LEDs
  • 1x Lasered acrylic cutout for the front logo
  • 1x 5v Sunon blower fan
  • 1x Custom copper heatsink w/soldered copper cutouts
  • 20+ Male/Female Headers of varying amounts of pins
  • 1x 3.5mm headphone jack
  • 1x Charging jack
  • 7x Tact switches
  • 8x Triwing Screws
  • 1x Pig of unknown purpose
  • Plus an incalculable amount of various wire types, kapton tape, thermal paste, paint/gloss, solder, and of course hot glue.
  • hlh_mff
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • nobble
    nobble over 8 years ago +14
    THIS is the Ultimate Portable Wii!
  • shockslayer
    shockslayer over 8 years ago +5
    I've been told by a few people that they're unable to comment on this page; is that intentional? Thanks.
  • shockslayer
    shockslayer over 8 years ago in reply to makerkaren +3
    I've being using the same two rolls of 38 and 34 gauge wire for about 2 years now for lots of different commissions and projects, and I've never had an issue with wires being scratched and bridging/shorting…
  • airbornesurfer
    airbornesurfer over 8 years ago

    Congrats, ShockSlayer! Great build!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • tbuddy
    tbuddy over 8 years ago

    Sicc, but not thicc

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mythiegcc
    mythiegcc over 8 years ago

    really well done, loved the video.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • tariq.ahmad
    tariq.ahmad over 8 years ago

    Very cool build!

     

    Enjoyed hearing about the background and everything that went into it as that heightened my appreciation of the what the final build looked like.

     

    The GameCube controller was a great call and congratulations on a build that is not only aesthetically pleasing but well engineered!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • nobble
    nobble over 8 years ago in reply to mayermakes

    I have had success with such wire so far. It does take a bit to scrape the enamel away. And if you glue your wires down it keeps them from getting moved and issues arising. They work great for tight spaces.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • airbornesurfer
    airbornesurfer over 8 years ago

    Definitely an inspired project. Great build!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shockslayer
    shockslayer over 8 years ago in reply to makerkaren

    I've being using the same two rolls of 38 and 34 gauge wire for about 2 years now for lots of different commissions and projects, and I've never had an issue with wires being scratched and bridging/shorting during handling. This including handling with various metal tweezers, which is how I do most of my soldering work. I would imagine that if you buy cheaper wire, it's more likely to happen.

     

    In the portable, since everything is run to mounted headers, there's very little chance of problems occurring since the wires aren't run long enough to wiggle around. The two halves of the portable plug together in line with the case. If you'd like, I can show you at MGC!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 8 years ago in reply to makerkaren

    Hi Karen,

    It's a good question, I guess in most cases the stranded version of 30AWG may be usable, (it is about 0.5-0.6mm thick with the insulation depending on the version, e.g. this Alphawire ThermoThin wireAlphawire ThermoThin wire is 0.56mm thick) but might not suit extremely cramped projects. Enamelled wire is fine I think, since it is a one-off project, just makes maintainability a bit awkward, and knowing if there are shorts or not is harder. The 'SH' and similar connectors are quite small, e.g. for 8 circuits, the Molex Picoblade is 1.5mm pitch, and the mated connectors together would take up 15x9x3.2mm space overall, i.e. smaller footprint than using 0.1" SIL header pins for connections, but just a bit thicker (maybe just under 1mm thicker). Another option if needing to go even smaller could be to make a custom PCB, with a small high density connector on it, a bit like those in mobile phones. Then you're down to less than 1cm2 footprint and a few mm thick, for 20+ circuits including a few mm for soldering 30AWG wires.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • makerkaren
    makerkaren over 8 years ago in reply to shabaz

    For modding game handhelds, modders want to keep everything as small as possible. I assume, that's why they use the magnet wire instead of insulated wire. Wouldn't adding all those connectors add bulk as well? Is there a small solution?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mayermakes
    mayermakes over 8 years ago in reply to shabaz

    thanks, I also use those premade JST-conectors from time to time, you can see one in my VRpi build video for HLH.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
>