Community Feedback
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Community Feedback
  • More
  • Cancel
Community Feedback
Documents Your Build Ideas - December 2015
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Feedback to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: joeman
  • Date Created: 5 Feb 2016 7:23 PM Date Created
  • Last Updated Last Updated: 30 Jul 2016 11:39 PM
  • Views 2123 views
  • Likes 3 likes
  • Comments 12 comments
Related
Recommended

Your Build Ideas - December 2015

image

element14's The Ben Heck Show

Every month Ben, Karen, and Felix discuss top build suggestions submitted by viewers. If your build idea is mentioned you win a free Ben Heck T-Shirt!

Back to The Ben Heck Show homepage image

Connect with TBHS
Featured Bonus Materials
See All Episodes

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image
Ben, Karen and Felix discuss the top 5 build ideas for December 2015.

 

Congratulations to this month's new build idea winners: hoppend, kingrahl, metroidprimerib, Blacksheep32, and hilts!

 

Submit your build idea for a chance to win!

 

See other Top Build Suggestions!

  • the ben heck show
  • ben heck
  • your_build_ideas
  • build ideas
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • makerkaren
    makerkaren over 10 years ago in reply to beacon_dave +1
    I used to do professional video and you are absolutely right. I think we used the audio mixer to send the audio feed we were recording through our ClearCom system and just kept it at a low level, so you…
  • metroidprimerib
    metroidprimerib over 10 years ago +1
    I did receive the shirt! Thanks Tariq and Karen [and Ben and Felix and camera guy's name I forgot] !
Parents
  • beacon_dave
    beacon_dave over 10 years ago

    The baby monitor/personal stereo combiner has another similar application in that if you are a camera operator you often need to be listening through headphones to the microphones connected to the camera as well as to headphones connected to a venue intercom headset as well. Being able to connect one set of headphones to both headphone outputs via a compact belt pack unit with some mixing/gating/ducking type control would be useful.

     

    Another area where this type of headphone combining problem is encountered is in live streaming webcast production where you often need to be listening to the vision mixer console headphones but also have the ability to monitor the headphone/line output from laptops and various mobile devices in order to monitor the outgoing streams on test devices along with the intercom output. In this case you ideally want multiple stereo aux headphone/line level outputs mixed/switched in with the main console and intercom headphone outputs as above. In this scenario however it would also be useful to have visible audio monitoring of each aux input (variable brightness / tricolour LED) so that you can verify that there is an audio signal still there without having to repeatedly switch to each aux input in turn.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • makerkaren
    makerkaren over 10 years ago in reply to beacon_dave

    I used to do professional video and you are absolutely right. I think we used the audio mixer to send the audio feed we were recording through our ClearCom system and just kept it at a low level, so you could hear it, but then communication through the coms came in at a normal volume. It would have been pretty nice to have the live audio be at normal volume and just get lowered when someone was talking through the coms. That would also be really useful in theatre. Oh man, I would have loved to have had that as a stage manager.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • makerkaren
    makerkaren over 10 years ago in reply to beacon_dave

    I used to do professional video and you are absolutely right. I think we used the audio mixer to send the audio feed we were recording through our ClearCom system and just kept it at a low level, so you could hear it, but then communication through the coms came in at a normal volume. It would have been pretty nice to have the live audio be at normal volume and just get lowered when someone was talking through the coms. That would also be really useful in theatre. Oh man, I would have loved to have had that as a stage manager.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • beacon_dave
    beacon_dave over 10 years ago in reply to makerkaren

    The higher end studio systems cameras tend to have intercom facilities built into the design so not an issue there, however if you are working with ENG type cameras on location then it is a common problem but one that there doesn't seem to be an off-the shelf solution for.

     

    As a result you often see camera operators attempting to wear two different sets of headphones so you get camera audio in one ear and intercom in the other, but in reality both end up slipping off halfway through the filming...

     

    As for the aux inputs scenario, then the RDL monitoring box is the closest I've found

    RM-MP12A ‐ Audio Monitor Panel - 12 Line or Speaker Inputs

    but it still doesn't have impedance matching specifically for headphone level signals, is only mono and doesn't have the audio ducking type functionality for the intercom. so 'close but no cigar...'