element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Documents Super Glue Gun 09: How to Make a Stand -- Episode 318
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 23 Jul 2017 12:58 AM Date Created
  • Last Updated Last Updated: 24 Nov 2017 8:24 AM
  • Views 3313 views
  • Likes 3 likes
  • Comments 13 comments
Related
Recommended

Super Glue Gun 09: How to Make a Stand -- Episode 318

image

element14's The Ben Heck Show

Join the Ben Heck team every week for amazing hacks! Watch them build and mod community-inspired projects using electronics!

Back to The Ben Heck Show homepage image

Super Glue Gun
Community Feedback
See All Episodes

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Previously, the team worked on all the individual parts and mechanisms within the super glue gun including the trigger, the circuitry, the hot end, the auto stand, and the extruder motor.  Now it’s time to bring things together to make a cohesive prototype.  They’ll also work on case design and how it works with the autostand.

 

 

Ben’s been drawing sketches for the case design to figure out placement of the innards. The bottom half will contain the electronics and the top half will bolt onto that and contain the motor, the hot end, and the auto retracting servo. He does a quick mockup with clay to get an idea of the concept in hand.  This will help him visualize how the stand will fit in with the enclosure.

Ben and Karen have a brainstorming session so they can take an in-depth look at the stand. They received some feedback in a previous episode about how the stand could get in the way, become a false trigger, and other problems.  For the stand to work it would have to be used to place the glue gun on a flat surface.  For that to happen they need a workable extension retraction but because it would extend past the gun barrel there is some concern that it will get gummed up.  To address these concerns, Ben returns to his sketchpad to try and come up with a new design.

Next, Ben begins working on a new 3D model in Autodesk Fusion 360. Karen and Ben both agree that it would be beneficial if the gun was longer. This also means that he’ll also need to make some adjustments to the code to accommodate the temperature difference in the hot end.  While their original goal was to come up with a mechanism to operate their auto stand, in doing so they come to the realization that they’ll need to redesign almost the entire top portion of the gun, rotating the motor 90 degrees, and adjusting the positioning (possibly swapping out for a bigger one) of the heating elements.

 

Disclaimer

  • how to make a stand
  • hack
  • super_glue_gun
  • episode 318: super glue gun 09
  • heck
  • ben
  • tbhs_ep
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • ramgarden
    ramgarden over 8 years ago +2
    Have you thought of a Solenoid for the stand? Have it's "off" position to be extended with a spring. Then when you press the trigger (or touch it, or pick it up) it powers the solenoid and retracts the…
  • makerkaren
    makerkaren over 8 years ago in reply to gavmo +1
    An interesting idea. I'll have to run the cordless idea past Ben. We've already discussed the stand solution being making the base wider thus more stable. And he's very aware of how the cord causes stability…
  • DAB
    DAB over 8 years ago in reply to makerkaren +1
    Hi Karen, Why not use a splay type tripod approach for the glue gun stand? Have the front stand angle out away from the barrel when deployed to give you three good points of contact rather than the flimsy…
Parents
  • DAB
    DAB over 8 years ago

    Great episode.

     

    I had two thoughts.

    First, given the issues that Ben had getting the glue to flow, how about an LED to indicate when the nozzle is at operating temperature.

     

    Second, instead of a free standing gun, why not go with a 3D printed holster stand with a glue drip tray so the user could pick it up and put it down easily.  That solution cuts your weight and clunking looking issues and make storage easier for the whole gun.

     

    Just a thought.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • makerkaren
    makerkaren over 8 years ago in reply to DAB

    Thanks for the input!

     

    1. Ben would definitely like to add this as a feature. We're waiting to see if we have enough I/O for it.

     

    2. Ben wants the user to be able to set the gun down anywhere rather having to return it to an external stand like a soldering iron. He's pretty set on that point. I suppose the user could wear the holster, but that seems hazardous from a burn potential standpoint as well as a cord management standpoint. If we made a silicone wearable holster and made it cordless, now that could potentially work, but I think Ben has a Tim "the Tool Man" Taylor attitude of "needs more power" thus batteries would not suffice.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 8 years ago in reply to makerkaren

    From watching my wife use her gun, having a stand to place it in helps keep the work area neat.

     

    Since you already have a cord limit issue anyway, having a place to put the gun down that keeps the hot tip away form anything would be better.

     

    As you have already pointed out, the attempt to free stand the gun makes it easy to tip over unless you are going to add a wider base for stability.

     

     

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 8 years ago in reply to makerkaren

    Hi Karen,

     

    Why not use a splay type tripod approach for the glue gun stand?

    Have the front stand angle out away from the barrel when deployed to give you three good points of contact rather than the flimsy two point approach.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 8 years ago in reply to makerkaren

    Hi Karen,

     

    Why not use a splay type tripod approach for the glue gun stand?

    Have the front stand angle out away from the barrel when deployed to give you three good points of contact rather than the flimsy two point approach.

     

    DAB