element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Polls SEGA Genesis VS Super Nintendo
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: element14Dave
  • Date Created: 7 Jun 2015 11:27 PM Date Created
  • Last Updated Last Updated: 7 Jun 2015 11:27 PM
  • Views 4870 views
  • Likes 0 likes
  • Comments 45 comments
Related
Recommended

SEGA Genesis VS Super Nintendo

Ben Heck recently broke down the Sega Genesis and a Super Nintendo to scientifically prove which 16 Bit console was the best. Which console do you think was better?

  • console_wars
  • 16bit
  • 16_bit
  • sega_vs_snes
  • snes
  • ben_heck
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • johnbeetem
    johnbeetem over 11 years ago +8
    Not having ever used either one or watched Ben's video, I went with the SEGA Genesis since it has a 68000 CPU. I have very fond memories of programming and writing compilers for the 68000. It's a very…
  • johnbeetem
    johnbeetem over 11 years ago in reply to clem57 +5
    Clem Martins wrote: How did you get this about IBM? Were you a CE? I was an assistant professor for six years. I taught two levels of computer architecture. People like to malign IBM as a bunch of…
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to mcb1 +4
    mcb1 , frankly it sounded clear to me that is a 16 bit with internal 32 bit architecture. Despite the wiki I remember this CPU. It was the "revolution" as I have used before the 6502 processor. Wiki says…
Parents
  • johnbeetem
    johnbeetem over 11 years ago

    Not having ever used either one or watched Ben's video, I went with the SEGA Genesis since it has a 68000 CPU.  I have very fond memories of programming and writing compilers for the 68000.  It's a very clean 32-bit architecture and... wait a minute... didn't you say this was a battle of 16-bit consoles?  Why in the world is a 32-bit 68000 considered a 16-bit machine?  Sure, it has an external 16-bit data bus but the internal architecture is all 32-bit.  That would be like saying an Intel 8088 is an 8-bit architecture rather than a 16-bit CPU with an 8-bit data bus.  Grumble grumble whine moan insinuate.

    • Cancel
    • Vote Up +8 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to johnbeetem

    If you believe Wiki it seems its not sure if its 16 or 32 bit.

    http://en.wikipedia.org/wiki/Motorola_68000

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • johnbeetem
    johnbeetem over 11 years ago in reply to mcb1

    mcb1 wrote:

     

    If you believe Wiki it seems its not sure if its 16 or 32 bit.

    http://en.wikipedia.org/wiki/Motorola_68000

    The bit size of a CPU architecture is usually the size of data registers and data ALU.  All the 68000 data and address registers are 32-bit, and arithmetic is all 32-bit.  So internally the 68000 is definitely a 32-bit machine.  A specific chip implementation may have different external data and address bus widths.  The 68020 has 32-bit address and data buses, the 68000 has 24-bit address and 16-bit data buses, and the 68008 has 20-bit address and 8-bit data buses.  Part of the bus width decision is package pin limitations.

     

    If you're planning to support an architecture for a long time it's good to design the architecture for future technology.  The 680X0 architects expected to have future implementations with 32-bit external buses even though they could only do 16-bit data with the first version.

     

    IBM did this with the 32-bit IBM 360.  The first implementations included 8-bit and 16-bit versions which performed 32-bit operations with multiple cycles through 8- or 16-bit ALUs.  I think these used logic made from discrete transistors, or else small-scale integration ICs.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to johnbeetem

    Guys

    I was convinced from the start ...

     

    I came into microcontrollers late, so I never did play with these, but it was certainly the day when the hardware and software limitations ensured the designers had to be clever.

     

    So maybe we should report element14Dave poll as false or misleading?? image

     

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 11 years ago in reply to johnbeetem

    How did you get this about IBM? Were you a CE? image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • screamingtiger
    screamingtiger over 11 years ago in reply to johnbeetem

    Not sure if that is the scientific definition, but if I were to use a "32-bit" processor I would expect to be able to:

    • Store 32 bit values in a single register and be able to use more than 1 32 bit register at a time.
    • Perform basic 32 bit operations such as add, shifting, moving, and multiply and store the result in a single register. (add eax,edx or mov eax,edx)

     

    For a 32 bit "system" I would expect to be able to read/write 32 bit values to memory in a single cycle and/or a single instruction.  I would also expect to be able to address somewhere in the vicinity of 2^32 bytes of memory.  I understand there is some overhead I need to take into account in those numbers but you get the point.

     

    If I had a processor with only a 32 bit accumulator I would not call it 32 bit.  A system with a 32 bit processor and 16 bit bus in my book is not 32 bit.

    I would however consider the "system" to be 32 bit if the processor is only 16 bit but there is an instruction set to move 32bits at a time across the memory bus in a single cycle.  I find memory moves, especially to a video buffer, are the most critical for gaming.

     

    That's my definition.  Based on what I see in the videos both systems are 16 bit by my definition, which has not authority what so ever.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • johnbeetem
    johnbeetem over 11 years ago in reply to clem57

    Clem Martins wrote:

     

    How did you get this about IBM? Were you a CE?

    I was an assistant professor for six years.  I taught two levels of computer architecture.  People like to malign IBM as a bunch of salesmen, but in fact IBM was the first to develop a lot of key computer technology.  For example, the IBM 360/91 (shipped in 1967) pioneered many pipeline speed-up techniques like out-of-order execution and register renaming.  A couple years ago I attended an ARM Techcon session on the then-new Cortex-A15 and its pipelining tricks.  It was pretty much the same material as my own lectures circa 1990.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to johnbeetem

    Every your post I read I should add about 10 years to your experience. Just to be curious, how was the life with babbage ? image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • johnbeetem
    johnbeetem over 11 years ago in reply to screamingtiger

    Joey Thompson wrote:

     

    Not sure if that is the scientific definition, but if I were to use a "32-bit" processor I would expect to be able to:

    • Store 32 bit values in a single register and be able to use more than 1 32 bit register at a time.
    • Perform basic 32 bit operations such as add, shifting, moving, and multiply and store the result in a single register. (add eax,edx or mov eax,edx)

     

    For a 32 bit "system" I would expect to be able to read/write 32 bit values to memory in a single cycle and/or a single instruction...

     

    That's my definition.  Based on what I see in the videos both systems are 16 bit by my definition, which has not authority what so ever.

    That's a good definition.  I also note that the SEGA Genesis case says "16-Bit" in large letters, so it's definitely declaring itself to be a 16-bit system even though it has a 32-bit processor.

     

    OTOH, the original IBM PC considered itself a 16-bit computer even though it was an 8-bit system.  This distinguished the IBM PC from the popular Z-80 systems of the day.  The original Apple Macintosh considered itself a 32-bit computer even though it was a 16-bit system.  This distinguished the Mac from the IBM PC/XT/AT.  So the definitions are somewhat flexible, especially when marketing gets involved image

     

    The BeagleBone uses 16-bit wide memory, but it's clearly a 32-bit computer.  OTOH, that 16-bit wide memory is DDR, so you are getting 32 bits transfered per complete clock cycle.  But then does a 32-bit DDR give you a 64-bit system?  At a certain point the debate gets rather silly IMO image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • johnbeetem
    johnbeetem over 11 years ago in reply to balearicdynamics

    Enrico Miglino wrote:

     

    Every your post I read I should add about 10 years to your experience.  Just to be curious, how was the life with Babbage?

    Chuck was a good guy, but he spent all his time in his machine shop trying to make gears that meshed properly.  And people here complain about having difficulty soldering image

     

    (I once saw Babbage's lathe at the Science Museum in London.)

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • screamingtiger
    screamingtiger over 11 years ago in reply to johnbeetem

    I think that this thread warrant pages of debate.  These are video games systems and this debate is not settled...

     

    I guess if it can transfer 32 bits in a single cycle then it is 32 bits, despite only having a 16 bit buss.  But doesn't DDR have two 16 bit busses?  If so I would call that a 32 bit wide bus.

     

    I wonder if they will ever go to a serial bus for memory?   Serial at the bit level that is.  Then we get a 1 bit bus and through more magic of marketing we have a million bit system?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 11 years ago in reply to screamingtiger

    screamingtiger

         Just like names and pseudonyms, much depends on the intent and not the actual usage. In computers there are variances in CPU, memory, cache, and bus which defines the architecture. It is not so important for the name but to understand the nuances so programming can be done as fast as possible. I have worked at low level and can tell you the 286 was a stupid chip relative to 386. Why? For the 286 to go from real mode to virtual was a simple setup and switch. But to return back on 286 to real for running those old programs took a soft reset of the processor which was nasty business if done wrong. Then they fixed that in 386. Intel has made many changes like this and others which drives low level assembler programmers to lose sleep at night. Look at my headimage

    Clem

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • clem57
    clem57 over 11 years ago in reply to screamingtiger

    screamingtiger

         Just like names and pseudonyms, much depends on the intent and not the actual usage. In computers there are variances in CPU, memory, cache, and bus which defines the architecture. It is not so important for the name but to understand the nuances so programming can be done as fast as possible. I have worked at low level and can tell you the 286 was a stupid chip relative to 386. Why? For the 286 to go from real mode to virtual was a simple setup and switch. But to return back on 286 to real for running those old programs took a soft reset of the processor which was nasty business if done wrong. Then they fixed that in 386. Intel has made many changes like this and others which drives low level assembler programmers to lose sleep at night. Look at my headimage

    Clem