element14 presents
  • Challenges & Projects
  • More
element14 presents
element14 presents Forum Dumb Question
  • Episodes
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14 presents to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 19 replies
  • Subscribers 144 subscribers
  • Views 4330 views
  • Users 0 members are here
Related

Dumb Question

mark1054
mark1054 over 6 years ago

I am a total newb, so this is probably a really dumb question. I have a DC Harmar scooter lift that I need to be able to run from household current. I need to modify it to make a lift to get my wife off the floor when she falls. I have all the plans to do it, I just don't know what I need to convert the DC to AC. Currently, the lift connects to DC via a standard "trailer" plug. So I need to connect it to a converter that will them plug into a wall socket. I spoke to a guy at Harmar and he seemed to think it was doable as long as the device put out a minimum load of 15amp. Any help would be really appreciated. Thanks!

  • Sign in to reply
  • Cancel

Top Replies

  • Fred27
    Fred27 over 6 years ago +3
    What is most important is the DC voltage and current the lift requires. Then it's really a case of finding a suitable power supply. Have you got any more details of the model of lift you're working with…
  • mp2100
    mp2100 over 6 years ago in reply to beacon_dave +3
    It operates from a car's battery, so it's 12 V nominal (really 14 volts) and as Dave said the manual states it could draw up to 20 amps. This item comes close, it can put out 15 amps at 12 volts. https…
  • beacon_dave
    beacon_dave over 6 years ago in reply to shabaz +3
    How about a caravan battery/charger type solution ? Might work out cheaper and be an off-the-shelf solution. Also gives you back-up power to complete the lifting operation during a power outage.
  • beacon_dave
    beacon_dave over 6 years ago in reply to mark1054 +2
    Looks like there is some documentation available here: https://harmar.com/vehicle-lifts/al300hd/ which suggests that it requires a 12V DC supply up to 20A
  • colporteur
    colporteur over 6 years ago +2
    Welcome to the E14 Community Mark. I don't consider your question dumb by any measure. You have a technical problem and you are asking a community that supports technical people a question in their wheelhouse…
  • Fred27
    Fred27 over 6 years ago +2
    This really isn't a dumb question. Maybe it's worth changing the title! It also makes it easier for someone to find useful information if they have a similar question.
  • mark1054
    mark1054 over 6 years ago +2
    It kinda sounds like the easiest way to do this would be with an external battery and trickel charger, Yes?
  • mark1054
    mark1054 over 6 years ago in reply to Fred27 +1
    Hi Fred, thanks for the reply. Ali know is that is a Harmar AL300. Loft capacity is 300lbs.
  • shabaz
    shabaz over 6 years ago in reply to mark1054 +1
    Hi Mark, That needs quite a high-end power supply if the aim is to run it off mains instead of a battery. The manual suggests surges of 20A may be needed (it doesn't suggest for how long) so this may require…
  • shabaz
    shabaz over 6 years ago in reply to mp2100 +1
    That looked like really good value, and wired to a plug too! Unfortunately it is AC output : ( I can't find a DC supply at reasonable cost : ( $600 and higher seem the ballpark : ( You've hit on something…
Parents
  • colporteur
    colporteur over 6 years ago

    Welcome to the E14 Community Mark. I don't consider your question dumb by any measure. You have a technical problem and you are asking a community that supports technical people a question in their wheelhouse.

     

    I have a two solutions. My focus is not aesthetics. The solution is easy to create and safe. It is using technology that already exists today.

     

    I would consider an RV battery and a battery charger. The RV battery can be charged using the charger from an AC source without generating toxic fumes. The battery will meet the current and voltage requirements within a range of uses. If the kids are using the device for a amusement ride it won't hold up.

     

    Good RV batteries can provide well over 30amp/hrs. Your current demand is not for hours but for short periods of time. The battery and charger in a plastic tub from a department store, keeps the cost down if the solution has budget constraints.

     

    If you wanted to go all in on just a battery charger, there are units capable of supplying that amperage and more. I did a quick search for battery charger and starter and got this hit. The 25amp rating meets your requirements. Make up some cables (be sure an use 10AWG wire and rated connectors and your good to go.

     

    image

     

    A wall wart power supply is not going to provide the capacity for such a job. A power supply that can provide the current specified is not going to come cheap. Hang around here long enough and a power supply RoadTest review might net you the ideal unit. Some of those suckers can support 40amps. It will just cost you a RoadTest:)

     

    I'm looking at solutions that are DC power supplies in themselves but are used for a specific task. A battery charger is just a DC supply.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 6 years ago in reply to colporteur

    The charger idea is a pretty robust, low cost solution.

    If the power is simply fed to the motor with a switch, a car battery charger should work without a battery.

    I have an old 16 A charger that has many times been asked to supply over 30 amps (while starting a car).

    I consider it bulletproof - it has been through the war and abused badly, but still works fine.

    At 14.7 Volts it supplies less than 2 Amps, so it doesn't need a voltage limiter/regulator.

    The chargers are about as low cost as you can find. I paid about $30.

    If you want a low cost regulated power supply, the one I have found is an MFJ-4245MV - it works well:

    https://mfjenterprises.com/products/sec-4245mv

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mark1054
    mark1054 over 6 years ago in reply to dougw

    So are you saying I could wire the lift directly to the charger to use it?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 6 years ago in reply to mark1054

    If the lift has electronic circuitry, (for example a speed controller) it may need a regulated voltage.

    If the lift control is just a switch, it should work, as the charger is able to power DC motors.

    Can you describe the controller and what it does?

    If you want to try it, have someone knowledgeable look over your wiring and explain the charger voltage is unregulated - not clean DC.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 6 years ago in reply to mark1054

    image

    I have concerns with your experience level. That being said this is not a complicated project. If you have tried starting a car with booster cables and didn't cause damage during the process then you have knowledge of what you are trying to do. If you fried either car electrical system in your booster attempt then don't attempt this.

     

    If you are going to use the charger to power the lift, then I recommend the charger has some safety features. Some old chargers had no protection circuits. The circuit breaker in the house tripping was the only indication there was a problem. The safety circuits in the charger are providing protection. Yeah you can depend on tripping the house breaker but don't. If the lift draws to much current your expecting the charger protection circuits to work and shut the system down.

     

    If you screw up the polarity of the connections between the devices one or both of the devices will give up their magic smoke that allows them to work. Your not guessing or working on an I think this is right. Be sure.

     

    The charger needs to be capable of supporting the load. Check the specifications. Ensure the cables are sufficient to handle the current load. Like I indicated you need a minimum of 10 awg but that is the electrical code in my area. Ensure the switch is rated to handle the load. The connections have to be mechanically and electrically sound. All connections need to be well insulated.  Your not just twisting two wires together and wrapping it with gaff tape.

     

    I'm trusting you are not using this around water. This is not a 9V battery your sticking your tongue on. Your talking some pretty serious current that has the potential to do some damage. Don't overlook safety just so you can have it working. The charger is just a fancy power supply it can do the job if done correctly.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Fred27
    Fred27 over 6 years ago in reply to mark1054

    I'd be very wary of trying to use just a battery charger to operate the lift. A battery charger is designed to provide a low current (for slow charging) over a long period of time. A car battery is capable of short burst of very high power. It can even melt a spanner if you short out the terminal with one!

     

    I was going to suggest the same as Sean - use a battery for the heavy lifting and a charger to slowly recharge it between uses.

     

    There are devices designed to starts cars from mains power and provide a large amount of power. This may also do the job but is likely to be a more expensive solution.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Fred27
    Fred27 over 6 years ago in reply to mark1054

    I'd be very wary of trying to use just a battery charger to operate the lift. A battery charger is designed to provide a low current (for slow charging) over a long period of time. A car battery is capable of short burst of very high power. It can even melt a spanner if you short out the terminal with one!

     

    I was going to suggest the same as Sean - use a battery for the heavy lifting and a charger to slowly recharge it between uses.

     

    There are devices designed to starts cars from mains power and provide a large amount of power. This may also do the job but is likely to be a more expensive solution.