element14 presents
  • Challenges & Projects
  • More
element14 presents
element14 presents Forum Custom Soldering Station
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14 presents to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 24 replies
  • Subscribers 144 subscribers
  • Views 3823 views
  • Users 0 members are here
  • soldering wishlist
  • soldering iron
  • soldering
  • workbench
  • workshop
Related

Custom Soldering Station

milosrasic98
milosrasic98 over 1 year ago

Hi everyone!

This year, I will be finally moving all of my tools and stuff from the bedroom into a dedicated shop area, which means it's time to make some new custom workshop benches and stuff like that. Since I don't want to have everything built to be fixed to the walls but rather be able to move stuff around, I want to make custom, modular, moveable stations, and the first station I want to work on is the soldering station. To describe the idea closer, here is a list of requirements I would like to fulfill with this build:

  1. Fume extraction hood - This is a must. My idea is to have it enclosed on 3 sides and have some kind of a bigger fan that would get all of the fumes out and, using something like a kitchen hood hose, get that out of the workshop. This is something I really want to do good since I've had health issues from this kind of thing before. Since I won't have any industrial style filters, of course, the main goal is to get the air out of the shop.
  2. Digital microscope - While I've worked with both analog and digital microscopes, and an analog microscopes is superior in many things, for my setup, I still prefer using a digital one since it's smaller and I can pop it up on a monitor. I already have a small digital microscope, which has worked okay, but I also got a microscope lens for a Raspberry Pi HQ camera, so I am going to give that a shot! If that works nicely, my idea would be to attach two monitors to something like a Raspberry Pi 4/5, so I can use one of them for the scope view and the other one for schematics, datasheets, etc.
  3. Tools & Tool Storage - I want to have everything I usually use for soldering right on hand, from power tools such as the soldering iron (currently using the Pinecil V1, love it), hot air gun, and hot plate, to everything else such as tweezers, solder wick, solder, etc. I want everything to have its own dedicated space and also everything to be within arm's reach.
  4. General storage - Have something like an IKEA Alex drawer for common components, etc.
  5. Power management - Since I want this to be a unit on wheels that I can just move around the shop or to a different space, I don't want to have to tackle 10 cables every time, I want a single power cable for the whole unit with a master switch for it in the front.
  6. If a Raspberry is integrated, maybe some smart features like remote power control, smoke sensors?

The main reason I am writing this is because I would love to hear everyone's ideas on what I should integrate and what they would like to see for such a soldering station. I will be covering this build either through blogs or through a video here, so everyone will see how it turns out in the upcoming months!

Let me know your ideas and what are some things that are a must-have on your desk when it comes to soldering and working on PCBs. After this, I will be doing some 3D printer stations also!

Kind regards,

Milos

  • Sign in to reply
  • Cancel

Top Replies

  • strb
    strb over 1 year ago +3
    I would add a good light source. For me, it's just easier to work on small stuff when they are well illuminated.
  • kmikemoo
    kmikemoo over 1 year ago +3
    milosrasic98 Instead of going with a fume extraction hood, try something either to the back or on your non-dominant hand side. This will make placing the good light source that strb recommends an easier…
  • beacon_dave
    beacon_dave over 1 year ago +3
    Clamps and helping hands to hold stuff in place whilst working on it, instead of chasing it around the bench.
  • anniel747
    anniel747 over 1 year ago +2
    Deleted
  • aspork42
    aspork42 over 1 year ago +2
    Add lots of power outlets! I’m waging war on extension cords and power strips at my new place.
  • anniel747
    anniel747 over 1 year ago in reply to kmikemoo +2
    Deleted
  • kmikemoo
    kmikemoo over 1 year ago in reply to anniel747 +2
    anniel747 I did think of that, except I favor horizontal fume extraction because I tend to hoover over my workpiece. Vertical extraction draws it past my face. Not good. I guess it depends on how Milos…
  • robogary
    robogary over 1 year ago +2
    Expanding operations is pretty exciting. Im not sure it possible to keep everything within arms reach, when I try, things get buried in piles in the heat of battle, to pardon the pun. There are also…
  • milosrasic98
    milosrasic98 over 1 year ago in reply to beacon_dave +2
    Those are a must for sure! Recently I started 3D printing custom stands for any of the PCBs I designed, since I can keep the PCB lowers while I am soldering and still keep one of the sides off of the bench…
  • milosrasic98
    milosrasic98 over 1 year ago in reply to shabaz +2
    Hi! The idea with the Pi was also to have easy access to the layout and schematics without having to have a laptop somewhere (connecting to a laptop via AnyDesk or something similar). Now that I think…
Parents
  • robogary
    robogary over 1 year ago

    Expanding operations is pretty exciting.  Im not sure it possible to keep everything within arms reach, when I try, things get buried in piles in the heat of battle, to pardon the pun.  

    There are also families of stuff in the solder area. I have a 100W soldering pencil, a USB solder pencil, and it sounds like you also have surface mount equipment too ? 

    Even tho its a soldering area, I always battle with the need to have tiny tools there too : tiny pliers, small screwdrivers, a needle size drill bit, tweezers, a DVM with tiny probes, a tiny caliper, and magnifying glasses.  

    You're on the right track with rolling drawers. I also have a rolling toolbox just for tiny tools.     

    I also use a magnetic wristband, even tho I might not wear it, I keep it nearby so the stuff Im presently using doesnt roll away and hide me from me. 

    image 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • anniel747
    anniel747 over 1 year ago in reply to robogary
    This reply was deleted.
    • Cancel
    • Cancel
  • robogary
    robogary over 1 year ago in reply to anniel747

    I don't know. I never put a soldering iron on a magnetic band. They get kinda warm.

    I use the wristband to hold screws and little tools. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • robogary
    robogary over 1 year ago in reply to anniel747

    I don't know. I never put a soldering iron on a magnetic band. They get kinda warm.

    I use the wristband to hold screws and little tools.