element14 presents
  • Challenges & Projects
  • More
element14 presents
element14 presents Forum Custom Soldering Station
  • Episodes
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14 presents to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 24 replies
  • Subscribers 144 subscribers
  • Views 4025 views
  • Users 0 members are here
  • soldering wishlist
  • soldering iron
  • soldering
  • workbench
  • workshop
Related

Custom Soldering Station

milosrasic98
milosrasic98 over 1 year ago

Hi everyone!

This year, I will be finally moving all of my tools and stuff from the bedroom into a dedicated shop area, which means it's time to make some new custom workshop benches and stuff like that. Since I don't want to have everything built to be fixed to the walls but rather be able to move stuff around, I want to make custom, modular, moveable stations, and the first station I want to work on is the soldering station. To describe the idea closer, here is a list of requirements I would like to fulfill with this build:

  1. Fume extraction hood - This is a must. My idea is to have it enclosed on 3 sides and have some kind of a bigger fan that would get all of the fumes out and, using something like a kitchen hood hose, get that out of the workshop. This is something I really want to do good since I've had health issues from this kind of thing before. Since I won't have any industrial style filters, of course, the main goal is to get the air out of the shop.
  2. Digital microscope - While I've worked with both analog and digital microscopes, and an analog microscopes is superior in many things, for my setup, I still prefer using a digital one since it's smaller and I can pop it up on a monitor. I already have a small digital microscope, which has worked okay, but I also got a microscope lens for a Raspberry Pi HQ camera, so I am going to give that a shot! If that works nicely, my idea would be to attach two monitors to something like a Raspberry Pi 4/5, so I can use one of them for the scope view and the other one for schematics, datasheets, etc.
  3. Tools & Tool Storage - I want to have everything I usually use for soldering right on hand, from power tools such as the soldering iron (currently using the Pinecil V1, love it), hot air gun, and hot plate, to everything else such as tweezers, solder wick, solder, etc. I want everything to have its own dedicated space and also everything to be within arm's reach.
  4. General storage - Have something like an IKEA Alex drawer for common components, etc.
  5. Power management - Since I want this to be a unit on wheels that I can just move around the shop or to a different space, I don't want to have to tackle 10 cables every time, I want a single power cable for the whole unit with a master switch for it in the front.
  6. If a Raspberry is integrated, maybe some smart features like remote power control, smoke sensors?

The main reason I am writing this is because I would love to hear everyone's ideas on what I should integrate and what they would like to see for such a soldering station. I will be covering this build either through blogs or through a video here, so everyone will see how it turns out in the upcoming months!

Let me know your ideas and what are some things that are a must-have on your desk when it comes to soldering and working on PCBs. After this, I will be doing some 3D printer stations also!

Kind regards,

Milos

  • Sign in to reply
  • Cancel

Top Replies

  • strb
    strb over 1 year ago +3
    I would add a good light source. For me, it's just easier to work on small stuff when they are well illuminated.
  • kmikemoo
    kmikemoo over 1 year ago +3
    milosrasic98 Instead of going with a fume extraction hood, try something either to the back or on your non-dominant hand side. This will make placing the good light source that strb recommends an easier…
  • beacon_dave
    beacon_dave over 1 year ago +3
    Clamps and helping hands to hold stuff in place whilst working on it, instead of chasing it around the bench.
  • anniel747
    anniel747 over 1 year ago +2
    Deleted
  • aspork42
    aspork42 over 1 year ago +2
    Add lots of power outlets! I’m waging war on extension cords and power strips at my new place.
  • anniel747
    anniel747 over 1 year ago in reply to kmikemoo +2
    Deleted
  • kmikemoo
    kmikemoo over 1 year ago in reply to anniel747 +2
    anniel747 I did think of that, except I favor horizontal fume extraction because I tend to hoover over my workpiece. Vertical extraction draws it past my face. Not good. I guess it depends on how Milos…
  • robogary
    robogary over 1 year ago +2
    Expanding operations is pretty exciting. Im not sure it possible to keep everything within arms reach, when I try, things get buried in piles in the heat of battle, to pardon the pun. There are also…
  • milosrasic98
    milosrasic98 over 1 year ago in reply to beacon_dave +2
    Those are a must for sure! Recently I started 3D printing custom stands for any of the PCBs I designed, since I can keep the PCB lowers while I am soldering and still keep one of the sides off of the bench…
  • milosrasic98
    milosrasic98 over 1 year ago in reply to shabaz +2
    Hi! The idea with the Pi was also to have easy access to the layout and schematics without having to have a laptop somewhere (connecting to a laptop via AnyDesk or something similar). Now that I think…
  • aspork42
    aspork42 over 1 year ago in reply to anniel747

    That’s a really good deal! I love those things but have always seen them at like $50+

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 1 year ago

    Hi,

    A few random comments:

    You could save space and cost, by removing any microscope and Pi, since a head-mount Optivisor is possibly more convenient. For inspection, any decent small magnifier should be sufficient for general work.

    Definitely a good idea to have the PDU, you could also use the ones with IEC connectors, if you're short on space.

    Hot air tool and hot plate don't have a lot in common with a soldering iron, so you could separate them if you like, they don't need to be close.

    Worth getting a soldering station (could be a used one from ebay to save cost) since it will have proper grounding versus the USB irons, plus rubber ESD mat and wrist strap would be good at a minimum.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • robogary
    robogary over 1 year ago in reply to anniel747

    I don't know. I never put a soldering iron on a magnetic band. They get kinda warm.

    I use the wristband to hold screws and little tools. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • milosrasic98
    milosrasic98 over 1 year ago in reply to anniel747

    Great recommendation, thanks! I'm surpised at how low cost this actually is, I just need to find a 220V EU Plug version, but I will be getting something like this for sure!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • milosrasic98
    milosrasic98 over 1 year ago in reply to strb

    Thanks for the recommendation, definitely! I keep using strong filming lights on my workbench to get enough light, so this is something I'll need to tackle for sure.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • milosrasic98
    milosrasic98 over 1 year ago in reply to aspork42

    There are never enough power outlets for sure!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • milosrasic98
    milosrasic98 over 1 year ago in reply to kmikemoo

    The reason why I was thinking of experimenting with a hood is that I currently use one that is off to the side. I constantly tend to bump into it as I'm working. As for the light source, the idea was to have the whole inside well illuminated plus an additional ring light on the microscope. Monitor on the back for sure, especially because I often lean back into the chair rather than being hunched over the bench, I like getting further from the fumes and I can also sit like that and work for hours!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • milosrasic98
    milosrasic98 over 1 year ago in reply to beacon_dave

    Those are a must for sure! Recently I started 3D printing custom stands for any of the PCBs I designed, since I can keep the PCB lowers while I am soldering and still keep one of the sides off of the bench!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • milosrasic98
    milosrasic98 over 1 year ago in reply to robogary

    They get buried for sure! I force myself to do a 15-minute tidy up after any soldering work to put all of the stuff in place, since I of course, just grab what I need while I am working and throw it to an empty spot as I am done with it!

    So for the soldering equipment, I have a small station that has a soldering iron and a hot air gun, and a USB soldering iron, which is the main iron I use for 95% of the tasks if I don't need hot air. Also, have the hot plate, though it doesn't see as much use as the other stuff.

    I am still trying to figure out what would be a better option for some of those tools, a rolling cart or just having a double of some of the stuff. But some things like tweezers, a DMM with needle probes, etc, are essential to have on hand for sure!

    Having something magnetic to keep the stuff from rolling off is a great idea! I often push hex keys and screws off with my elbows!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • milosrasic98
    milosrasic98 over 1 year ago in reply to shabaz

    Hi!

    The idea with the Pi was also to have easy access to the layout and schematics without having to have a laptop somewhere (connecting to a laptop via AnyDesk or something similar). Now that I think of it, I've seen the head-mounted Optivisors, but I've never actually used one hahaha. I know they are pretty inexpensive, so I'll pick one up to try it! I mostly work with 0603/0402, QFN packages, etc, not going smaller than that yet, and the microscope has been a pretty solid thing so far, but I'll give the visor a try to see how it goes, thanks!

    PDU looks like a really good option, I'll integrate it for sure!

    The hot plate doesn't get a lot of use, it's just convenient to have it to preheat PCBs in some cases. So the plate itself doesn't have to have a permanent spot on the surface for sure. The hot air gets a lot of use.

    Trying out some friends soldering stations to see what else I could get, the Pinceil works great and is really tiny which is why I love using it, though a JBC station I tried I loved as well of course! ESD mat for sure!

    Thanks for the comments!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
<>