element14 presents
  • Challenges & Projects
  • More
element14 presents
Files Episode 573: Using a Pi Pico to Convert Keyboard Input to Morse Code Supplemental File
  • Episodes
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14 presents to participate - click to join for free!
Actions
  • Next
  • Previous
  • Share
  • More
  • Cancel
  • Author Author: cstanton
  • Views 2255 views
  • Downloads 79 downloads
  • Likes 0 likes
  • Comments 11 comments
Related
Recommended

Episode 573: Using a Pi Pico to Convert Keyboard Input to Morse Code Supplemental File

As used in Episode 573: Using a Pi Pico to Convert Keyboard Input to Morse Code.

Please create an account and/or login to see the ability to download this file if you do not see the Download button.

  • episode 573
  • supplemental content
cstanton
cstanton
  • 14 Oct 2022
  • 79 Downloads
  • Share
  • More
  • Cancel
  • Sign in to reply
Parents
  • stefanT64
    stefanT64 over 2 years ago

    I have used usb type of ''hello world'' after compiling this, not sure this uses tinyusb though. I could read message both with putty and serial port in VSC.
    Pls confirm if this is a good sign that this example work regarding tinyusb.

    Compiling other examples in usb example folder also works without errors but have not really tried if they behave as expected, only loaded UF2 file.
    This by using Windows SDK.

    Yesterday I cleaned and updated RPI4B with new Raspian and also SDK for pico and plan to try this also for programming the pico, but not tested yet. This to make sure my setup in Windows is not the root cause.

    The picoprobe for debug/load that I would like to use has not arrived yet.And will continue fight with this cw keyboard when available, hopefully later this week.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to stefanT64

    I have used usb type of ''hello world'' after compiling this, not sure this uses tinyusb though. I could read message both with putty and serial port in VSC.
    Pls confirm if this is a good sign that this example work regarding tinyusb.

    Try this one:

    image

    The morse code project is an adapted version of that one.
    If you can make this one build, you should be able to start from there, and retrofit the morse code into it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to stefanT64

    I have used usb type of ''hello world'' after compiling this, not sure this uses tinyusb though. I could read message both with putty and serial port in VSC.
    Pls confirm if this is a good sign that this example work regarding tinyusb.

    Try this one:

    image

    The morse code project is an adapted version of that one.
    If you can make this one build, you should be able to start from there, and retrofit the morse code into it.