Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents Lego Spike Prime Weather Station with Raspberry Pi -- Episode 543
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 10 Mar 2022 6:37 PM Date Created
  • Last Updated Last Updated: 25 Mar 2022 8:24 AM
  • Views 18360 views
  • Likes 9 likes
  • Comments 27 comments

Lego Spike Prime Weather Station with Raspberry Pi -- Episode 543

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

It felt like it was time for another lego based project, but with the Rpi Build Hat, combining Lego and a Raspberry Pi together has never been easier!

 

Supplemental Content:

  • Episode 465: Lego Raspberry Pi HQ Camera
  • Build Hat Compatibility
  • Build Hat setup
  • Met Office weather API
  • Resources

Bill of Material:

Product Name Manufacturer Quantity Buy Kit
RPI4-MODBP-4GB - Raspberry Pi 4 Model B RASPBERRY-PI 1 Buy Now
16GB MicroSD Card with NOOBS for Raspberry Pi TRANSCEND 1 Buy Now
SC0622 RASPBERRY PI BUILD HAT RASPBERRY-PI 1 Buy Now
SC0746 Power Supply, Raspberry Pi Board, 48W, UK RASPBERRY-PI 1 Buy Now
 

Additional Parts:

Lego Spike Prime set

element14 presents

element14 presents  |  About Katie Dumont |  Project Videos

  • LEGO
  • e14p_KD
  • Lego Spike Prime
  • weather
  • raspberry pi
  • katie
  • rpi
  • Daily Weather Display
  • friday_release
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • kmikemoo
    kmikemoo over 4 years ago +1
    hifromkatie Nice project. Very cute. Well executed.
Parents
  • beacon_dave
    beacon_dave over 4 years ago

    Great project.

    ( Now, can you make an input version that allows you to select the weather ?  Slight smile )

    One issue I find though is that these type of projects often tie-up what is often a very limited Lego resource. If you want to keep that weather station, you now have to go replenish your Lego box with the parts you have used, which I suspect could be quite expensive as motors were never the cheapest of Lego parts. Alternatively you view this as the prototype version and then you recreate it with a final build using cheaper components along with 3D printing and then return the Lego parts from the prototype version back to Lego stock for the next project.

    With this build, you have hidden most of the Lego look behind the printed cover sheet. Perhaps for true 'LegoLand' style you could use some of the flat shiny tiles (yup the ones that are a nightmare to remove) mosaic stile with stick-on numbers where required.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hifromkatie
    hifromkatie over 4 years ago in reply to beacon_dave

    Yes, I think this fits the prototyping model really well, quick to build up a working model and test the theory and code before buying specific hardware.

    As a bonus, I do lots of school sessions as a stem ambassador, and taking this in to the schools has sparked alot of attention from the children.

    If only I could use it as a weather input, that would be bliss!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 4 years ago in reply to shabaz

    Some napkin sketch type calculations would suggest that the overall motor brick would likely end up being 4x4 Lego units square by three bricks high. 31.8 x 31.8 x 28.8mm (WxDxH) to keep it nice with standard Lego geometry and yet be large enough to accommodate the motor plus room for a 4x4 Lego unit plate glued on top and bottom.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 4 years ago in reply to beacon_dave

    motor in a toy building block

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 4 years ago in reply to beacon_dave

    Hi Dave,

    Wow - that's really neat! It looks better than real Lego motors : ) Very nice compact design. I take it just the green bit is 3D printed and the plates would be normal Lego as you mentioned earlier.

    I think I might bit the bullet and get a 3D printer at some point this year (and just rely on 3D files created by others for now, since I'm still a beginner).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 4 years ago in reply to beacon_dave

    If you don't mind, can I add that image into the motor controller blog post? Just so it doesn't get lost in the comments, that this is how people could use such motors. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 4 years ago in reply to shabaz

    I can't edit the comments : (

    I was thinking, perhaps an iteration of it could also have holes on the rear (maybe the other sides too) to accommodate studs for both old and new style technic beams as shown here in yellow and blue. But that may result in a bigger cube if the plastic doesn't have the thickness internally for the studs to fit in, so perhaps it's not worth the effort, since the small cube design is nice and useful as-is.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 4 years ago in reply to shabaz

    Yes, the green bit is the 3D printed bit and the red and blue are the standard 4 x 4 plates used to cap it off.

    Could potentially get it a bit smaller but at the risk of ending up with non-standard spacings.

    motor in block

    Currently it matches the height of 3 normal bricks (or 9 plates).

    By rotating the flange by 45 degrees it may be possible to fit it into 3 units wide but not sure if you can get a 4 x 3 plate to cap it with. Could also reduce the height to 2 bricks plus 2 plates, but thought it was easier to start off like this as a proof of concept.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 4 years ago in reply to shabaz

    Feel free. I'm already feeling guilty about filling up Katie's project thread here... 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 4 years ago in reply to shabaz

    Lots of holes like that can be tricky with FDM 3D printing. What might be easier is to build three sides out of the motor block out of Technic beams and then just 3D print the faceplate for the motor on the fourth side and then trap it between the top and bottom plates. A few dabs of glue if you want to make it a permanent motor block. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 4 years ago in reply to beacon_dave

    Done, thanks.

    This is a really affordable alternative to Lego motors if a 3D printer is available (which probably a lot of schools have by now).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 4 years ago in reply to shabaz

    A small laser cutter could be used as an alternative to make it as well. Could cut a load of end panels out of a single sheet to mount the motors on, using castellation top and bottom to knit with the lego bumps for additional strength.  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • beacon_dave
    beacon_dave over 4 years ago in reply to shabaz

    A small laser cutter could be used as an alternative to make it as well. Could cut a load of end panels out of a single sheet to mount the motors on, using castellation top and bottom to knit with the lego bumps for additional strength.