Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents 3D Object Rendering Using an FPGA -- Episode 558
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 7 Jul 2022 2:04 PM Date Created
  • Last Updated Last Updated: 8 Jul 2022 7:24 AM
  • Views 136453 views
  • Likes 8 likes
  • Comments 15 comments

3D Object Rendering Using an FPGA -- Episode 558

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Rendering of 3D models is a computationally expensive task and often slow. With hardware customization and reprogrammable flexibility using FPGAs, highest performance can be achieved. So we are going to build customized hardware on a FPGA Cyclone IV E (DE0 nano board) to render 3D objects into images, and finally, display the rendered images on a monitor over VGA. I have used Verilog for the hardware implementation so that the code can be easily compiled for most FPGAs out there. Happy Rendering!

 

Supplemental Material:

  • Triangle rasterization
  • Download Quartus Prime Lite
  • Rotation Matrix
  • 558_Resources.zip

Bill of Material:

Product Name Manufacturer Quantity Buy Kit
Development Kit, Altera Cyclone IV FPGA , DE0-Nano, 2x GPIO Headers, 32MB SDRAM, Accelerometer TERASIC TECHNOLOGIES 1 Buy Now
 

Additional Parts:

Wire Gauge:28AWG

element14 presents

element14 presents  |  About Surbika Rastogi |  Project Videos

  • Rasterization
  • fpga
  • rendering
  • surbika
  • element14 presents
  • verilog
  • friday_release
  • vlsi
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • surbhika
    surbhika over 4 years ago in reply to shabaz +1
    shabaz i am keen to get the complete results too and also going through few boards which facilitates easy integration with micro-controllers... may be that will be a better and optimised step forward.
  • surbhika
    surbhika over 4 years ago in reply to beacon_dave +1
    There was no way to fit more than few triangles in this design. Though there are few little things in terms of floating point representation etc.which can be optimized in the code (which i realized afterwards…
  • surbhika
    surbhika over 4 years ago in reply to cstanton +1
    Indeed. Limited resources lead to optimized designs!
Parents
  • beacon_dave
    beacon_dave over 4 years ago

    How much FPGA resource was left by the end ? Part of the way through it looked like there was still enough resource to model about 25% of the car. Just wondering if there was enough resource left to model a few more triangles to render a bit more of the car model, or if the two triangles were about the limit ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • surbhika
    surbhika over 4 years ago in reply to beacon_dave

    There was no way to fit more than few triangles in this design. Though there are few little things in terms of floating point representation etc.which can be optimized in the code (which i realized afterwards) to fit more triangles. But that complete car model (i showed initially) was almost impossible to even store in ROM let alone rendering it. It's a single clock cycle implementation right now. I wish to build pipeline to allow rendering of just few triangles in a single cycle.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • surbhika
    surbhika over 4 years ago in reply to beacon_dave

    There was no way to fit more than few triangles in this design. Though there are few little things in terms of floating point representation etc.which can be optimized in the code (which i realized afterwards) to fit more triangles. But that complete car model (i showed initially) was almost impossible to even store in ROM let alone rendering it. It's a single clock cycle implementation right now. I wish to build pipeline to allow rendering of just few triangles in a single cycle.