Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents How to Automate Industrial Welding Positioners with Arduino -- Episode 566
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 11 Aug 2022 5:03 PM Date Created
  • Last Updated Last Updated: 2 Sep 2022 7:24 AM
  • Views 467472 views
  • Likes 7 likes
  • Comments 15 comments

How to Automate Industrial Welding Positioners with Arduino -- Episode 566

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

In this episode we are looking at a couple of welding positioners that I worked on. Retrofitting one from an old lost PLC to arduino, and another built from scratch. Both of these devices are designed for use with a TIG welder. The rotary positioner puts the work where you need it, and the linear positioner holds the torch and moves it in a precise line to get perfect dimes!

Bill of Material:

Product Name Manufacturer Quantity Buy Kit
Arduino UNO Arduino 2 Buy Now
Toggle Switch EATON 2 Buy Now
Rotary Encoder Bourns 1 Buy Now
Power Supply XP Power 2 Buy Now
 

Additional Parts:

3v Relay Module
8ch Optoisolator
NEMA 34 Stepper Motor
NEMA 32 Stepper Motor Driver
20x4 I2C LCD Display Module
Arduino UNO Screw Terminal Breakout Board

element14 presents

element14 presents  |  About Kaleb |  Project Videos

  • welding
  • diy
  • TIG
  • Welder
  • arduino
  • e14p_KC
  • friday_release
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • KalebTheMaker
    KalebTheMaker over 4 years ago in reply to kmikemoo +1
    That is interesting, I did not know about that. I have some other projects that are going to be near TIG welders coming up, I will have to give this a shot. The interference was able to put enough voltage…
  • KalebTheMaker
    KalebTheMaker over 4 years ago +1
    One thing I forgot to mention in the video is how the system was grounded. I'll try to explain. When this shop was built, the guy that owns it built a steel mesh into the concrete with 3/4" threaded…
Parents
  • RichG
    RichG over 4 years ago

    For the interference from the welder refer to the operators manual for radio and tv or electronic interference or the welder manufacturer. The arduino should be in a steel enclosure with a solid ground connection, and all cables going in and out must be sheilded and the sheild must be grounded only on the end in the control box.

    I worked in an electric motor shop where we built control boxes for industrial customers. We used PLCs but the interference problems are the same. I also went to welder repair school at the Lincoln Electric factory. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • KalebTheMaker
    KalebTheMaker over 4 years ago in reply to RichG

    The guy that I was working on this for was quite proud of his reused festool box for an enclosure and wanted to use that, haha... In place of that, he had the enclosure lined with a thick foil, which was grounded. The cables were shielded and grounded inside the enclosure. Maybe the steel box would have made the difference. However, after I removed all of the inputs from the control pendant, the arduino stopped resetting or freaking out when the welder fired.

    I forgot to talk about the grounding in this building in the video. The guy that owns the shop built in some interesting grounding when he built it. All outlets and breaker boxes were tied to a common ground that was sunk into earth per normal spec, but then he tied that into a system of steel anchors he built into the concrete floor. It was a grid of steel something like 1m x 1m, with 1" threaded inserts at each intersection for him to bolt things down onto the floor. The ground was also tied into the rebar in the concrete. He claimed that his acts as a huge ground plane, as well as giving many points to tie in an extra ground. 

    The welder was running 3 phase 480, and had a separate ground that was tied directly to one of those threaded inserts. The control box ground was just tied in through the 110v receptacle. 

    Maybe this helped, or maybe it made it worse. Anybody have any ideas on that?

    Thanks,
    -Kaleb

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kmikemoo
    kmikemoo over 4 years ago in reply to KalebTheMaker

    That's an impressive ground system.  It is a huge equipotential ground plane - similar to what goes under high voltage substations.  The hope is that if something goes catastrophically wrong, you are the bird on the wire.  No step potential (delta V between your legs).  Think "dissipating lightning strike" and it really makes sense.

    A great grounding system didn't work against you.  Proximity transmitter to receiver worked against you.  At least you didn't have to worry about circulating ground currents.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • kmikemoo
    kmikemoo over 4 years ago in reply to KalebTheMaker

    That's an impressive ground system.  It is a huge equipotential ground plane - similar to what goes under high voltage substations.  The hope is that if something goes catastrophically wrong, you are the bird on the wire.  No step potential (delta V between your legs).  Think "dissipating lightning strike" and it really makes sense.

    A great grounding system didn't work against you.  Proximity transmitter to receiver worked against you.  At least you didn't have to worry about circulating ground currents.