Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents Multi-Spectrum UV Resin Curing Station with Würth Elektronik LEDs -- Episode 569
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 8 Sep 2022 8:24 PM Date Created
  • Last Updated Last Updated: 23 Sep 2022 7:24 AM
  • Views 123937 views
  • Likes 8 likes
  • Comments 7 comments

Multi-Spectrum UV Resin Curing Station with Würth Elektronik LEDs -- Episode 569

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

If you have cured a resin 3d print before, you may have noticed that some resins take longer to cure than others, and they also react differently in various curing stations. Most of the commercially available devices just blast the part with broad spectrum UV and don't care how much energy they are using. In some extreme cases this energy builds up heat inside the 3d printed part which can lead to cracking. Clem is hunting for solution! Is there a perfect spectrum and intensity to allow each Resin to get the fastest curing time while using the least amount of energy? Which spectrum exactly is responsible for curing, and can we cut energy bills by just omitting any spectrum that doesn't help the process? To find out, Clem constructs a curing station with Würth Elektronik high precision UV leds and Magi³C Led Drivers!

The results were incomplete at the time of filming of the video so you can view them in the following writeup:

I have printed 5 samples for each spectrum and compared the curing results after 10 mins and 20 mins for each spectrum.
In comparison there is also a pic of a part cured 1hour in broad daylight, but that is not really comparable as the spectrum and power intake is not controlled.

image


Each sample got exposed to 700mA at 24V over 6 LEDs for each spectrum.
The comparison pictures are color graded to make the differences more pronounced.
Here are my initial findings:
Resin: MAYER MAKES Engineering Resin
Test: which spectrum is responsible for Curing
Test: is one of these specifically affecting the curing indicator(aka could it lead to false positives)
370 No effect noticeable (only curing due to unwanted activation of 405??)
385 very limited effect after 10 min (overlapping with 395 in spectrum)
395 part mostly cured, expected behavior.
405 part mostly cured, expected behavior.
The material is intended to be cured by UV light in the range of 395-405nm, which the test confirmed.
it also showed that UV range below this spectrum did not affect the curing process- > therefore these ranges would only waste energy.
The curing indicator faded after 20mins at 2mm, so we can derive an expected curing time of 10min/1mm @405nm
I suspect most of the indicator that faded in the 395nm test is due to overlap in spectrum at the high end.
Concluding that indeed 405nm is the spectrum that is responsible for the curing and decomposition of the indicator.
Thicker portions of course need longer exposure and this effect is non linear. we don't have long term tests under controlled conditions, but i expect the amount to be logarithmic in nature analogous to the fall of of light intensity when travelling through thick glass.

Supplemental Content:

  • You can also download all the CAD, ECAD,and Code for this project for free:  Episode 569 Resources
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
Bill of Material:

Product Name Manufacturer Quantity Buy Kit
"MEAN WELL AC/DC Power Supply mean well Buy Now
"NANOTEC Stepper Motor nanotec Buy Now
"TDK SMD Multilayer Ceramic Capacitor TDK Buy Now
"ONSEMI Fixed LDO Voltage Regulator onsemi Buy Now
"MULTICOMP USB Connector multicomp pro Buy Now
"MULTICOMP PRO Heat Sink multicomp pro Buy Now
"KYOCERA AVX SMD Multilayer Ceramic Capacitor Kyocera Buy Now
"PRO POWER Tape pro power Buy Now
"BOURNS Rotary Encoder Bourns Buy Now
Würth Elektronik UV LED 370/365nm Würth Elektronik Buy Now
Würth Elektronik  UV LED 385nm Würth Elektronik Buy Now
Würth Elektronik UV LED 395nm Würth Elektronik Buy Now
Würth Elektronik UV LED 405nm Würth Elektronik Buy Now
Würth Elektronik Led Driver magi³c Dev kit Würth Elektronik Buy Now
Individual drivers not listed on Farnell yet. Würth Elektronik Buy Now
 

Additional Parts:

Esp32S2-Wroom
Midas Oled from previous project.
TMC2208 stepstick
element14 presents

element14 presents  |  About Clem  |  Project Videos

  • esp32
  • Resin curing
  • Resin 3d print
  • würth
  • Wurth LEDs
  • würth elektronik
  • Multi Spectrum
  • friday_release
  • e14p_CMM
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply
Parents
  • dougw
    dougw over 4 years ago

    If you paint or dip a PLA additive model with UV resin and then cure it with UV light, does it adhere to the PLA and does it improve the smoothness of the finish?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mayermakes
    mayermakes over 4 years ago in reply to dougw

    Yes, it does if the surface is clean and degreased.
    there are commercial products sold for exactly this purpose, and they are just UV reactive resins.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mayermakes
    mayermakes over 4 years ago in reply to dougw

    Yes, it does if the surface is clean and degreased.
    there are commercial products sold for exactly this purpose, and they are just UV reactive resins.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • dougw
    dougw over 4 years ago in reply to mayermakes

    I am wondering if the index of refraction could be matched well enough to make "clear" PLA end up as a transparent window by coating it with a clear resin.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mayermakes
    mayermakes over 4 years ago in reply to dougw

    the issue lies within the layer contact areas, you can get fairly translucent PETG prints wit h100% linera infill and big layer hights and surely can make that effect a bit better wit hcoating, but its never 100% transparent. For PLA not so much.
    if one needs robust transparent prints than Engineering Resin is the way to go.