Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents Making a WiFi Connected Audio Spectrum Analyzer with ESP32 -- Episode 570
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 8 Sep 2022 8:27 PM Date Created
  • Last Updated Last Updated: 30 Sep 2022 7:24 AM
  • Views 127821 views
  • Likes 10 likes
  • Comments 31 comments

Making a WiFi Connected Audio Spectrum Analyzer with ESP32 -- Episode 570

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

This IoT/Web based Spectrum Analyzer uses a single ESP32 to create up to 64 channels to visualize the different audio bands.It uses only 6 external components to function .It has no LEDS or TFT screens but it uses a HTML webpage to display all the frequency bars. The ESP32 used is running on both processor cores. Core 1 is used to run the main loop of the program while core 0 is used to constantly update the webdata. Although the program itself makes it possible to run on a single core, using both cores will lead to better performance. This is so easy to build and program; you just have to try it! You won’t even have to install the ARDUINO software. Just use the web programmer to upload the precompiled binary file.

 

Supplemental Content:

  • Episode 570 Resources
  • Web Browser Programming:  https://donnersm.github.io/WebSpecElement/flash.html
  • ESP32 Repository: :  https://dl.espressif.com/dl/package_esp32_index.json
Layout Schematic
image image

Bill of Material:

Product Name Manufacturer Quantity Buy Kit
Resistor Te Connectivity 4 Buy Now
Capacitor TDK 1 Buy Now
Switch Tactil Te Connectivity 1 Buy Now
 

Additional Parts:

ESP32 DOIT DEVKIT V1.0. You can use other ESP32 but you will have to adjust the wiring accordingly
A breadboard or experimantal PCB to build the circuit on.

element14 presents

element14 presents  |  About Mark Donners |  Project Videos

  • esp32
  • webserver
  • devkit
  • spectrum analyzer
  • DOIT
  • e14p_MD
  • Audio Visualizer
  • iot
  • arduino
  • friday_release
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • donnersm
    donnersm over 4 years ago in reply to kmikemoo +1
    And the best part, using the webprogrammer makes it so easy.
Parents
  • DavidB
    DavidB over 3 years ago

    Hi Mark, interesting project.

    I am having problems with the webprogrammer. I have used a windows 10 and windows 11  PC and tried both Edge and Chrome. I have successfully loaded the blink sketch into the ESP32 on both PCs. The first message I get is "Failed to initialize. Try resetting your device or holding the BOOT while selecting your serial port." After trying the boot button the new message that I get is "Error: Downlading firmware WebSpecElement.binfailed: 404" Yes that was how downloading was spelt in the error message.

    From the Chrome inspection console I see this message "GET donnersm.github.io/.../WebSpecElement.bin 404" four times. Browsing to the indicated webpage returns a file not found error. 

    Does the webpage still exist? Has the browser evolved to the point where this functionality is no longer supported?

    Thanks David

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DavidB
    DavidB over 3 years ago

    Hi Mark, interesting project.

    I am having problems with the webprogrammer. I have used a windows 10 and windows 11  PC and tried both Edge and Chrome. I have successfully loaded the blink sketch into the ESP32 on both PCs. The first message I get is "Failed to initialize. Try resetting your device or holding the BOOT while selecting your serial port." After trying the boot button the new message that I get is "Error: Downlading firmware WebSpecElement.binfailed: 404" Yes that was how downloading was spelt in the error message.

    From the Chrome inspection console I see this message "GET donnersm.github.io/.../WebSpecElement.bin 404" four times. Browsing to the indicated webpage returns a file not found error. 

    Does the webpage still exist? Has the browser evolved to the point where this functionality is no longer supported?

    Thanks David

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • HolleDD64
    HolleDD64 over 2 years ago in reply to DavidB

    Hallo, ich habe das gleich Problem wie David, erst kommt die Fehlermeldung: Failed to initialize. Try resetting your device or holding the BOOT button while selecting your serial port. Dann nach Boost die Meldung: Error: Downlading firmware WebSpecElement.bin failed: 404 was kann ich tun? ESP-WROOM-32 38 Pin - USB-C PORT Silicon Labs CP210x USB to UART Brige (COM4) bitte um Hilfe
    -----------------------------------------------
    Hello, I have the same problem as David, first I get the error message: Failed to initialize. Try resetting your device or holding the BOOT button while selecting your serial port. Then after Boost the message: Error: Downlading firmware WebSpecElement.bin failed: 404 what can I do? ESP-WROOM-32 38 Pin - USB-C PORT Silicon Labs CP210x USB to UART Brige (COM4) please help