Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents Enhancing a Magnifying Headband with Auto Sensing Light -- Episode 585
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 12 Jan 2023 4:58 PM Date Created
  • Last Updated Last Updated: 13 Jan 2023 8:24 AM
  • Views 25501 views
  • Likes 8 likes
  • Comments 27 comments

Enhancing a Magnifying Headband with Auto Sensing Light -- Episode 585

Do you often use a illuminated magnification headband? Do you get annoyed that you need to turn it off and on when looking away from your work? This project contains 2 solutions, a basic tilt sensor option that can be added in minutes, and a more complex distance detecting circuit which will change the illumination depending on how far away the object you are looking at is.

Watch the Video:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Bonus Content:

  • Download Code and Schematics

Bill of Material:

Product Name Manufacturer Quantity Buy Kit
LC1780USB Magnifier, Spectacles & Headband, 1x, 1.5x, 2x, 2.5x & 3.5x LIGHTCRAFT 1 Buy Now
102010328 Arduino Microcontroller Board, SAMD21G18, ARM Cortex-M0+ SEEED STUDIO 1 Buy Now
STMICROELECTRONICS Daughter Board, VL53L0X Gesture and Ranging Sensor, FlightSense STMICROELECTRONICS 1 Buy Now
MICROCHIP Power MOSFET, N Channel, 60 V, 200 mA, 5 ohm, TO-92, Through Hole MICROCHIP 1 Buy Now
COMUS (ASSEMTECH) Tilt Switch, 15 °, 60 Vac, 0.25 A, Nickel COMUS (ASSEMTECH) 1 Buy Now
 

element14 presents

element14 presents  |  About Katie Dumont |  Project Videos

  • tilt
  • e14p_KD
  • magnification
  • Xiao
  • Distance sense
  • illuminate
  • modify
  • friday_release
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • hifromkatie
    hifromkatie over 3 years ago in reply to DAB +1
    Thanks, it hard to find the culprit further than "something under the epoxy blob", by bypassing the switch circuit which has the auto power off and other stuff hidden under expoxy, the problem is resolved…
Parents
  • dougw
    dougw over 3 years ago

    Check if the FET control signal is "flickering".

    You can separate the supply to the MCU with a diode and capacitor. If the sensor is dragging the supply around, power it directly or separately from the battery (have the diode and capacitor only on the MCU. 

    If the MCU is not crashing, it should also be possible to put a diode and capacitor on the FET control signal, to prevent it from flickering.

    If there really isn't enough current to run everything even with diode separation, one thing to try is running the MCU and sensors from a separate battery.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dougw
    dougw over 3 years ago

    Check if the FET control signal is "flickering".

    You can separate the supply to the MCU with a diode and capacitor. If the sensor is dragging the supply around, power it directly or separately from the battery (have the diode and capacitor only on the MCU. 

    If the MCU is not crashing, it should also be possible to put a diode and capacitor on the FET control signal, to prevent it from flickering.

    If there really isn't enough current to run everything even with diode separation, one thing to try is running the MCU and sensors from a separate battery.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • hifromkatie
    hifromkatie over 3 years ago in reply to dougw

    Separating the supply is a good call. I had been hoping to do a bit of a redesign and get a fix before the video was out, but Christmas got in the way.
    The Micro or the Sensor aren't resetting/browning out, as comms says up between the 2 of them, and the PC without missing a beat (or bit).
    My next call is to remove the switch and the PCB it's attached to (which at a minimum has some sort of switch IC under the blob) and replace them with a latching switch.
    That should fix it, as when the micro is plugged in to the USB, and the switch on the light is off it all works as it should with no flickering, it's only as soon as the battery is powering it through that switch PCB that it begins to fail.