Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents Enhancing a Magnifying Headband with Auto Sensing Light -- Episode 585
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 12 Jan 2023 4:58 PM Date Created
  • Last Updated Last Updated: 13 Jan 2023 8:24 AM
  • Views 25488 views
  • Likes 8 likes
  • Comments 27 comments

Enhancing a Magnifying Headband with Auto Sensing Light -- Episode 585

Do you often use a illuminated magnification headband? Do you get annoyed that you need to turn it off and on when looking away from your work? This project contains 2 solutions, a basic tilt sensor option that can be added in minutes, and a more complex distance detecting circuit which will change the illumination depending on how far away the object you are looking at is.

Watch the Video:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Bonus Content:

  • Download Code and Schematics

Bill of Material:

Product Name Manufacturer Quantity Buy Kit
LC1780USB Magnifier, Spectacles & Headband, 1x, 1.5x, 2x, 2.5x & 3.5x LIGHTCRAFT 1 Buy Now
102010328 Arduino Microcontroller Board, SAMD21G18, ARM Cortex-M0+ SEEED STUDIO 1 Buy Now
STMICROELECTRONICS Daughter Board, VL53L0X Gesture and Ranging Sensor, FlightSense STMICROELECTRONICS 1 Buy Now
MICROCHIP Power MOSFET, N Channel, 60 V, 200 mA, 5 ohm, TO-92, Through Hole MICROCHIP 1 Buy Now
COMUS (ASSEMTECH) Tilt Switch, 15 °, 60 Vac, 0.25 A, Nickel COMUS (ASSEMTECH) 1 Buy Now
 

element14 presents

element14 presents  |  About Katie Dumont |  Project Videos

  • tilt
  • e14p_KD
  • magnification
  • Xiao
  • Distance sense
  • illuminate
  • modify
  • friday_release
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • hifromkatie
    hifromkatie over 3 years ago in reply to DAB +1
    Thanks, it hard to find the culprit further than "something under the epoxy blob", by bypassing the switch circuit which has the auto power off and other stuff hidden under expoxy, the problem is resolved…
  • hifromkatie
    hifromkatie over 3 years ago in reply to dougw

    Separating the supply is a good call. I had been hoping to do a bit of a redesign and get a fix before the video was out, but Christmas got in the way.
    The Micro or the Sensor aren't resetting/browning out, as comms says up between the 2 of them, and the PC without missing a beat (or bit).
    My next call is to remove the switch and the PCB it's attached to (which at a minimum has some sort of switch IC under the blob) and replace them with a latching switch.
    That should fix it, as when the micro is plugged in to the USB, and the switch on the light is off it all works as it should with no flickering, it's only as soon as the battery is powering it through that switch PCB that it begins to fail.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 3 years ago

    Could be power or it could be software.

    You can check if it is the latter with the following code which should turn the LEDs on for 5s then off for 5s. If you still get flickering then it's probably not to do with your code.

     unsigned long time;

    bool led = 0;

    void setup() {
    pinMode(ledPin, OUTPUT);
    digitalWrite(ledPin, LOW);

    if (!lox.begin()) {
    while(1);
       }

    time = millis();
    }

    void loop() {
    VL53L0X_RangingMeasurementData_t measure;

    lox.rangingTest(&measure, false); // pass in 'true' to get debug data printout!

    if (measure.RangeStatus != 4) { // phase failures have incorrect data
    distance = measure.RangeMilliMeter;
    }

    if (millis() - time > 5000) {
          led = !led;
          digitalWrite(ledPin, led);
          time = millis()

    }

    delay(100);

    There's also a different example you can base your solution on which is the continuous scan. 

    https://github.com/adafruit/Adafruit_VL53L0X/blob/master/examples/vl53l0x_continuous/vl53l0x_continuous.ino


    You mentioned a blob chip on the visor. We can speculate what this might do, it could be something like an LED driver or perhaps something that does an auto power off? It might also be a voltage booster depending on how the LEDs are being driven.
    Obvious thing is to try and bypass that and drive the LEDs yourself. You've got a microcontroller there so you could use an PWM output to drive your FED instead of a simple digital one.






    github.com/.../vl53l0x_continuous.ino

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 3 years ago

    Nice project!

    Just curious, what resistance is in series with the LED? The schematic shows 1 kohm, but I'm guessing that was for the red LED, and not the one in the head-magnifier. It could be worth increasing the resistance slightly, to see what happens. It could be a brownout causing a repeated reset of the microcontroller. 

    If you can't access the LED to see what resistance was in there by the manufacturer (assuming they did that!) then just another resistor could be added, e.g. 100 ohm or 47 ohm just to see what happens.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kmikemoo
    kmikemoo over 3 years ago

    hifromkatie  Nice project.  I LOVED the troubleshooting.  Getting out the oscilloscope... brilliant.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 3 years ago in reply to dougw

    and/or filtering of the range readings.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 3 years ago

    Another thought. If the flickering is due to range fluctuations, you could add hysteresis to your range decision.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 3 years ago

    Check if the FET control signal is "flickering".

    You can separate the supply to the MCU with a diode and capacitor. If the sensor is dragging the supply around, power it directly or separately from the battery (have the diode and capacitor only on the MCU. 

    If the MCU is not crashing, it should also be possible to put a diode and capacitor on the FET control signal, to prevent it from flickering.

    If there really isn't enough current to run everything even with diode separation, one thing to try is running the MCU and sensors from a separate battery.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<