Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents DIY Open Source Bluetooth Headphones -- Episode 586
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 17 Jan 2023 3:59 PM Date Created
  • Last Updated Last Updated: 20 Jan 2023 8:24 AM
  • Views 37426 views
  • Likes 6 likes
  • Comments 41 comments

DIY Open Source Bluetooth Headphones -- Episode 586

Dodgy apps, subscription fees, and exclusive phone apps for a pair of headphones? Clem says: no thanks! He's fed up with the shenanigans some manufacturers pull for simple products that should just work. And why change to a different model of headphones when you've found the perfect wired pair? Can't you have that same fit and style, but wireless? So, for this project, Clem sets out to add Bluetooth to some of his favorite wired AKG headphones, using a DFRobot FireBeetle and an I2S audio module. But, to be a true open-source alternative, Clem has to whip up a custom PCB, which doesn't go according to plan. Learn the pitfalls of overly similar part numbers by following his process of figuring out the problem! What Device should have an open source variant in your opinion and would you build it yourself?

Watch the Video:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Bonus Content:

  • Download All CAD and Code for Free!

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Bill of Material:

Product Name Manufacturer Quantity Buy Kit
DF robot firebeetle Esp32 DFROBOT 1 Buy Now
 

Additional Parts:

PCM5100 i2s module
Your favourite wired headphones

element14 presents

element14 presents  |  About Clem  |  Project Videos

  • DFrobot Firebeetle
  • Bluetooth Headphones
  • diy
  • e14_CMM
  • open source
  • I2S audio module
  • friday_release
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • beacon_dave
    beacon_dave over 3 years ago +1
    This was another interesting element14 presents project. Up until now I've been using the likes of Denon or Radial Engineering Bluetooth receivers: https://www.denonpro.com/products/view/dn-200br …
Parents
  • beacon_dave
    beacon_dave over 3 years ago

    This was another interesting element14 presents project.

    Up until now I've been using the likes of Denon or Radial Engineering Bluetooth receivers:  

    https://www.denonpro.com/products/view/dn-200br

    https://www.radialeng.com/product/bt-pro

    to accommodate those pesky mobile device users... Starts to get expensive when you need to pair with multiple devices.

    However, this open-source project looks like this could open up some alternatives and experimentation.

    USB Audio 'Class Compliant' interfaces would be another interesting area to explore further. It would be great to have some 'problem-solving' adapters that can plug into a computer USB port without needing additional drivers and provide basic channel mixing / splitting type functionality along with basic level control and metering, ideally all within the limited USB power budget to avoid the need for yet another wall wart power supply.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mayermakes
    mayermakes over 3 years ago in reply to beacon_dave

    that sounds indeed like a neat problem solving product! would be cool to elaborate on that.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to mayermakes

    To keep it simple, the mono/stereo could perhaps just be a pair of slide switches.

    I was concerned about the power consumption of the addressable LED VU meters but it makes for an interesting UX feature.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mayermakes
    mayermakes over 3 years ago in reply to beacon_dave

    I think some dinky 20mA leds would be bright enough, no need for fancy neopixels IMO
    since the device could fall under the EU- USB-C recommendetion the power limitations of USB 1.1. don't apply really, but having it all doable with 5V @500mA would of course be preferrable for max compability.

    slide switches would be the simplest way for passive routing ,but beeing able to mix them lets say via digital pot would be cool...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to mayermakes

    Yes, that was intended as a separate project idea.  Slight smile

    ( The Inogenie devices do the webcam switching:
    https://inogeni.com/product/share2u/  )

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mayermakes
    mayermakes over 3 years ago in reply to beacon_dave

    Seems the intended use is dunymic composition of additional sources into an hdmi feed, that is passed on downstream.
    yeah a simpler solution for just the mentioned usecase seems to fit aniche here!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to mayermakes

    They do a 4:1 switcher 2xUSB/2xHDMI as well:

    https://inogeni.com/product/cam300/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to mayermakes

    Originally, I was thinking of passive routing with the switches but then I was thinking of GPIO inputs so that their function could be defined in software depending on an individual's use case making it more flexible.

    They could also be push buttons though that act as a simple mode selector that uses the LED VU bar position to show what mode you are in and then the rotary selector does inc/dec push to set.

    5V at 500mA would be ideal as there is a lot of kit out there that isn't USB-C yet. It could use a second USB port though to bring it up to 1000mA, without reaching for a wall-wart PSU.  

    In a lot of cases, the LEDs don't need to be on for the duration. They would mainly be used for configuration purposes, so a small battery could be used to provide the additional power demand for LEDs or even a small OLED display. However that adds to the design.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mayermakes
    mayermakes over 3 years ago in reply to beacon_dave

    oh i just saw how expensive these devices are, well a simple solution just focused on the task would surely be abit more accessibly priced.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mayermakes
    mayermakes over 3 years ago in reply to beacon_dave

    the internal battery for the higher demands and charging while its not in use is such a cool idea, of course it adds complexity but would also make the device better for payortable applications like podcasting on site.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to mayermakes

    That's one of the problem areas, most people can probably pull together a few low-cost USB devices, but when it comes to using several together, it can quickly become an overly complicated and expensive business.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mayermakes
    mayermakes over 3 years ago in reply to beacon_dave

    also making them all play nicely togethers and have no wonky conenctions is a cluttered desk in itself

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mayermakes
    mayermakes over 3 years ago in reply to beacon_dave

    also making them all play nicely togethers and have no wonky conenctions is a cluttered desk in itself