Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents Repairing a Neewer 660 Studio light - How Hard Can It Be? -- Episode 594
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 9 Mar 2023 2:01 AM Date Created
  • Last Updated Last Updated: 17 Mar 2023 8:24 AM
  • Views 24998 views
  • Likes 10 likes
  • Comments 46 comments

Repairing a Neewer 660 Studio light - How Hard Can It Be? -- Episode 594

I’ve got a studio light which has suddenly become faulty, how hard could it be to fix it rather than replace? In today’s episode I try and fault find the PCB to see if its a fault I can fix.

Watch the Video:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Bill of Material:

Product Name Manufacturer Quantity Buy Kit
8 bit MCU, STM8S003F3P6TR STMICROELECTRONICS 1 Buy Now
Fixed LDO Voltage Regulator HOLTEK 1 Buy Now
Pluggable Terminal Block WAGO 3 Buy Now
 

Additional Parts:

Fault studio light

element14 presents

element14 presents  |  About Katie Dumont |  Project Videos

  • fault finding
  • e14p_KD
  • neewar
  • Pluggable Voltage Regulator
  • 8 bit mcu
  • Fixed LDO Voltage Regulator
  • Studio Light
  • st
  • friday_release
  • led panel repair
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • hifromkatie
    hifromkatie over 3 years ago in reply to RichG +3
    I'm quite tempted to go completely away from the original design and do a 555 based controller, the main operation of the micro was to take the potentiometer input and turn it in to a PWM to the LED driver…
  • RichG
    RichG over 3 years ago +1
    Yes a new project with a microcontroller.
Parents
  • beacon_dave
    beacon_dave over 3 years ago

    You could perhaps look at adding:

    • wireless control that allows individual or group adjustments
    • DMX interface so as they can double up as party lights
    • preset store/recall option
    • display on the back
    • strobe feature 

    If you plan to re-lamp them in the future, then you could do RGB / white and then some colour temp control options.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to beacon_dave

    Might want to verify that the LED and driver side is still working before jumping head-first into a new microcontroller though. Something killed the microcontroller. 

    However looks like a good fevive for 'upcycling' as a lot of the tricky bits can be reused as is e.g. case with yoke attachment, barn doors attachments, battery holders, diffuser slot, rails for LED strips and so on. The single PCB looks like it could be traced and a new custom one dropped in to replace it. Perhaps all that is missing on that particular model is a cut-out for adding a LCD/OLED display.

    Do the rotary pots control the LED driver directly or are they analogue inputs into the microcontroller which are used to control the PWM to the driver ? Also, is there  a charging circuit for the camera battery pack portable power ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago in reply to beacon_dave

    I think we posted the same thing at the same time, nice work!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to scottiebabe

    I think I beat you to it by 4minutes Joy

    image

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago in reply to beacon_dave

    lol I don't know, I blame vernit! Zipper mouth

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to scottiebabe

    If you are connected to different forum instances, then two people can think they were both first to reply, but when things finally sync up, you realise you were beaten to it and now look as if you have just plagiarised the previous post Scream

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago in reply to beacon_dave

    I know posting the same idea 4 minutes later makes me look like even more of a goof than usual! Face palm

    But yes, I would be interested to  know if the MCU is bringing anything interesting to the party. Or is it just doing basic telemetry to for overtemperature and battery SOC shutdown... 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to scottiebabe

    Slight smile

    At first sight, the MCU appears a bit overkill for just dimming the LEDs. However perhaps they have just standardised on parts as some of the other models have to drive a small display screen.

    I was wondering what killed the MCU though. Did a failure in the driver dump 12v through the GPIO perhaps, which caused a short which killed the MCU regulator ? Quite often it is the LEDs that fail first as they are often pushed hard to get maximum light output. Chain reaction.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago in reply to beacon_dave

    Should have used a 7805/LM317, I'm sure that cheap CMOS LDO got up to no good when the 15V supply is plugged in.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hifromkatie
    hifromkatie over 3 years ago in reply to beacon_dave

    Lots of interesting ideas, in fact the replacement I got for this one is a new "upgraded" version which has a small LCD screen for displaying the brightness and colour temp, and is wirelessly controlled by a remote either individually or you can change all of them in a room at the same time!

    The LED side works perfectly, I checked that, but I don't think it made the cut for the video, we almost ended up with a 1hour long video of the highlights!
    Definitely will be reusing the external casing, barn doors, LED panel (It's a single PCB).
    The pots are analogue inputs to the micro which is then PWM control to the LED drivers, I'm tempted to simplify the circuit and make a drop in replacement PCB which will line up with the holes for the pots, but these will be fed into a 555  (or 556, as theres 2 to control) and output a PWM to the LED drivers.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • hifromkatie
    hifromkatie over 3 years ago in reply to beacon_dave

    Lots of interesting ideas, in fact the replacement I got for this one is a new "upgraded" version which has a small LCD screen for displaying the brightness and colour temp, and is wirelessly controlled by a remote either individually or you can change all of them in a room at the same time!

    The LED side works perfectly, I checked that, but I don't think it made the cut for the video, we almost ended up with a 1hour long video of the highlights!
    Definitely will be reusing the external casing, barn doors, LED panel (It's a single PCB).
    The pots are analogue inputs to the micro which is then PWM control to the LED drivers, I'm tempted to simplify the circuit and make a drop in replacement PCB which will line up with the holes for the pots, but these will be fed into a 555  (or 556, as theres 2 to control) and output a PWM to the LED drivers.