Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents Repairing a Neewer 660 Studio light - How Hard Can It Be? -- Episode 594
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 9 Mar 2023 2:01 AM Date Created
  • Last Updated Last Updated: 17 Mar 2023 8:24 AM
  • Views 24989 views
  • Likes 10 likes
  • Comments 46 comments

Repairing a Neewer 660 Studio light - How Hard Can It Be? -- Episode 594

I’ve got a studio light which has suddenly become faulty, how hard could it be to fix it rather than replace? In today’s episode I try and fault find the PCB to see if its a fault I can fix.

Watch the Video:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Bill of Material:

Product Name Manufacturer Quantity Buy Kit
8 bit MCU, STM8S003F3P6TR STMICROELECTRONICS 1 Buy Now
Fixed LDO Voltage Regulator HOLTEK 1 Buy Now
Pluggable Terminal Block WAGO 3 Buy Now
 

Additional Parts:

Fault studio light

element14 presents

element14 presents  |  About Katie Dumont |  Project Videos

  • fault finding
  • e14p_KD
  • neewar
  • Pluggable Voltage Regulator
  • 8 bit mcu
  • Fixed LDO Voltage Regulator
  • Studio Light
  • st
  • friday_release
  • led panel repair
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • hifromkatie
    hifromkatie over 3 years ago in reply to RichG +3
    I'm quite tempted to go completely away from the original design and do a 555 based controller, the main operation of the micro was to take the potentiometer input and turn it in to a PWM to the LED driver…
  • RichG
    RichG over 3 years ago +1
    Yes a new project with a microcontroller.
Parents
  • phoenixcomm
    phoenixcomm over 3 years ago

    When I said: "Use what you have and just build a new controller." I did not mean to trash the existing PCB. You have two parts on the current PCB: The drivers, and the 5vdc power supply. So the easy way is to Remove the CPU which gave up the magic smoke. Now you have to identify all of the outputs and inputs. Then you have a choice, use the same CPU as They did or one of your own on a small PCB and wire the IO pins to the others IO pins and write the code. I would stay away from parts that have potential "death upon read" - Good Luck.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hifromkatie
    hifromkatie over 3 years ago in reply to phoenixcomm

    I immediately thought I'd just replace the microcontroller with a replacement, and write my own code, especially as the programming header is on the PCB and easy to connect in to.
    I'm tempted to challenge myself and replace it with a 555 based circuit though, to output the PWM signal based on the pots to the LED drivers, potentially still using the existing drivers, but if I re do them, I can get a single drop in replacement PCB made with the 555s(/556), LED drivers and power produced, which I think would be a pretty neat solution, just a little more time consuming.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 3 years ago in reply to hifromkatie

      hifromkatie You are building a bigger box, for no reason. As an Integration & Sustaining Engineer, I used to work on all sorts of stuff,   And I had a problem, which you seem to have. STOP BUILDING BIGGER BOXES! It's a disease. please refer to Occam's razor. Where the simplest solution is most likely the best.  You started to build the bigger box:
         "I'm tempted to challenge myself and replace it with a 555-based circuit though, to output the PWM signal based on the pots to the LED drivers,              potentially still using the existing drivers, but if I redo them, I can get a single drop-in replacement PCB made with the 555s(/556), LED drivers and        power produced, which I think would be a pretty neat solution, just a little more time-consuming." 
    I hope you don't. do easier things like wire a new CPU to the board, maybe something different if you have the toolset. You just need to get the I/O of the new CPU to the old CPU and start to program it. AND get rid of the LDO in favor of a better device like an LM780x but with one more component a Zener Diode across the input side of the regulator and you want it about .5vdc above the input voltage. This way a transient from the wall wart, will not do any damage, as when the voltage rises it will be directed to the ground. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago in reply to phoenixcomm

    Forget about using C code, go with micropython Heart eyes KISS FTW!

    from machine import Pin, ADC, PWM
    from time import sleep
    
    warmPot = ADC(0)
    warmPWM = PWM(Pin(0))
    warmPWM.freq(1000)
    while True:
        warmPWM.duty_u16(warmPot.read_u16())
        sleep(0.01)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 3 years ago in reply to scottiebabe

    I like it, assuming that tiny MCU that can handle micropython.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago in reply to dougw

    Thanks, and Its a fair point! I had to splurge a few more dollars for a rpi pico.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • scottiebabe
    scottiebabe over 3 years ago in reply to dougw

    Thanks, and Its a fair point! I had to splurge a few more dollars for a rpi pico.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • kmikemoo
    kmikemoo over 3 years ago in reply to scottiebabe

    scottiebabe  Totally agree!  To save $2, you have to get into another programming interface.  If you are already using it, not a problem.  If not... Thumbsdown.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago in reply to kmikemoo

    Totally agree, I also recognize she has to produce an entertaining and educational video. Whatever she decides to do I know I'll enjoy the video and learn something new, katie is the best!

    I have also recently realized clipchamp is free on windows, what a hoot!