Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents Member Challenge Accepted - Universal LANC Controller for DSLR cameras -- Episode 595
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 16 Mar 2023 4:52 PM Date Created
  • Last Updated Last Updated: 24 Mar 2023 8:24 AM
  • Views 23956 views
  • Likes 11 likes
  • Comments 14 comments

Member Challenge Accepted - Universal LANC Controller for DSLR cameras -- Episode 595

The element14 community asks and Clem delivers. This time we are building a project suggested by one of our community members. An affordable open source alternative to expensive filmmaker gear, that allows anyone to control the focus and zoom of manual DSLR lenses similar to expensive professional Lanc and focus pulling systems. Clem wants to one up the commercial solutions in one key aspect, the unit has to be fully self contained, so no external battery packs needed. that is quite the challenge as it means he tries to run a Nema 17 stepper motor from just a single Lipo cell. Clem really needs to step up his power supply game for this project ;)

Watch the Video:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Bonus Content:

  • Download all the CAD and Code for Free

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Bill of Material:

Product Name Manufacturer Quantity Buy Kit
TRINAMIC / ANALOG DEVICES Evaluation Board, TMC2100 Bipolar Stepper Motor Driver, For StepStick TRINAMIC / ANALOG DEVICES 1 Buy Now
ONSEMI Linear Voltage Regulator, 7805, Fixed, 35V In, 5V And 1A Out, TO-252-3 ONSEMI 2 Buy Now
SANYO DENKI Stepper Motor, Single Shaft, 42 mm, Bipolar, 1.8 °, 0.186 N-m, 1 A SANYO DENKI 1 Buy Now
ANALOG DEVICES DC-DC Switching Buck, Boost Regulator, Adjustable, 2.3 to 5.5V in, 2.8 to 5.5V/1A out, LFCSP-10 ANALOG DEVICES 1 Buy Now
VISHAY Power Inductor (SMD), 1.5 µH, 9 A, Shielded, 18 A, IHLP-2525CZ-01, 2525 [6363 Metric] VISHAY 1 Buy Now
MULTICOMP PRO SMD Multilayer Ceramic Capacitor, 0.1 µF, 50 V, 0603 [1608 Metric], ± 10%, X7R, MC MULTICOMP PRO 4 Buy Now
MIKROELEKTRONIKA Rechargeable Battery, 3.7 V, Lithium Polymer, 2 Ah, JST MIKROELEKTRONIKA 1 Buy Now
MULTICOMP PRO Audio / Video Cable Assembly, 3.5mm Stereo Jack Plug, 3.5mm Stereo Jack Plug, 3.9 ft, 1.2 m, Black MULTICOMP PRO 1 Buy Now
MOLEX USB Connector, USB Type C, USB 3.1, Receptacle, 24 Ways, Surface Mount, Right Angle MOLEX 1 Buy Now
MCP73832T-2ACI/OT MICROCHIP 1 Buy Now
AP9101CK-AHTRG1 DioDES inc 1 Buy Now
DMN2024UQ-7 DioDES inc 2 Buy Now
DM1231-02SO-7 DioDES inc 2 Buy Now
Rotary encoder Bourns 1 Buy Now
3,5mm jack Kycon 2 Buy Now
 

Additional Parts:

MAYER MAKES Engineering Resin for the Case
Closed loop GT2 belt, Idlers and Pulley salvaged from a 3d printer.
DSLR Camera with manual Lens (Example shown Nikon d3300 and vintage Canon Fd lens)

element14 presents

element14 presents  |  About Clem  |  Project Videos

  • dc-dc
  • dslr
  • molex
  • focus pulling
  • diy
  • stepper motor
  • linear voltage regulator
  • analog devices
  • Filmmaker gear
  • boost regulator
  • friday_release
  • e14p_CMM
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply
Parents
  • phoenixcomm
    phoenixcomm over 3 years ago

    Clem, Good Solution. But the camera lens does not take kindly to large or even small side loads! Just a thought what would happen if you attached a 3D-printed gear to the lens ring?  just think of how you hold the camera and use just two fingers on the focus ring. You could do the same thing.  ~~ Cris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mayermakes
    mayermakes over 3 years ago in reply to phoenixcomm

    i have a commercial sidefocus for dslrs and the side loads are very comparable, moreover because the adjustments for the positioning of the motor(and in return the tension) is just held by friction, excerting to much force is not of aconcern as the camera would just turn a bit when the load gets to big, same with reachign endpositions (the belt just slips).
    A 3d printed ring with GT2 teeth would improve trackiong, but also loose this little safety feature. OS there are tradeoff to be made.
    for bigger lenses I would certainly recommend to print a ring with the right teeth as it might slip during fast movements.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mayermakes
    mayermakes over 3 years ago in reply to phoenixcomm

    i have a commercial sidefocus for dslrs and the side loads are very comparable, moreover because the adjustments for the positioning of the motor(and in return the tension) is just held by friction, excerting to much force is not of aconcern as the camera would just turn a bit when the load gets to big, same with reachign endpositions (the belt just slips).
    A 3d printed ring with GT2 teeth would improve trackiong, but also loose this little safety feature. OS there are tradeoff to be made.
    for bigger lenses I would certainly recommend to print a ring with the right teeth as it might slip during fast movements.