Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents DIY AC Dimmer Circuit: Control Your Lights with a Raspberry Pi Pico -- Episode 602
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 3 May 2023 6:50 PM Date Created
  • Last Updated Last Updated: 12 May 2023 7:24 AM
  • Views 29657 views
  • Likes 9 likes
  • Comments 11 comments

DIY AC Dimmer Circuit: Control Your Lights with a Raspberry Pi Pico -- Episode 602

Dimmer circuits consisting of Phase Angle Control are used to efficiently adjust the AC power delivered to the AC loads by controlling the conduction angle. In this episode, Surbhika developed such a circuit to enable dimming of commonly used AC lights bulbs at home. This was an interesting DIY project as it meant realizing one of the fundamental concepts in power electronics and control theory to generally usable hardware.

Watch the Video:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Bonus Content:

  • Download Code!
image image

Bill of Materials

Product Name Manufacturer Quantity Buy Kit
RASPBERRY-PI Raspberry Pi Pico Board, RP2040, 32 bit, ARM Cortex-M0+ RASPBERRY-PI 2 Buy Now
MULTICOMP PRO TERMINAL BLOCK EUROSTYLE, 2 POSITION, 26-16AWG MULTICOMP PRO 5 Buy Now
ONSEMI Optocoupler, Triac Output, DIP, 6 Pins, 5.3 kV, Non Zero Crossing, 400 V ONSEMI 1 Buy Now
VISHAY Optocoupler, Transistor Output, 1 Channel, DIP, 4 Pins, 50 mA, 5.3 kV, 160 % VISHAY 1 Buy Now
WEEN SEMICONDUCTORS Triac, 800 V, 16 A, TO-220AB, 1.5 V, 170 A, 45 mA WEEN SEMICONDUCTORS 1 Buy Now
BOURNS LINEAR POTENTIOMETER, 10KOHM, 20%, 50mW BOURNS 1 Buy Now
PHILIPS LIGHTING LED Light Bulb, Reflector, GU10, Warm White, 3000 K, Dimmable, 36° PHILIPS LIGHTING 1 Buy Now
ETERNA GU10 Lampholder with Flying Leads ETERNA 1 Buy Now
LEDVANCE LED Light Bulb, Reflector, GU10, Daylight White, 6500 K, Not Dimmable, 36° LEDVANCE 1 Buy Now
 

image

element14 presents  |  About Surbhika |  Project Videos

  • AC power control
  • ac dimmer
  • home automation
  • raspberry pi pico
  • Dimmer switch
  • power control
  • triac
  • optocoupler
  • Light dimming
  • raspberry pi
  • circuit design
  • Phase angle control
  • electrical engineering
  • energy efficiency
  • e14p_SR
  • diy electronics
  • friday_release
  • pi pico
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • michaelkellett
    michaelkellett over 3 years ago +3
    The subject is interesting (although some discussion of EMC issues would be helpful) but the bench practice is life threateningly dangerous. Main voltages should never be applied to a breadboard operated…
  • surbhika
    surbhika over 3 years ago in reply to Workshopshed +1
    No the optocoupler IC does the isolation. I see the confusion arises due to the improper symbol of SFH628A. Thanks for pointing that out! It should be like this (as given in the datasheet):
Parents
  • CharlieDelta
    CharlieDelta over 1 year ago

    May be a good solution would be to use a 12 volt lamp run from a mains transformer as the load. In this case there would be no issues with electrical safety. As an alternative may be you should use an opto-triac (eg CT3021) to trigger the main triac. This would then provide the requisite electrical isolation   when using a mains driven light bulbs. I believe that there are a number of assembled boards on the market (eg  RobotDyn) but be AWARE that some of them do not have the required mains isolation between pcb traces.
    Perhaps an interesting extension would be to use the Pico PIO circuits to control the triac firing so that the Pico could get on with other things (like measuring the local temperature or light levels) and working remotely over WiFi using (say) one of the new ESP8285 modules (or even the Pico W) .
    Just some ideas. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • CharlieDelta
    CharlieDelta over 1 year ago

    May be a good solution would be to use a 12 volt lamp run from a mains transformer as the load. In this case there would be no issues with electrical safety. As an alternative may be you should use an opto-triac (eg CT3021) to trigger the main triac. This would then provide the requisite electrical isolation   when using a mains driven light bulbs. I believe that there are a number of assembled boards on the market (eg  RobotDyn) but be AWARE that some of them do not have the required mains isolation between pcb traces.
    Perhaps an interesting extension would be to use the Pico PIO circuits to control the triac firing so that the Pico could get on with other things (like measuring the local temperature or light levels) and working remotely over WiFi using (say) one of the new ESP8285 modules (or even the Pico W) .
    Just some ideas.