Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents Charlieplexing Buttons and LEDs at the Same Time - How Hard Can It Be? -- Episode 604
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 10 May 2023 5:43 PM Date Created
  • Last Updated Last Updated: 26 May 2023 7:24 AM
  • Views 32169 views
  • Likes 9 likes
  • Comments 15 comments

Charlieplexing Buttons and LEDs at the Same Time - How Hard Can It Be? -- Episode 604

So many buttons so little IO. When you want to drive a large number of LEDs or read buttons the obvious choice is multiplexing them. But there is a method called charlieplexing that lets you use even more LEDs and buttons with even less IO pins. Clem wants to interface a large amount of buttons and LEDs with a microcontroller but has a limited number of pins.   He's also trying to save money on parts. Could you just replace expensive signal diodes with cheap LEDs? Could you use the same pins to read buttons and drive LEDs in the same matrix? Could you also achieve true n-key rollover without having a diode on every single button? How hard can it be?

Watch the Video:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Bonus Content:

  • Login to Download the Code!

Bill of Material:

Product Name Manufacturer Quantity Buy Kit
LED, Super Red, Through Hole, T-1 3/4 (5mm), 12 mA, 5 V, 640 nm Multicomp 9 Buy Now
Arduino Mega 2560, ATmega2560, 54 I/O, 256KB Flash, 8KB SRAM, 4KB EEPROM Arduino 1 Buy Now
Jumper Wire Kit, Multicolour, 2 mm - 125 mm, 22 AWG, 140 Piece Multicomp 1 Buy Now
Breadboard, Mounted, 1580 Pin, 10mm, x 135mm Multicomp 1 Buy Now
 

element14 presents

element14 presents  |  About Clem  |  Project Videos

  • buttons
  • keyboard
  • multiplexing
  • leds
  • Charlieplexing
  • arduino
  • friday_release
  • arduino mega
  • e14p_CMM
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply
Parents
  • phoenixcomm
    phoenixcomm over 3 years ago

    I ran into "Charlieplexing", about 20 years ago when I was going to use a MAX6954 to drive four 16-segment incandescent and another thirteen 7-segment incandescent displays. The displays are used on my NAV panel, Since they are incandescent and not LED my search continues. My search continued for some time, and basically, it takes an entire Arduino Mega to do the job, :(   plus a boatload of BJTs (Bipolar Junction Transistor) as it turns out you need one BJT on every segment, and one more for the common rail. So It's a lot of parts. this includes two BCD to 7 segment decoders as the fan-out is too much, could use three but then there are the enables to consider.

    The 16 segments are going to be driven directly (via BJTs) to one group of 4 devices. So I need 145 segment pins plus 17 more for the column drive. I you don't want to see refresh then your rate is < 0.2 seconds, and if you do the math .20 / 17 you end up with 0,011764706 if you round down it's 0.012 sec/per column. ouch. 

    In my opinion, "Charlieplexing" is nice but I really don't want to use this technic, as you don't want to try and fix a dead segment. :( It's a headache and you will need more than a few pints to get through it. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mayermakes
    mayermakes over 3 years ago in reply to phoenixcomm

    yeah, its obvious why its mostly done with leds and buttons, and not high current devices.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mayermakes
    mayermakes over 3 years ago in reply to phoenixcomm

    yeah, its obvious why its mostly done with leds and buttons, and not high current devices.