Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents Handheld BASIC computer in Badge Format with the Arduino Uno -- Episode 612
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 19 Jul 2023 4:47 PM Date Created
  • Last Updated Last Updated: 6 Nov 2023 12:11 PM
  • Views 28925 views
  • Likes 12 likes
  • Comments 42 comments

Handheld BASIC computer in Badge Format with the Arduino Uno -- Episode 612

Since the new 32-Bit Arduino Uno R4 has arrived, it is time to make a glorious farewell project to the classic 8-Bit UNO R3, by using all the pins and turning it into a handheld BASIC computer, quite similar to a ZX81 from the 80s! It is finally time to build a badge that uses up all the pins and shows that an 8-Bit microcontroller is in fact a tiny computer! The badge form factor makes it ideal for your next meetup with fellow makers!

Watch the Video:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Can the Arduino UNO Function as a Computer?

Clem introduces us to the extraordinary world of the Arduino Uno R3 and its farewell project, reminding us that the microcontrollers we use on Arduinos are more than just components; they are real computers. Inspired by the possibilities, he embarks on a journey to create an Arduino Uno-based handheld computer that rivals the capabilities of the ZX-81.

TinyBASIC Plus v0.15

The Hardware is more than BASIC

His project begins with Tiny Basic, a complete BASIC programming environment for Arduino. Tiny BASIC barely fits on an ATmega 238p on its own, so Clem utilizes a secondary chip to read the keyboard and drive the screen, offloading these tasks from the main processor running the operating system. This ensures that we have 1k of RAM left for writing programs (in the same ballpark as the Zx81). To make it fully portable, Clem incorporates a second processor to handle the keyboard and LCD screen, allowing the main microcontroller to focus solely on the operating system.

CAD Screenshot

Even a BASIC Computer needs a Keyboard

With a custom PCB, Clem designs a badge-sized handheld computer. A tiny keyboard for the thumbs and a character LCD for text output complete the device. Throughout the process, Clem faces challenges in LED addressing and keyboard functionality but manages to get it all working.

3D Printed Enclosure

Complimented by a 3D Printed Enclosure

The finished handheld computer badge is a testament to the power and versatility of the Arduino Uno R3. By utilizing all available pins and space on the chip, Clem successfully transforms the Arduino Uno into a handheld computer with capabilities like the ZX-81. The project serves as a fitting tribute to the beloved Arduino Uno R3 and showcases the potential for DIY electronics with microcontrollers.

Creating this handheld computer badge exemplifies the essence of the Arduino community—innovation, exploration, and a passion for pushing the boundaries of what's possible with electronics.

Bonus Content:

  • Download Code and CAD Files!
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
Bill of Material:

Product Name Manufacturer Quantity Buy Kit
Arduino uno R4 minima ARDUINO 1 Buy Now
FORDATA Alphanumeric LCD, 20 x 4, Black on Yellow / Green, 5V, English, Euro, Transflective FORDATA 1 Buy Now
MULTICOMP PRO LED, Green, SMD, 0603 [1608 Metric], 20 mA, 2.3 V, 577 nm MULTICOMP PRO 55 Buy Now
C&K COMPONENTS Tactile Switch, PTS645 Series, Top Actuated, Through Hole, Round Button, 130 gf, 50mA at 12VDC C&K COMPONENTS 50 Buy Now
MICROCHIP 8 Bit MCU, AVR ATmega Family ATmega328 Series Microcontrollers, AVR, 20 MHz, 32 KB, 32 Pins, TQFP Microchip 2 Buy Now
IQD FREQUENCY PRODUCTS Oscillator, Crystal, 16 MHz, 50 ppm, SMD, 7mm x 5mm, 5 V, CFPS-72 Series IQD FREQUENCY PRODUCTS 2 Buy Now
MICROCHIP Fixed LDO Voltage Regulator, 2.1V to 6V, 210mV Dropout, 5Vout, 500mAout, SOT-223-3 MICROCHIP 2

Buy Now

 

Additional Products:

CASE 3d printed with MAYER MAKES ENGINEERING RESIN
+ Blue dye

element14 presents

element14 presents  |  About Clem  |  Project Videos

  • sinclair
  • pocket computer
  • arduino uno
  • tiny BASIC
  • retro computer
  • uno r4
  • uno r3
  • zx81
  • 80s computer
  • arduino uno r3
  • friday_release
  • e14p_CMM
  • basic computer
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 3 years ago in reply to Jan Cumps +1
    can't add a Youtube video anymore it seems, but here's a direct link: https://youtu.be/ThXslt1hTV0
Parents
  • ElectronicDuke
    ElectronicDuke over 1 year ago

    YT video mentions that this project was only for the Arduino UNO R3 SMD version at the beginning.  Why is the R4 on the BOM?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mayermakes
    mayermakes over 1 year ago in reply to ElectronicDuke

    So you have a source /link for the new one.
    I used the bare atmega328 chips on a custom pcb as also noted in the BOM, but the project would also run on two Arduino uno R3.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mayermakes
    mayermakes over 1 year ago in reply to ElectronicDuke

    So you have a source /link for the new one.
    I used the bare atmega328 chips on a custom pcb as also noted in the BOM, but the project would also run on two Arduino uno R3.