Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents Building a Magic Wand Talking Sound Board -- Episode 613
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 26 Jul 2023 10:29 PM Date Created
  • Last Updated Last Updated: 28 Jul 2023 7:24 AM
  • Views 17732 views
  • Likes 7 likes
  • Comments 15 comments

Building a Magic Wand Talking Sound Board -- Episode 613

In this episode, Mark Donners demonstrates how to create a captivating magical wand board using polymer clay. The wall-mounted ornament showcases several magic wands, each producing unique effects when activated. With a custom-designed PCB and Arduino Nano, the ornament comes alive with interactive LED strips and sound effects. The tutorial covers clay molding, power management, and Arduino programming, enabling makers to personalize their creations and add an element of whimsical magic to their workspaces. Unleash your creativity and explore the possibilities of this enchanting project. 

Watch the Video:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

In this episode of element14 presents, Mark demonstrates how to build a magical gadget for the office—a wall-mounted ornament adorned with magic wands. Rather than using wood, he opts for polymer clay as the material of choice, providing a more malleable and customizable medium for the project. Mark takes inspiration from eBay's examples and starts shaping the clay into the desired scroll-like ornament. After moulding and letting the clay dry, he achieves an antique appearance by adding paint for an aged parchment look. 

Rolling clay

Another Kind of Hardware

The next step involves incorporating electronics into the ornament. Mark provides two options for powering the setup. The first involves using an Arduino Nano and an SD card module for playback, but this lacks power management, requiring a manual switch for on/off. The second option is a custom-designed PCB with advanced power management, making it more automatic. He shares the schematic for both approaches, emphasizing the versatility of the clay material even when dry. The clay allows for drilling holes and adjustments, facilitating the installation of components like connectors and speakers. 

Hardware layout

Introducing the Magic

Moving on to the software, Mark walks through the Arduino sketch he wrote, which uses various libraries for SD card access, button inputs, and Neopixel control for LED strips. The code cycles through different wand effects, playing random sounds for each one. The final product allows for interactive fun in the office, helping colleagues to make decisions or simply enjoy a magical experience. 

Custom PCB

Taming Electricity inside Rocks

Mark also provides an overview of his PCB design, showcasing the power management circuitry, the level shifter, and the connections for the Arduino Nano, SD card, and LED strip. The assembly process is straightforward, and he demonstrates how to wire the components onto the board. With the setup complete, the magical ornament responds to button presses, activating random wand effects with accompanying sounds, adding an element of excitement to the office. 

All done

This project encourages creativity and experimentation, as makers can customize the ornament's appearance and even modify the sounds and effects to suit their preferences. With this magical wand board, adding a touch of enchantment to the office has never been more accessible and fun. So why not indulge in a bit of office magic and see where the wands take you? 

Bonus Content:

  • Download Code, Schematics, CAD Files, and More!
  • Pre-assembled PCB

Bill of Material:

Product Name Manufacturer Quantity Buy Kit
Arduino Nano, Evaluation Board Arduino 1 Buy Now
Switch, SPST 3A 125V Solder Multicomp Pro 1 Buy Now
Battery Retainer Clip Bud Industries 1 Buy Now
Loudspeaker, Sub Miniature Projects unlimited 1 Buy Now
 

Additional Parts:

Fumo Synthetic Clay
Magic Wands…..Just go the the forest and pick up come branches…or order movie props.
LedStrip WS2812 Pixelledstrip about 20 leds max
9V Battery PP3 format
PCB, download the PCB production files from the Element 14 Community Project page and order your own at your favourite PCB manufactorer or order a pre-assembled version ( SMD only) here
https://www.tindie.com/products/markdonners/talking-cr-timers-pcb/
Headers and sockets and some wires

element14 presents

element14 presents  |  About Mark Donners |  Project Videos

  • synthetic clay
  • Office Gadget
  • potter
  • Wands
  • Gadget
  • e14p_MD
  • magic wand
  • talking sound board
  • custom pcb
  • arduino
  • friday_release
  • magic
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply
Parents
  • baldengineer
    baldengineer over 3 years ago

    Cool project and excellent build. The wands and board look great!

    It gives me the idea of making a task tracking board where you remove the wand for the current task you're working on. (Then track the time for that task.)

    It would be a bit of overkill but would add some fun to mundane activities.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • donnersm
    donnersm over 3 years ago in reply to baldengineer

    Now, why didn't I think of that! Nice idea. And if I did that, I could remove the random generator and play a specific sound for each wand when it was picked up.....hmmm...Feel a version 2.0 brewing

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • donnersm
    donnersm over 3 years ago in reply to baldengineer

    Now, why didn't I think of that! Nice idea. And if I did that, I could remove the random generator and play a specific sound for each wand when it was picked up.....hmmm...Feel a version 2.0 brewing