Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents All-Purpose Debugging: A Practical Universal Screen with LCD Displays -- Episode-631
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 30 Nov 2023 2:59 PM Date Created
  • Last Updated Last Updated: 1 Dec 2023 2:34 PM
  • Views 4748 views
  • Likes 10 likes
  • Comments 17 comments

All-Purpose Debugging: A Practical Universal Screen with LCD Displays -- Episode-631

In every maker project, there comes a moment when a specific tool would be immensely beneficial. Sometimes, that tool is unavailable, not yet acquired due to cost, or simply doesn't exist commercially. Clem frequently encounters such challenges, particularly in projects involving various forms of serial communication. While plugging a project into a PC during software development is common, it underutilizes the PC's capabilities and is inconvenient for Clem's soldering workbench setup. Clem’s "00Screen" project emerges as a solution, providing a portable display for quick serial checks during hardware debugging, addressing challenges like misbehaving Wi-Fi projects and brownouts during boot. 

Watch the Video:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Clem's 00Screen serves as a universal Serial/USB/Wi-Fi display, aptly named after its starting point, "00" representing the first address in a computer's memory. Central to the design is the readability of information, as it features a Midas HD44780 compatible alphanumeric LCD with a generous 40x4 character array size. Clem's fondness for the classic backlit LCD, demonstrated in a previous build (Basic Badge Computer), influences the form factor of the device. The ESP32-S2 Wroom module serves as the project's brain, utilizing leftover parts from previous element14 presents videos, creating a curious resemblance to a laptop. 

 image

Utilizing components from past projects, such as the Molex FPC connector from the BLE Keyboard episode and the MCP1825S LDO used in numerous 2021/2022 projects, Clem emphasizes sustainability in design. Clem showcases the already-working unit, emphasizing that the code is mainly composed of standard Arduino libraries. He highlights the ease of adding custom functions to the device, providing flexibility for makers. 

 image

The integrated LiPo cell allows Clem to take the 00Screen anywhere without worrying about a power source. 3D-printed adjustable feet, designed in FreeCAD, facilitate convenient mounting. The device's functionality, including source selection with buttons and indications for new data through a blinking display and beep, is demonstrated. Clem showcases USB and UDP Wi-Fi messages, emphasizing the buzzer as a convenient feature to alert him without needing to look at the display. The 00Screen stands not only as a solution to a specific problem, but also as a testament to Clem's resourceful and sustainable approach to electronics projects. 

image

image

Links and Downloads:

  • Download CAD Files and Code!

Bill of Material:

Product Name Manufacturer Quantity Buy Kit
MULTICOMP PRO MP-ABI-050-RC MULTICOMP PRO 1 Buy Now
MIDAS DISPLAYS MC44005A6W-SPTLY3.3-V2 MIDAS DISPLAYS 1 Buy Now
MULTICOMP MC32829 MULTICOMP 2 Buy Now
MOLEX 105450-0101 molex 1 Buy Now
MICROCHIP MCP73831T-2ACI/OT MICROCHIP 1 Buy Now
DIODES INC. AP9101CK-AHTRG1 DIODES INC. 1 Buy Now
DIODES INC. DMN2024UQ-7 DIODES INC. 3 Buy Now
MIKROELEKTRONIKA MIKROE-1120 MIKROELEKTRONIKA 1 Buy Now
MOLEX 52207-1033 Molex 1 Buy Now
MICROCHIP MCP1825S-3302E/DB MICROCHIP 2 Buy Now
 

Additional Parts:

PCB available at Aisler: https://aisler.net/p/VBTWNVFJ
Esp32-S2 Wroom  (NRND)
slide switch with 2,54mm spacing

element14 presents

element14 presents  |  About Clem  |  Project Videos

  • LiPo cell portable power solution
  • USB and UDP-wifi message demonstration
  • Wifi message board
  • Ble Keyboard episode components
  • USB Display
  • ESP32-S2 Wroom module applications
  • lcd display
  • Maker project display solution
  • serial data
  • HD44780 compatible alphanumeric LCD
  • Arduino library customization
  • Serial communication debugging tool
  • 3D printed adjustable feet design
  • KiCad PCB design tutorial
  • MCP1825S LDO applications
  • Element14 present video project
  • friday_release
  • Clem's electronics project insights
  • Serial display
  • Sustainable electronics design
  • "00Screen" universal display
  • e14p_CMM
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • gam3t3ch
    gam3t3ch over 2 years ago +1
    funny how after watching this.....I need this now lol great job mayermakes
Parents
  • genebren
    genebren over 2 years ago

    I really enjoyed your episode! I found it to be supportive of an idea that I have working on for a little while now.

    I am working on building a handheld terminal that will allow me to communicate with devices that are using EnOcean transcievers (I am using several of these in home automation projects).  As I was laying things out, I thought about using and LCD display and joystick as the UI portion of the terminal, when I also thought how convenient it would be to have an I2C interface to a generic LCD module that I could use in future projects.  Wow, if I get really fancy like you, I could add a couple more interfaces to the LCD module, making it more useful to other projects.

    The added benefit to this approach is that I can free up pins from my ATTINY3225 processor to handle all of the other circuitry (EnOcean and USB transceivers, battery charger, LEDs) in my terminal board and use I2C to communicate with the LCD module/joystick module.

    Thanks, and keep up the good work!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • genebren
    genebren over 2 years ago

    I really enjoyed your episode! I found it to be supportive of an idea that I have working on for a little while now.

    I am working on building a handheld terminal that will allow me to communicate with devices that are using EnOcean transcievers (I am using several of these in home automation projects).  As I was laying things out, I thought about using and LCD display and joystick as the UI portion of the terminal, when I also thought how convenient it would be to have an I2C interface to a generic LCD module that I could use in future projects.  Wow, if I get really fancy like you, I could add a couple more interfaces to the LCD module, making it more useful to other projects.

    The added benefit to this approach is that I can free up pins from my ATTINY3225 processor to handle all of the other circuitry (EnOcean and USB transceivers, battery charger, LEDs) in my terminal board and use I2C to communicate with the LCD module/joystick module.

    Thanks, and keep up the good work!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • mayermakes
    mayermakes over 2 years ago in reply to genebren

    Exactlyx that is the purpose of the device, you fully got it! I2C Sp etc are just a bit of code away you have exposed uart pins that can be remapped thangs to pinmux of the esp32s2. But of course you can also alter the design to use a different mcu that allows for HW I2C etc to be tracked which further offloads computing power.